sl_iostream_leuart_context_t Struct Reference

Struct representing an IO Stream LEUART context.

#include <sl_iostream_leuart.h>

Data Fields

sl_iostream_uart_context_t context
 underlying uart context
 
LEUART_TypeDef * leuart
 leuart instance handle
 
CMU_Clock_TypeDef clock
 Peripheral Clock.
 
GPIO_Port_TypeDef tx_port
 Transmit port.
 
unsigned int tx_pin
 Transmit pin.
 
GPIO_Port_TypeDef rx_port
 Receive port.
 
unsigned int rx_pin
 Receive pin.
 

Struct representing an IO Stream LEUART context.

Field Documentation

◆ context

sl_iostream_uart_context_t sl_iostream_leuart_context_t::context

underlying uart context

◆ leuart

LEUART_TypeDef* sl_iostream_leuart_context_t::leuart

leuart instance handle

◆ clock

CMU_Clock_TypeDef sl_iostream_leuart_context_t::clock

Peripheral Clock.

◆ tx_port

GPIO_Port_TypeDef sl_iostream_leuart_context_t::tx_port

Transmit port.

◆ tx_pin

unsigned int sl_iostream_leuart_context_t::tx_pin

Transmit pin.

◆ rx_port

GPIO_Port_TypeDef sl_iostream_leuart_context_t::rx_port

Receive port.

◆ rx_pin

unsigned int sl_iostream_leuart_context_t::rx_pin

Receive pin.