EFP - Energy Friendly PMIC

Description

EFP (Energy Friendly PMIC) driver.

EFP (Energy Friendly PMIC) Driver Documentation


Introduction

The EFP is a flexible, highly efficient, multi-output power management IC. This driver provides an API to configure and control EFP ICs. The EFP is controlled by the host SoC using an I2C bus. The driver support systems with multiple EFP ICs.


Configuring the EFP driver

Your application must provide a header file named efp_instance_config.h. instance can be freely selected and could for example be EFP0 and EFP1 in a system with two EFP devices. Configuration file templates are found in the driver config folder.

Configuration options:

  • Energy mode transition mode. Host SoC can use several methods for changing EFP energy mode. Methods are either direct mode or I2C mode. I2C mode change EFP energy mode with I2C commands, direct mode use level transitions on I2C SDA and SCL lines. This provides fast energy mode transitions. Direct mode is achieved by host SoC using GPIO bit-banging or automatically by EMU hardware on SoCs with built in EFP support (check EMU section of reference manual for EFP support).
  • EFP interrupt. The EFP has an interrupt line that can be useful for a host SoC. Set this option to have the EFP driver configure a GPIO for this use.
  • EFP powers host SoC. Set if the EFP IC power the host SoC, there can only be one EFP with this option in a system.
  • I2C instance: Select which I2C peripheral to use.
  • GPIO definitions for I2C SDA/SCL and IRQ pins.

Here is an example configuration file:

#ifndef EFP_INSTANCE_CONFIG_H
#define EFP_INSTANCE_CONFIG_H

#include "sl_efp.h"

#ifdef __cplusplus
extern "C" {
#endif

// <<< Use Configuration Wizard in Context Menu >>>

// <h>EFP driver configuration

// <o EFP_INSTANCE_EM_CTRL_MODE> Selects method of controlling EFP Energy Mode (EM) transitions.
// <efp_em_transition_mode_gpio_bitbang=> GPIO driven direct mode EM transitions
// <efp_em_transition_mode_i2c=> I2C transfers control EM transitions
// <efp_em_transition_mode_emu=> Built in EMU controlled direct mode EM transitions
// <i> Default: efp_em_transition_mode_gpio_bitbang
#define EFP_INSTANCE_EM_CTRL_MODE       efp_em_transition_mode_gpio_bitbang

// <q EFP_INSTANCE_ENABLE_IRQ> Enable GPIO as interrupt input line from EFP.
// <i> Default: 1
#define EFP_INSTANCE_ENABLE_IRQ         1

// <q EFP_INSTANCE_POWERS_HOST> This EFP powers host SoC.
// <i> Default: 1
#define EFP_INSTANCE_POWERS_HOST        1

// </h> end EFP configuration

// <<< end of configuration section >>>

// <<< sl:start pin_tool >>>

// <gpio optional> EFP_INSTANCE_IRQ
// $[GPIO_EFP_INSTANCE_IRQ]
#define EFP_INSTANCE_IRQ_PORT           gpioPortC
#define EFP_INSTANCE_IRQ_PIN            9
// [GPIO_EFP_INSTANCE_IRQ]$

// <i2c signal=SDA,SCL> EFP_INSTANCE_I2C
// $[I2C_EFP_INSTANCE_I2C]
#define EFP_INSTANCE_I2C_PERIPHERAL     I2C0

#define EFP_INSTANCE_I2C_SDA_PORT       gpioPortC
#define EFP_INSTANCE_I2C_SDA_PIN        11
#define EFP_INSTANCE_I2C_SDA_LOC        16

#define EFP_INSTANCE_I2C_SCL_PORT       gpioPortC
#define EFP_INSTANCE_I2C_SCL_PIN        10
#define EFP_INSTANCE_I2C_SCL_LOC        14
// [I2C_EFP_INSTANCE_I2C]$

// <<< sl:end pin_tool >>>

#define SL_EFP_INSTANCE_INIT {                                                         \
    .config_size = 0,                                   // No initial config           \
    .config_data = NULL,                                // No config data              \
    .is_host_efp = EFP_INSTANCE_POWERS_HOST,            // This EFP powers host SOC    \
    .em_transition_mode = EFP_INSTANCE_EM_CTRL_MODE,    // EFP EM transition mode      \
    .enable_irq_pin = EFP_INSTANCE_ENABLE_IRQ,          // Init GPIO as EFP IRQ        \
    .irq_port = EFP_INSTANCE_IRQ_PORT,                  // EFP IRQ port                \
    .irq_pin = EFP_INSTANCE_IRQ_PIN,                    // EFP IRQ pin                 \
    .i2c_peripheral = EFP_INSTANCE_I2C_PERIPHERAL,      // I2C port instance           \
    .i2c_scl_port = EFP_INSTANCE_I2C_SCL_PORT,          // SCL port                    \
    .i2c_scl_pin = EFP_INSTANCE_I2C_SCL_PIN,            // SCL pin                     \
    .i2c_sda_port = EFP_INSTANCE_I2C_SDA_PORT,          // SDA port                    \
    .i2c_sda_pin = EFP_INSTANCE_I2C_SDA_PIN,            // SDA pin                     \
    .i2c_scl_port_location = EFP_INSTANCE_I2C_SCL_LOC,  // SCL port location           \
    .i2c_sda_port_location = EFP_INSTANCE_I2C_SDA_LOC,  // SDA port location           \
}

#ifdef __cplusplus
}
#endif

#endif // EFP_INSTANCE_CONFIG_H 


EFP driver example code

Basic example:

#include "efp_instance_config.h"

sl_efp_handle_data_t efp_handle_data;          // EFP instance data structure
sl_efp_handle_t      efp = &efp_handle_data;   // EFP instance pointer

int main( void )
{

  ...

  // Initialize EFP.

  // Load all configurations into an init structure, and pass it to the
  // driver initialization function.
  sl_efp_init_data_t init = SL_EFP_INSTANCE_INIT;
  sl_efp_init(efp, &init);

  // Set voltage regulator B (VOB) output voltage and peak currents.
  sl_efp_set_vob_em01_voltage(efp, 1100);
  sl_efp_set_vob_em23_voltage(efp, 1100);
  sl_efp_set_vob_em01_peak_current(efp, 108, 3300, 1100, 3300);
  sl_efp_set_vob_em23_peak_current(efp, 108, 3300, 1100, 3300);

  // Enable VOB in buck mode.
  sl_efp_set_vob_mode(efp, efp_vob_mode_buck);

  ...

} 


Code for preparing for EFP interrupts:

#include "efp_instance_config.h"

int main( void )
{

  ...

  // Prepare for EFP IRQ from Coulomb counter (CC) full flag.
  sl_efp_write_register(efp, EFP01_STATUS_GM, 0xFF);    // Unmask all G flags
  sl_efp_write_register(efp, EFP01_CC_CAL, 0x28);       // Enable CC A

  // Setup GPIO interrupt.
  NVIC_ClearPendingIRQ(GPIO_ODD_IRQn);
  NVIC_EnableIRQ(GPIO_ODD_IRQn);
  GPIO_IntConfig(init.irq_port, init.irq_pin, false, true, true);

  ...

  // Force CC full flag interrupt. This will trigger an IRQ.
  sl_efp_write_register(efp, EFP01_CMD, 0x10);          // Start CC Calibration

  ...

}

void GPIO_ODD_IRQHandler(void)
{
  // Make sure any ongoing EFP I2C transfer is completed before writing to EFP.

  // Clear EFP IRQ flag.
  sl_efp_write_register(efp, EFP01_STATUS_G, 0x40);

  // Clear GPIO interrupt flag.
  GPIO_IntClear(1 << init.irq_pin);
} 


Example with custom EFP configuration data. The sl_efp_init() function can perform EFP configuration by passing an array of EFP {address,value} pairs. This array can be generated by the EFP calculator tool in Simplicity Studio.

#include "efp_instance_config.h"

#define SL_EFP_INSTANCE_GEN_SIZE 10

// Array of 10 {address,data} pairs.
#define SL_EFP_INSTANCE_GEN {      \
    { EFP01_VOA_V,        4   },   \
    { EFP01_BB_IPK,       146 },   \
    { EFP01_BB_CTRL6,     0   },   \
    { EFP01_LDOC_BB_CTRL, 0   },   \
    { EFP01_BB_CTRL3,     181 },   \
    { EFP01_VOB_EM0_V,    13  },   \
    { EFP01_VOB_EM2_V,    13  },   \
    { EFP01_BK_IPK,       38  },   \
    { EFP01_BK_CTRL2,     80  },   \
    { EFP01_BK_CTRL1,     24  },   \
}

uint8_t efp_settings[SL_EFP_INSTANCE_GEN_SIZE][2] = SL_EFP_INSTANCE_GEN;

int main( void )
{

  ...

  // Initialize EFP, pass array of custom settings to init function.
  sl_efp_init_data_t init = SL_EFP_INSTANCE_INIT;
  init.config_size        = SL_EFP_INSTANCE_GEN_SIZE;
  init.config_data        = efp_settings[0];
  sl_efp_init(efp, &init);

  ...

} 

Data Structures

struct  sl_efp_init_data_t
 EFP driver initialization structure.
 
struct  sl_efp_handle_data_t
 An EFP driver instance handle data structure.
 

Functions

sl_status_t sl_efp_deinit (sl_efp_handle_t handle)
 Deinitialize EFP driver and underlying EFP hardware.
 
sl_status_t sl_efp_enable_direct_mode (sl_efp_handle_t handle)
 Configure I2C GPIO pins for "direct mode" EM transfer mode.
 
sl_status_t sl_efp_enter_em0 (sl_efp_handle_t handle)
 Set EFP in EM0 energy mode.
 
sl_status_t sl_efp_enter_em2 (sl_efp_handle_t handle)
 Set EFP in EM2 energy mode.
 
sl_status_t sl_efp_get_vdd_avg (sl_efp_handle_t handle, uint16_t *voltage_mv)
 Measure average VDD.
 
sl_status_t sl_efp_get_vdd_max (sl_efp_handle_t handle, uint16_t *voltage_mv)
 Measure maximum VDD.
 
sl_status_t sl_efp_get_vdd_min (sl_efp_handle_t handle, uint16_t *voltage_mv)
 Measure minimum VDD.
 
sl_status_t sl_efp_init (sl_efp_handle_t handle, const sl_efp_init_data_t *init)
 Initialize EFP driver and configure underlying EFP hardware.
 
sl_status_t sl_efp_read_otp (sl_efp_handle_t handle, uint8_t addr, uint8_t *data)
 Read EFP OTP register.
 
sl_status_t sl_efp_read_register (sl_efp_handle_t handle, uint8_t addr, uint8_t *data)
 Read EFP control register.
 
sl_status_t sl_efp_read_register_field (sl_efp_handle_t handle, uint8_t addr, uint8_t *data, uint8_t mask, uint8_t pos)
 Read EFP control register field.
 
sl_status_t sl_efp_reset (sl_efp_handle_t handle)
 Reset EFP.
 
sl_status_t sl_efp_reset_to_default (sl_efp_handle_t handle)
 Reprogram all EFP registers with default values.
 
sl_status_t sl_efp_set_em_transition_mode (sl_efp_handle_t handle, sl_efp_em_transition_mode_t mode)
 Set EM transition mode.
 
sl_status_t sl_efp_set_voa_em01_peak_current (sl_efp_handle_t handle, unsigned int current_ma, unsigned int vddb_mv, unsigned int voa_mv, unsigned int inductor_nh)
 Set regulator VOA EM01 peak output current.
 
sl_status_t sl_efp_set_voa_em23_peak_current (sl_efp_handle_t handle, unsigned int current_ma, unsigned int vddb_mv, unsigned int voa_mv, unsigned int inductor_nh)
 Set regulator VOA EM23 peak output current.
 
sl_status_t sl_efp_set_voa_mode (sl_efp_handle_t handle, sl_efp_voa_mode_t mode)
 Set regulator VOA mode.
 
sl_status_t sl_efp_set_voa_sw_mode (sl_efp_handle_t handle, sl_efp_voa_sw_mode_t mode)
 Set VOA SW (switched output) mode.
 
sl_status_t sl_efp_set_voa_voltage (sl_efp_handle_t handle, unsigned int voltage_mv)
 Set regulator VOA output voltage.
 
sl_status_t sl_efp_set_vob_em01_peak_current (sl_efp_handle_t handle, unsigned int current_ma, unsigned int vddb_mv, unsigned int vob_mv, unsigned int inductor_nh)
 Set regulator VOB EM01 peak output current.
 
sl_status_t sl_efp_set_vob_em01_voltage (sl_efp_handle_t handle, unsigned int voltage_mv)
 Set regulator VOB EM01 output voltage.
 
sl_status_t sl_efp_set_vob_em23_peak_current (sl_efp_handle_t handle, unsigned int current_ma, unsigned int vddb_mv, unsigned int vob_mv, unsigned int inductor_nh)
 Set regulator VOB EM23 peak output current.
 
sl_status_t sl_efp_set_vob_em23_voltage (sl_efp_handle_t handle, unsigned int voltage_mv)
 Set regulator VOB EM23 output voltage.
 
sl_status_t sl_efp_set_vob_mode (sl_efp_handle_t handle, sl_efp_vob_mode_t mode)
 Set regulator VOB mode.
 
sl_status_t sl_efp_set_voc_voltage (sl_efp_handle_t handle, unsigned int voltage_mv)
 Set regulator VOC output voltage.
 
sl_status_t sl_efp_emu_ldo_enable (sl_efp_handle_t handle, bool enable)
 Turn the internal EMU LDO regulator that supplies DECOUPLE pin on or off.
 
sl_status_t sl_efp_write_register (sl_efp_handle_t handle, uint8_t addr, uint8_t data)
 Write EFP control register.
 
sl_status_t sl_efp_write_register_field (sl_efp_handle_t handle, uint8_t addr, uint8_t data, uint8_t mask, uint8_t pos)
 Write EFP control register field.
 

Typedefs

typedef sl_efp_handle_data_tsl_efp_handle_t
 An EFP driver instance handle.
 

Enumerations

enum  sl_efp_em_transition_mode_t {
  efp_em_transition_mode_gpio_bitbang,
  efp_em_transition_mode_i2c,
  efp_em_transition_mode_emu
}
 Method for controlling EFP Energy Mode (EM) transitions.
 
enum  sl_efp_voa_mode_t {
  efp_voa_mode_disabled = _EFP01_BB_CTRL3_BB_MODE_DISABLED,
  efp_voa_mode_wired_buck = _EFP01_BB_CTRL3_BB_MODE_WIREDBUCK,
  efp_voa_mode_wired_boost = _EFP01_BB_CTRL3_BB_MODE_WIREDBOOST,
  efp_voa_mode_wired_buck_ldo = _EFP01_BB_CTRL3_BB_MODE_WIREDBUCKLDO,
  efp_voa_mode_buck_boost_autonomous = _EFP01_BB_CTRL3_BB_MODE_AUTONOMOUS,
  efp_voa_mode_buck_boost_forced_buck = _EFP01_BB_CTRL3_BB_MODE_FORCEBUCK,
  efp_voa_mode_buck_boost_forced_ntm = _EFP01_BB_CTRL3_BB_MODE_FORCENTM,
  efp_voa_mode_buck_boost_forced_boost = _EFP01_BB_CTRL3_BB_MODE_FORCEBOOST
}
 VOA regulator modes.
 
enum  sl_efp_voa_sw_mode_t {
  efp_voa_sw_mode_off = _EFP01_BIAS_SW_VOA_SW_CON_OFF,
  efp_voa_sw_mode_on = _EFP01_BIAS_SW_VOA_SW_CON_ON,
  efp_voa_sw_mode_on_in_em0 = _EFP01_BIAS_SW_VOA_SW_CON_ONINEM0,
  efp_voa_sw_mode_on_in_em02 = _EFP01_BIAS_SW_VOA_SW_CON_ONINEM02
}
 VOA SW (switched output) modes.
 
enum  sl_efp_vob_mode_t {
  efp_vob_mode_disabled = _EFP01_BK_CTRL1_BK_MODE_DISABLED,
  efp_vob_mode_buck = _EFP01_BK_CTRL1_BK_MODE_BUCKONLY,
  efp_vob_mode_ldo = _EFP01_BK_CTRL1_BK_MODE_LDOONLY,
  efp_vob_mode_buck_ldo = _EFP01_BK_CTRL1_BK_MODE_BUCKLDO
}
 VOB regulator modes.
 

Function Documentation

◆ sl_efp_deinit()

sl_status_t sl_efp_deinit ( sl_efp_handle_t  handle)

Deinitialize EFP driver and underlying EFP hardware.

Parameters
[in]handleEFP instance handle.
Returns
SL_STATUS_OK.

◆ sl_efp_enable_direct_mode()

sl_status_t sl_efp_enable_direct_mode ( sl_efp_handle_t  handle)

Configure I2C GPIO pins for "direct mode" EM transfer mode.

Parameters
[in]handleEFP instance handle.
Note
This must be the last EFP driver function called prior to entering EM2/3 via EMU_EnterEMx() calls. Any EFP API call that involves an I2C transfer will leave the I2C GPIO pins in I2C mode.
Returns
SL_STATUS_OK on success. SL_STATUS_INVALID_MODE if current EM transfer mode is I2C. SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_enter_em0()

sl_status_t sl_efp_enter_em0 ( sl_efp_handle_t  handle)

Set EFP in EM0 energy mode.

Parameters
[in]handleEFP instance handle.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_enter_em2()

sl_status_t sl_efp_enter_em2 ( sl_efp_handle_t  handle)

Set EFP in EM2 energy mode.

Parameters
[in]handleEFP instance handle.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_get_vdd_avg()

sl_status_t sl_efp_get_vdd_avg ( sl_efp_handle_t  handle,
uint16_t *  voltage_mv 
)

Measure average VDD.

Note
This function measures VDDA or VDDB depending of the voltage on the VDDA pin after power on. If VDDA is powered this function returns a VDDA reading, otherwise a VDDB reading is returned.
Parameters
[in]handleEFP instance handle.
[out]voltage_mvAverage VDD voltage expressed in millivolts.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_get_vdd_max()

sl_status_t sl_efp_get_vdd_max ( sl_efp_handle_t  handle,
uint16_t *  voltage_mv 
)

Measure maximum VDD.

Note
This function measures VDDA or VDDB depending of the voltage on the VDDA pin after power on. If VDDA is powered this function returns a VDDA reading, otherwise a VDDB reading is returned.
Parameters
[in]handleEFP instance handle.
[out]voltage_mvMaximum VDD voltage expressed in millivolts.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_get_vdd_min()

sl_status_t sl_efp_get_vdd_min ( sl_efp_handle_t  handle,
uint16_t *  voltage_mv 
)

Measure minimum VDD.

Note
This function measures VDDA or VDDB depending of the voltage on the VDDA pin after power on. If VDDA is powered this function returns a VDDA reading, otherwise a VDDB reading is returned.
Parameters
[in]handleEFP instance handle.
[out]voltage_mvMinimum VDD voltage expressed in miilivolts.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_init()

sl_status_t sl_efp_init ( sl_efp_handle_t  handle,
const sl_efp_init_data_t init 
)

Initialize EFP driver and configure underlying EFP hardware.

Note
This function must not be called from interrupt context.
Parameters
[in]handleEFP instance handle.
[in]initInitialization data structure.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors, or SL_STATUS_FAIL on illegal initialization.

◆ sl_efp_read_otp()

sl_status_t sl_efp_read_otp ( sl_efp_handle_t  handle,
uint8_t  addr,
uint8_t *  data 
)

Read EFP OTP register.

Parameters
[in]handleEFP instance handle.
[in]addrRegister address.
[out]dataThe value read from the OTP register.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_read_register()

sl_status_t sl_efp_read_register ( sl_efp_handle_t  handle,
uint8_t  addr,
uint8_t *  data 
)

Read EFP control register.

Parameters
[in]handleEFP instance handle.
[in]addrRegister address.
[out]dataThe value read from the register.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_read_register_field()

sl_status_t sl_efp_read_register_field ( sl_efp_handle_t  handle,
uint8_t  addr,
uint8_t *  data,
uint8_t  mask,
uint8_t  pos 
)

Read EFP control register field.

Parameters
[in]handleEFP instance handle.
[in]addrRegister address.
[out]dataThe value read from the register field.
[in]maskBit mask corresponding to target bit field.
[in]posBit number of least significant bit of target bit field.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_reset()

sl_status_t sl_efp_reset ( sl_efp_handle_t  handle)

Reset EFP.

Perform a full reset of the EFP, this is eqvivalent to a power on reset.

Parameters
[in]handleEFP instance handle.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_reset_to_default()

sl_status_t sl_efp_reset_to_default ( sl_efp_handle_t  handle)

Reprogram all EFP registers with default values.

Parameters
[in]handleEFP instance handle.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_em_transition_mode()

sl_status_t sl_efp_set_em_transition_mode ( sl_efp_handle_t  handle,
sl_efp_em_transition_mode_t  mode 
)

Set EM transition mode.

Parameters
[in]handleEFP instance handle.
[in]modeNew EFP Energy Mode (EM) transition mode. See sl_efp_em_transition_mode_t for valid modes.
Returns
SL_STATUS_OK.

◆ sl_efp_set_voa_em01_peak_current()

sl_status_t sl_efp_set_voa_em01_peak_current ( sl_efp_handle_t  handle,
unsigned int  current_ma,
unsigned int  vddb_mv,
unsigned int  voa_mv,
unsigned int  inductor_nh 
)

Set regulator VOA EM01 peak output current.

Parameters
[in]handleEFP instance handle.
[in]current_maTarget peak current expressed in milliamperes.
[in]vddb_mvVDDB expressed in millivolt.
[in]voa_mvVOA expressed in millivolt.
[in]inductor_nhInductor size expressed in nanohenry.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_voa_em23_peak_current()

sl_status_t sl_efp_set_voa_em23_peak_current ( sl_efp_handle_t  handle,
unsigned int  current_ma,
unsigned int  vddb_mv,
unsigned int  voa_mv,
unsigned int  inductor_nh 
)

Set regulator VOA EM23 peak output current.

Parameters
[in]handleEFP instance handle.
[in]current_maTarget peak current expressed in milliamperes.
[in]vddb_mvVDDB expressed in millivolt.
[in]voa_mvVOA expressed in millivolt.
[in]inductor_nhInductor size expressed in nanohenry.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_voa_mode()

sl_status_t sl_efp_set_voa_mode ( sl_efp_handle_t  handle,
sl_efp_voa_mode_t  mode 
)

Set regulator VOA mode.

Parameters
[in]handleEFP instance handle.
[in]modeRegulator mode.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_voa_sw_mode()

sl_status_t sl_efp_set_voa_sw_mode ( sl_efp_handle_t  handle,
sl_efp_voa_sw_mode_t  mode 
)

Set VOA SW (switched output) mode.

Parameters
[in]handleEFP instance handle.
[in]modeVOA SW mode.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_voa_voltage()

sl_status_t sl_efp_set_voa_voltage ( sl_efp_handle_t  handle,
unsigned int  voltage_mv 
)

Set regulator VOA output voltage.

Parameters
[in]handleEFP instance handle.
[in]voltage_mvVoltage in millivolt.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_vob_em01_peak_current()

sl_status_t sl_efp_set_vob_em01_peak_current ( sl_efp_handle_t  handle,
unsigned int  current_ma,
unsigned int  vddb_mv,
unsigned int  vob_mv,
unsigned int  inductor_nh 
)

Set regulator VOB EM01 peak output current.

Parameters
[in]handleEFP instance handle.
[in]current_maTarget peak current expressed in milliamperes.
[in]vddb_mvVDDB expressed in millivolt.
[in]vob_mvVOB expressed in millivolt.
[in]inductor_nhInductor size expressed in nanohenry.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_vob_em01_voltage()

sl_status_t sl_efp_set_vob_em01_voltage ( sl_efp_handle_t  handle,
unsigned int  voltage_mv 
)

Set regulator VOB EM01 output voltage.

Parameters
[in]handleEFP instance handle.
[in]voltage_mvVoltage in millivolt.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_vob_em23_peak_current()

sl_status_t sl_efp_set_vob_em23_peak_current ( sl_efp_handle_t  handle,
unsigned int  current_ma,
unsigned int  vddb_mv,
unsigned int  vob_mv,
unsigned int  inductor_nh 
)

Set regulator VOB EM23 peak output current.

Parameters
[in]handleEFP instance handle.
[in]current_maTarget peak current expressed in milliamperes.
[in]vddb_mvVDDB expressed in millivolt.
[in]vob_mvVOB expressed in millivolt.
[in]inductor_nhInductor size expressed in nanohenry.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_vob_em23_voltage()

sl_status_t sl_efp_set_vob_em23_voltage ( sl_efp_handle_t  handle,
unsigned int  voltage_mv 
)

Set regulator VOB EM23 output voltage.

Parameters
[in]handleEFP instance handle.
[in]voltage_mvVoltage in millivolt.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_vob_mode()

sl_status_t sl_efp_set_vob_mode ( sl_efp_handle_t  handle,
sl_efp_vob_mode_t  mode 
)

Set regulator VOB mode.

Parameters
[in]handleEFP instance handle.
[in]modeRegulator mode.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_set_voc_voltage()

sl_status_t sl_efp_set_voc_voltage ( sl_efp_handle_t  handle,
unsigned int  voltage_mv 
)

Set regulator VOC output voltage.

Parameters
[in]handleEFP instance handle.
[in]voltage_mvVoltage in millivolt.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_emu_ldo_enable()

sl_status_t sl_efp_emu_ldo_enable ( sl_efp_handle_t  handle,
bool  enable 
)

Turn the internal EMU LDO regulator that supplies DECOUPLE pin on or off.

Note
Make sure that an external source supply the DECOUPLE pin turning the LDO off.
Parameters
[in]handleEFP instance handle.
[in]enableTrue to turn LDO on, false to turn off.
Returns
SL_STATUS_OK or SL_STATUS_NOT_SUPPORTED, or SL_STATUS_FAIL if not a host EFP instance.

◆ sl_efp_write_register()

sl_status_t sl_efp_write_register ( sl_efp_handle_t  handle,
uint8_t  addr,
uint8_t  data 
)

Write EFP control register.

Parameters
[in]handleEFP instance handle.
[in]addrRegister address.
[in]dataThe value to write to the register.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

◆ sl_efp_write_register_field()

sl_status_t sl_efp_write_register_field ( sl_efp_handle_t  handle,
uint8_t  addr,
uint8_t  data,
uint8_t  mask,
uint8_t  pos 
)

Write EFP control register field.

Note
This function performs a read-modify-write of a EFP register.
Parameters
[in]handleEFP instance handle.
[in]addrRegister address.
[in]dataThe value to write to the register field.
[in]maskBit mask corresponding to target bit field.
[in]posBit number of least significant bit of target bit field.
Returns
SL_STATUS_OK or SL_STATUS_IO on I2C transfer errors.

Typedef Documentation

◆ sl_efp_handle_t

An EFP driver instance handle.

Enumeration Type Documentation

◆ sl_efp_em_transition_mode_t

Method for controlling EFP Energy Mode (EM) transitions.

Enumerator
efp_em_transition_mode_gpio_bitbang 

GPIO driven "direct mode" EM transitions.

efp_em_transition_mode_i2c 

I2C transfers control EM transitions.

efp_em_transition_mode_emu 

Built in EMU controlled "direct mode" EM transitions.

◆ sl_efp_voa_mode_t

VOA regulator modes.

Enumerator
efp_voa_mode_disabled 

VOA disabled.

efp_voa_mode_wired_buck 

VOA wired buck.

efp_voa_mode_wired_boost 

VOA wired boost.

efp_voa_mode_wired_buck_ldo 

VOA wired buck and LDO.

efp_voa_mode_buck_boost_autonomous 

VOA buck boost autonomous.

efp_voa_mode_buck_boost_forced_buck 

VOA buck boost forced buck.

efp_voa_mode_buck_boost_forced_ntm 

VOA buck boost forced NTM.

efp_voa_mode_buck_boost_forced_boost 

VOA buck boost forced boost.

◆ sl_efp_voa_sw_mode_t

VOA SW (switched output) modes.

Enumerator
efp_voa_sw_mode_off 

VOA SW off.

efp_voa_sw_mode_on 

VOA SW on in EM0, EM2 and EM4.

efp_voa_sw_mode_on_in_em0 

VOA SW on in EM0 only.

efp_voa_sw_mode_on_in_em02 

VOA SW on in EM0 and EM2.

◆ sl_efp_vob_mode_t

VOB regulator modes.

Enumerator
efp_vob_mode_disabled 

VOB disabled.

efp_vob_mode_buck 

VOB buck only.

efp_vob_mode_ldo 

VOB LDO only.

efp_vob_mode_buck_ldo 

VOB buck and LDO.