HalCrashIcsrType Union Reference

Data Fields

struct {
   uint32_t   VECTACTIVE: 9
 
   uint32_t   __pad0__: 2
 
   uint32_t   RETTOBASE: 1
 
   uint32_t   VECTPENDING: 9
 
   uint32_t   __pad1__: 1
 
   uint32_t   ISRPENDING: 1
 
   uint32_t   ISRPREEMPT: 1
 
   uint32_t   __pad2__: 1
 
   uint32_t   PENDSTCLR: 1
 
   uint32_t   PENDSTSET: 1
 
   uint32_t   PENDSVCLR: 1
 
   uint32_t   PENDSVSET: 1
 
   uint32_t   __pad3__: 2
 
   uint32_t   NMIPENDSET: 1
 
bits
 
uint32_t word