// Gecko Platform//Version 4.4.1 //Services ... a date format sl_sleeptimer_date_t. API : sl_status_t sl_sleeptimer_get_datetime(sl_ ... SL_SLEEPTIMER_NO_HIGH_PRECISION_HF_CLOCKS_REQUIRED_FLAG
The SE Manager API is multi-thread safe, but does not support preemption. ... Configure sl_se_command_context_t with sl_se_set_yield to yield the CPU core when the SE Manager is waiting for ...
Configuration Options The API Flow Control Support ... the UARTDRV_InitLeuart() function for LEUART peripherals. The API This section contains brief descriptions of the functions in the API.
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/3.2/emlib/api/efm32tg/driver/api/structsl-pwm-config