sl_button_t Struct Reference

A BUTTON instance.

#include <sl_button.h>

Data Fields

void * context
 The context for this BUTTON instance.
 
sl_status_t(* init )(void *context)
 Member function to initialize BUTTON instance.
 
void(* poll )(void *context)
 Member function to poll BUTTON.
 
void(* enable )(void *context)
 Member function to enable BUTTON.
 
void(* disable )(void *context)
 Member function to disable BUTTON.
 
sl_button_state_t(* get_state )(void *context)
 Member function to retrieve BUTTON state.
 

A BUTTON instance.

Field Documentation

◆ context

void* sl_button_t::context

The context for this BUTTON instance.

◆ init

sl_status_t(* sl_button_t::init) (void *context)

Member function to initialize BUTTON instance.

◆ poll

void(* sl_button_t::poll) (void *context)

Member function to poll BUTTON.

◆ enable

void(* sl_button_t::enable) (void *context)

Member function to enable BUTTON.

◆ disable

void(* sl_button_t::disable) (void *context)

Member function to disable BUTTON.

◆ get_state

sl_button_state_t(* sl_button_t::get_state) (void *context)

Member function to retrieve BUTTON state.