A struct containing all of the function pointers needed to implement secure element Authenticated Encryption with Additional Data operations.

#include <crypto_se_driver.h>

Public Member Functions

psa_drv_se_aead_encrypt_t MBEDTLS_PRIVATE (p_encrypt)
 Function that performs the AEAD encrypt operation.
 
psa_drv_se_aead_decrypt_t MBEDTLS_PRIVATE (p_decrypt)
 Function that performs the AEAD decrypt operation.
 

A struct containing all of the function pointers needed to implement secure element Authenticated Encryption with Additional Data operations.

PSA Crypto API implementations should populate instances of the table as appropriate upon startup.

If one of the functions is not implemented, it should be set to NULL.

Member Function Documentation

◆ MBEDTLS_PRIVATE() [1/2]

psa_drv_se_aead_encrypt_t psa_drv_se_aead_t::MBEDTLS_PRIVATE ( p_encrypt  )

Function that performs the AEAD encrypt operation.

◆ MBEDTLS_PRIVATE() [2/2]

psa_drv_se_aead_decrypt_t psa_drv_se_aead_t::MBEDTLS_PRIVATE ( p_decrypt  )

Function that performs the AEAD decrypt operation.