sl_cpc_endpoint_debug_counters_t Struct Reference

Struct representing CPC Core debug stats.

#include <sl_cpc.h>

Data Fields

uint32_t rxd_packet
 
uint32_t rxd_data_frame
 
uint32_t rxd_data_frame_queued
 
uint32_t rxd_data_frame_dropped
 
uint32_t rxd_supervisory_frame
 
uint32_t rxd_supervisory_frame_processed
 
uint32_t rxd_supervisory_frame_dropped
 
uint32_t rxd_unnumbered_frame
 
uint32_t rxd_unnumbered_frame_processed
 
uint32_t rxd_unnumbered_frame_dropped
 
uint32_t rxd_duplicate_data_frame
 
uint32_t rxd_ack
 
uint32_t rxd_reject_destination_unreachable
 
uint32_t rxd_reject_seq_mismatch
 
uint32_t rxd_reject_checksum_mismatch
 
uint32_t rxd_reject_security_issue
 
uint32_t rxd_reject_out_of_memory
 
uint32_t rxd_reject_fault
 
uint32_t txd_data_frame
 
uint32_t txd_ack
 
uint32_t txd_reject_destination_unreachable
 
uint32_t txd_reject_seq_mismatch
 
uint32_t txd_reject_checksum_mismatch
 
uint32_t txd_reject_security_issue
 
uint32_t txd_reject_out_of_memory
 
uint32_t txd_reject_fault
 
uint32_t retxd_data_frame
 
uint32_t frame_transmit_submitted
 
uint32_t frame_transmit_completed
 
uint32_t data_frame_transmit_completed
 
uint32_t supervisory_frame_transmit_completed
 

Struct representing CPC Core debug stats.