sl_cpc_system_cmd_header_t Struct Reference
Data Fields | |
sl_cpc_system_cmd_id_t | command_id |
Identifier of the command. | |
uint8_t | seq |
Command sequence number. | |
uint16_t | length |
Length of the payload in bytes. | |
Field Documentation
◆ command_id
sl_cpc_system_cmd_id_t sl_cpc_system_cmd_header_t::command_id |
Identifier of the command.
◆ seq
uint8_t sl_cpc_system_cmd_header_t::seq |
Command sequence number.
◆ length
uint16_t sl_cpc_system_cmd_header_t::length |
Length of the payload in bytes.