Cpc_system_common
Description
CPC System Endpoint Common.
Data Structures | |
struct | sl_cpc_system_cmd_header_t |
struct | sl_cpc_system_cmd_t |
struct | sl_cpc_system_property_cmd_t |
Macros | |
#define | EP_ID_TO_PROPERTY_ID(ep_id) ((sl_cpc_property_id_t)((0x00001000 | ((ep_id) & 0x000000FF)))) |
Helper macros to convert an enpoint id (uint8_t) to a PROP_ENDPOINT_STATE_x enum value. | |
#define | PROPERTY_ID_TO_EP_ID(property_id) ((uint8_t)(property_id) & 0x000000FF) |
Helper macros to convert a PROP_ENDPOINT_STATE_x enum value to an endpoint id (uint8_t) | |
#define | AGGREGATED_STATE_LOW(agg) ((sl_cpc_endpoint_state_t)(agg & 0x0F)) |
Helper macros to extract the two aggregated endpoint states encoded in one single byte. | |
#define | AGGREGATED_STATE_HIGH(agg) ((sl_cpc_endpoint_state_t)(agg >> 4)) |
#define | GET_ENDPOINT_STATE_FROM_STATES(payload, ep_id) |
#define | CPC_CAPABILITIES_SECURITY_ENDPOINT_MASK (1 << 0) |
Capabilities mask. | |
#define | CPC_CAPABILITIES_PACKED_ENDPOINT_MASK (1 << 1) |
#define | CPC_CAPABILITIES_GPIO_ENDPOINT_MASK (1 << 2) |
#define | PAYLOAD_LENGTH_MAX 16 |
System endpoint command type. | |
Enumerations | |
enum | sl_cpc_property_id_t { PROP_LAST_STATUS = 0x00, PROP_PROTOCOL_VERSION = 0x01, PROP_CAPABILITIES = 0x02, PROP_SECONDARY_VERSION = 0x03, PROP_RX_CAPABILITY = 0x20, PROP_BOOTLOADER_INFO = 0x200, PROP_BOOTLOADER_REBOOT_MODE = 0x202, PROP_SECURITY_STATE = 0x301, PROP_CORE_DEBUG_COUNTERS = 0x400, PROP_ENDPOINT_STATE_0 = 0x1000, PROP_ENDPOINT_STATE_1 = 0x1001, PROP_ENDPOINT_STATE_2 = 0x1002, PROP_ENDPOINT_STATE_3 = 0x1003, PROP_ENDPOINT_STATE_4 = 0x1004, PROP_ENDPOINT_STATE_5 = 0x1005, PROP_ENDPOINT_STATE_6 = 0x1006, PROP_ENDPOINT_STATE_7 = 0x1007, PROP_ENDPOINT_STATE_8 = 0x1008, PROP_ENDPOINT_STATE_9 = 0x1009, PROP_ENDPOINT_STATE_10 = 0x100a, PROP_ENDPOINT_STATE_11 = 0x100b, PROP_ENDPOINT_STATE_12 = 0x100c, PROP_ENDPOINT_STATE_13 = 0x100d, PROP_ENDPOINT_STATE_14 = 0x100e, PROP_ENDPOINT_STATE_15 = 0x100f, PROP_ENDPOINT_STATE_16 = 0x1010, PROP_ENDPOINT_STATE_17 = 0x1011, PROP_ENDPOINT_STATE_18 = 0x1012, PROP_ENDPOINT_STATE_19 = 0x1013, PROP_ENDPOINT_STATE_20 = 0x1014, PROP_ENDPOINT_STATE_21 = 0x1015, PROP_ENDPOINT_STATE_22 = 0x1016, PROP_ENDPOINT_STATE_23 = 0x1017, PROP_ENDPOINT_STATE_24 = 0x1018, PROP_ENDPOINT_STATE_25 = 0x1019, PROP_ENDPOINT_STATE_26 = 0x101a, PROP_ENDPOINT_STATE_27 = 0x101b, PROP_ENDPOINT_STATE_28 = 0x101c, PROP_ENDPOINT_STATE_29 = 0x101d, PROP_ENDPOINT_STATE_30 = 0x101e, PROP_ENDPOINT_STATE_31 = 0x101f, PROP_ENDPOINT_STATE_32 = 0x1020, PROP_ENDPOINT_STATE_33 = 0x1021, PROP_ENDPOINT_STATE_34 = 0x1022, PROP_ENDPOINT_STATE_35 = 0x1023, PROP_ENDPOINT_STATE_36 = 0x1024, PROP_ENDPOINT_STATE_37 = 0x1025, PROP_ENDPOINT_STATE_38 = 0x1026, PROP_ENDPOINT_STATE_39 = 0x1027, PROP_ENDPOINT_STATE_40 = 0x1028, PROP_ENDPOINT_STATE_41 = 0x1029, PROP_ENDPOINT_STATE_42 = 0x102a, PROP_ENDPOINT_STATE_43 = 0x102b, PROP_ENDPOINT_STATE_44 = 0x102c, PROP_ENDPOINT_STATE_45 = 0x102d, PROP_ENDPOINT_STATE_46 = 0x102e, PROP_ENDPOINT_STATE_47 = 0x102f, PROP_ENDPOINT_STATE_48 = 0x1030, PROP_ENDPOINT_STATE_49 = 0x1031, PROP_ENDPOINT_STATE_50 = 0x1032, PROP_ENDPOINT_STATE_51 = 0x1033, PROP_ENDPOINT_STATE_52 = 0x1034, PROP_ENDPOINT_STATE_53 = 0x1035, PROP_ENDPOINT_STATE_54 = 0x1036, PROP_ENDPOINT_STATE_55 = 0x1037, PROP_ENDPOINT_STATE_56 = 0x1038, PROP_ENDPOINT_STATE_57 = 0x1039, PROP_ENDPOINT_STATE_58 = 0x103a, PROP_ENDPOINT_STATE_59 = 0x103b, PROP_ENDPOINT_STATE_60 = 0x103c, PROP_ENDPOINT_STATE_61 = 0x103d, PROP_ENDPOINT_STATE_62 = 0x103e, PROP_ENDPOINT_STATE_63 = 0x103f, PROP_ENDPOINT_STATE_64 = 0x1040, PROP_ENDPOINT_STATE_65 = 0x1041, PROP_ENDPOINT_STATE_66 = 0x1042, PROP_ENDPOINT_STATE_67 = 0x1043, PROP_ENDPOINT_STATE_68 = 0x1044, PROP_ENDPOINT_STATE_69 = 0x1045, PROP_ENDPOINT_STATE_70 = 0x1046, PROP_ENDPOINT_STATE_71 = 0x1047, PROP_ENDPOINT_STATE_72 = 0x1048, PROP_ENDPOINT_STATE_73 = 0x1049, PROP_ENDPOINT_STATE_74 = 0x104a, PROP_ENDPOINT_STATE_75 = 0x104b, PROP_ENDPOINT_STATE_76 = 0x104c, PROP_ENDPOINT_STATE_77 = 0x104d, PROP_ENDPOINT_STATE_78 = 0x104e, PROP_ENDPOINT_STATE_79 = 0x104f, PROP_ENDPOINT_STATE_80 = 0x1050, PROP_ENDPOINT_STATE_81 = 0x1051, PROP_ENDPOINT_STATE_82 = 0x1052, PROP_ENDPOINT_STATE_83 = 0x1053, PROP_ENDPOINT_STATE_84 = 0x1054, PROP_ENDPOINT_STATE_85 = 0x1055, PROP_ENDPOINT_STATE_86 = 0x1056, PROP_ENDPOINT_STATE_87 = 0x1057, PROP_ENDPOINT_STATE_88 = 0x1058, PROP_ENDPOINT_STATE_89 = 0x1059, PROP_ENDPOINT_STATE_90 = 0x105a, PROP_ENDPOINT_STATE_91 = 0x105b, PROP_ENDPOINT_STATE_92 = 0x105c, PROP_ENDPOINT_STATE_93 = 0x105d, PROP_ENDPOINT_STATE_94 = 0x105e, PROP_ENDPOINT_STATE_95 = 0x105f, PROP_ENDPOINT_STATE_96 = 0x1060, PROP_ENDPOINT_STATE_97 = 0x1061, PROP_ENDPOINT_STATE_98 = 0x1062, PROP_ENDPOINT_STATE_99 = 0x1063, PROP_ENDPOINT_STATE_100 = 0x1064, PROP_ENDPOINT_STATE_101 = 0x1065, PROP_ENDPOINT_STATE_102 = 0x1066, PROP_ENDPOINT_STATE_103 = 0x1067, PROP_ENDPOINT_STATE_104 = 0x1068, PROP_ENDPOINT_STATE_105 = 0x1069, PROP_ENDPOINT_STATE_106 = 0x106a, PROP_ENDPOINT_STATE_107 = 0x106b, PROP_ENDPOINT_STATE_108 = 0x106c, PROP_ENDPOINT_STATE_109 = 0x106d, PROP_ENDPOINT_STATE_110 = 0x106e, PROP_ENDPOINT_STATE_111 = 0x106f, PROP_ENDPOINT_STATE_112 = 0x1070, PROP_ENDPOINT_STATE_113 = 0x1071, PROP_ENDPOINT_STATE_114 = 0x1072, PROP_ENDPOINT_STATE_115 = 0x1073, PROP_ENDPOINT_STATE_116 = 0x1074, PROP_ENDPOINT_STATE_117 = 0x1075, PROP_ENDPOINT_STATE_118 = 0x1076, PROP_ENDPOINT_STATE_119 = 0x1077, PROP_ENDPOINT_STATE_120 = 0x1078, PROP_ENDPOINT_STATE_121 = 0x1079, PROP_ENDPOINT_STATE_122 = 0x107a, PROP_ENDPOINT_STATE_123 = 0x107b, PROP_ENDPOINT_STATE_124 = 0x107c, PROP_ENDPOINT_STATE_125 = 0x107d, PROP_ENDPOINT_STATE_126 = 0x107e, PROP_ENDPOINT_STATE_127 = 0x107f, PROP_ENDPOINT_STATE_128 = 0x1080, PROP_ENDPOINT_STATE_129 = 0x1081, PROP_ENDPOINT_STATE_130 = 0x1082, PROP_ENDPOINT_STATE_131 = 0x1083, PROP_ENDPOINT_STATE_132 = 0x1084, PROP_ENDPOINT_STATE_133 = 0x1085, PROP_ENDPOINT_STATE_134 = 0x1086, PROP_ENDPOINT_STATE_135 = 0x1087, PROP_ENDPOINT_STATE_136 = 0x1088, PROP_ENDPOINT_STATE_137 = 0x1089, PROP_ENDPOINT_STATE_138 = 0x108a, PROP_ENDPOINT_STATE_139 = 0x108b, PROP_ENDPOINT_STATE_140 = 0x108c, PROP_ENDPOINT_STATE_141 = 0x108d, PROP_ENDPOINT_STATE_142 = 0x108e, PROP_ENDPOINT_STATE_143 = 0x108f, PROP_ENDPOINT_STATE_144 = 0x1090, PROP_ENDPOINT_STATE_145 = 0x1091, PROP_ENDPOINT_STATE_146 = 0x1092, PROP_ENDPOINT_STATE_147 = 0x1093, PROP_ENDPOINT_STATE_148 = 0x1094, PROP_ENDPOINT_STATE_149 = 0x1095, PROP_ENDPOINT_STATE_150 = 0x1096, PROP_ENDPOINT_STATE_151 = 0x1097, PROP_ENDPOINT_STATE_152 = 0x1098, PROP_ENDPOINT_STATE_153 = 0x1099, PROP_ENDPOINT_STATE_154 = 0x109a, PROP_ENDPOINT_STATE_155 = 0x109b, PROP_ENDPOINT_STATE_156 = 0x109c, PROP_ENDPOINT_STATE_157 = 0x109d, PROP_ENDPOINT_STATE_158 = 0x109e, PROP_ENDPOINT_STATE_159 = 0x109f, PROP_ENDPOINT_STATE_160 = 0x10a0, PROP_ENDPOINT_STATE_161 = 0x10a1, PROP_ENDPOINT_STATE_162 = 0x10a2, PROP_ENDPOINT_STATE_163 = 0x10a3, PROP_ENDPOINT_STATE_164 = 0x10a4, PROP_ENDPOINT_STATE_165 = 0x10a5, PROP_ENDPOINT_STATE_166 = 0x10a6, PROP_ENDPOINT_STATE_167 = 0x10a7, PROP_ENDPOINT_STATE_168 = 0x10a8, PROP_ENDPOINT_STATE_169 = 0x10a9, PROP_ENDPOINT_STATE_170 = 0x10aa, PROP_ENDPOINT_STATE_171 = 0x10ab, PROP_ENDPOINT_STATE_172 = 0x10ac, PROP_ENDPOINT_STATE_173 = 0x10ad, PROP_ENDPOINT_STATE_174 = 0x10ae, PROP_ENDPOINT_STATE_175 = 0x10af, PROP_ENDPOINT_STATE_176 = 0x10b0, PROP_ENDPOINT_STATE_177 = 0x10b1, PROP_ENDPOINT_STATE_178 = 0x10b2, PROP_ENDPOINT_STATE_179 = 0x10b3, PROP_ENDPOINT_STATE_180 = 0x10b4, PROP_ENDPOINT_STATE_181 = 0x10b5, PROP_ENDPOINT_STATE_182 = 0x10b6, PROP_ENDPOINT_STATE_183 = 0x10b7, PROP_ENDPOINT_STATE_184 = 0x10b8, PROP_ENDPOINT_STATE_185 = 0x10b9, PROP_ENDPOINT_STATE_186 = 0x10ba, PROP_ENDPOINT_STATE_187 = 0x10bb, PROP_ENDPOINT_STATE_188 = 0x10bc, PROP_ENDPOINT_STATE_189 = 0x10bd, PROP_ENDPOINT_STATE_190 = 0x10be, PROP_ENDPOINT_STATE_191 = 0x10bf, PROP_ENDPOINT_STATE_192 = 0x10c0, PROP_ENDPOINT_STATE_193 = 0x10c1, PROP_ENDPOINT_STATE_194 = 0x10c2, PROP_ENDPOINT_STATE_195 = 0x10c3, PROP_ENDPOINT_STATE_196 = 0x10c4, PROP_ENDPOINT_STATE_197 = 0x10c5, PROP_ENDPOINT_STATE_198 = 0x10c6, PROP_ENDPOINT_STATE_199 = 0x10c7, PROP_ENDPOINT_STATE_200 = 0x10c8, PROP_ENDPOINT_STATE_201 = 0x10c9, PROP_ENDPOINT_STATE_202 = 0x10ca, PROP_ENDPOINT_STATE_203 = 0x10cb, PROP_ENDPOINT_STATE_204 = 0x10cc, PROP_ENDPOINT_STATE_205 = 0x10cd, PROP_ENDPOINT_STATE_206 = 0x10ce, PROP_ENDPOINT_STATE_207 = 0x10cf, PROP_ENDPOINT_STATE_208 = 0x10d0, PROP_ENDPOINT_STATE_209 = 0x10d1, PROP_ENDPOINT_STATE_210 = 0x10d2, PROP_ENDPOINT_STATE_211 = 0x10d3, PROP_ENDPOINT_STATE_212 = 0x10d4, PROP_ENDPOINT_STATE_213 = 0x10d5, PROP_ENDPOINT_STATE_214 = 0x10d6, PROP_ENDPOINT_STATE_215 = 0x10d7, PROP_ENDPOINT_STATE_216 = 0x10d8, PROP_ENDPOINT_STATE_217 = 0x10d9, PROP_ENDPOINT_STATE_218 = 0x10da, PROP_ENDPOINT_STATE_219 = 0x10db, PROP_ENDPOINT_STATE_220 = 0x10dc, PROP_ENDPOINT_STATE_221 = 0x10dd, PROP_ENDPOINT_STATE_222 = 0x10de, PROP_ENDPOINT_STATE_223 = 0x10df, PROP_ENDPOINT_STATE_224 = 0x10e0, PROP_ENDPOINT_STATE_225 = 0x10e1, PROP_ENDPOINT_STATE_226 = 0x10e2, PROP_ENDPOINT_STATE_227 = 0x10e3, PROP_ENDPOINT_STATE_228 = 0x10e4, PROP_ENDPOINT_STATE_229 = 0x10e5, PROP_ENDPOINT_STATE_230 = 0x10e6, PROP_ENDPOINT_STATE_231 = 0x10e7, PROP_ENDPOINT_STATE_232 = 0x10e8, PROP_ENDPOINT_STATE_233 = 0x10e9, PROP_ENDPOINT_STATE_234 = 0x10ea, PROP_ENDPOINT_STATE_235 = 0x10eb, PROP_ENDPOINT_STATE_236 = 0x10ec, PROP_ENDPOINT_STATE_237 = 0x10ed, PROP_ENDPOINT_STATE_238 = 0x10ee, PROP_ENDPOINT_STATE_239 = 0x10ef, PROP_ENDPOINT_STATE_240 = 0x10f0, PROP_ENDPOINT_STATE_241 = 0x10f1, PROP_ENDPOINT_STATE_242 = 0x10f2, PROP_ENDPOINT_STATE_243 = 0x10f3, PROP_ENDPOINT_STATE_244 = 0x10f4, PROP_ENDPOINT_STATE_245 = 0x10f5, PROP_ENDPOINT_STATE_246 = 0x10f6, PROP_ENDPOINT_STATE_247 = 0x10f7, PROP_ENDPOINT_STATE_248 = 0x10f8, PROP_ENDPOINT_STATE_249 = 0x10f9, PROP_ENDPOINT_STATE_250 = 0x10fa, PROP_ENDPOINT_STATE_251 = 0x10fb, PROP_ENDPOINT_STATE_252 = 0x10fc, PROP_ENDPOINT_STATE_253 = 0x10fd, PROP_ENDPOINT_STATE_254 = 0x10fe, PROP_ENDPOINT_STATE_255 = 0x10ff, PROP_ENDPOINT_STATES = 0x1100 } |
System endpoint property id enum. | |
enum | sl_cpc_system_status_t { STATUS_OK = 0, STATUS_FAILURE = 1, STATUS_UNIMPLEMENTED = 2, STATUS_INVALID_ARGUMENT = 3, STATUS_INVALID_STATE = 4, STATUS_INVALID_COMMAND = 5, STATUS_INVALID_INTERFACE = 6, STATUS_INTERNAL_ERROR = 7, STATUS_SECURITY_ERROR = 8, STATUS_PARSE_ERROR = 9, STATUS_IN_PROGRESS = 10, STATUS_NOMEM = 11, STATUS_BUSY = 12, STATUS_PROP_NOT_FOUND = 13, STATUS_PACKET_DROPPED = 14, STATUS_EMPTY = 15, STATUS_CMD_TOO_BIG = 16, STATUS_NO_ACK = 17, STATUS_CCA_FAILURE = 18, STATUS_ALREADY = 19, STATUS_ITEM_NOT_FOUND = 20, STATUS_INVALID_COMMAND_FOR_PROP = 21, STATUS_RESET_POWER_ON = 112, STATUS_RESET_EXTERNAL = 113, STATUS_RESET_SOFTWARE = 114, STATUS_RESET_FAULT = 115, STATUS_RESET_CRASH = 116, STATUS_RESET_ASSERT = 117, STATUS_RESET_OTHER = 118, STATUS_RESET_UNKNOWN = 119, STATUS_RESET_WATCHDOG = 120 } |
System status code id. | |
enum | sl_cpc_system_reboot_mode_t { REBOOT_APPLICATION = 0, REBOOT_BOOTLOADER = 1 } |
Bootloader reboot mode. | |
enum | sl_cpc_system_cmd_id_t { CMD_SYSTEM_NOOP = 0x00, CMD_SYSTEM_RESET = 0x01, CMD_SYSTEM_PROP_VALUE_GET = 0x02, CMD_SYSTEM_PROP_VALUE_SET = 0x03, CMD_SYSTEM_PROP_VALUE_IS = 0x06 } |
System endpoint command id enum. | |
Macro Definition Documentation
◆ EP_ID_TO_PROPERTY_ID
#define EP_ID_TO_PROPERTY_ID | ( | ep_id | ) | ((sl_cpc_property_id_t)((0x00001000 | ((ep_id) & 0x000000FF)))) |
Helper macros to convert an enpoint id (uint8_t) to a PROP_ENDPOINT_STATE_x enum value.
◆ PROPERTY_ID_TO_EP_ID
#define PROPERTY_ID_TO_EP_ID | ( | property_id | ) | ((uint8_t)(property_id) & 0x000000FF) |
Helper macros to convert a PROP_ENDPOINT_STATE_x enum value to an endpoint id (uint8_t)
◆ AGGREGATED_STATE_LOW
#define AGGREGATED_STATE_LOW | ( | agg | ) | ((sl_cpc_endpoint_state_t)(agg & 0x0F)) |
Helper macros to extract the two aggregated endpoint states encoded in one single byte.
◆ GET_ENDPOINT_STATE_FROM_STATES
#define GET_ENDPOINT_STATE_FROM_STATES | ( | payload, |
|
ep_id |
|||
) |
Value:
((ep_id % 2 == 0) ? AGGREGATED_STATE_LOW(((uint8_t*)payload)[ep_id / 2]) \
: AGGREGATED_STATE_HIGH(((uint8_t*)payload)[ep_id / 2]))
◆ CPC_CAPABILITIES_SECURITY_ENDPOINT_MASK
#define CPC_CAPABILITIES_SECURITY_ENDPOINT_MASK (1 << 0) |
Capabilities mask.
- Note
- Used with the value returned by a property-get on PROP_CAPABILITIES
◆ PAYLOAD_LENGTH_MAX
#define PAYLOAD_LENGTH_MAX 16 |
System endpoint command type.
Enumeration Type Documentation
◆ sl_cpc_property_id_t
enum sl_cpc_property_id_t |
◆ sl_cpc_system_status_t
System status code id.
This enum contains each of the spinel protocol status code
- Note
- This enum is encoded with 4 bytes.
◆ sl_cpc_system_reboot_mode_t
◆ sl_cpc_system_cmd_id_t
System endpoint command id enum.