CLI Commands in RAM

Description

Support for CLI commands stored in and executed from RAM.

Data Structures

struct  cli_storage_ram_t
 Struct representing an instance of the CLI storage RAM.
 

Functions

void sl_cli_storage_ram_clear (sl_cli_command_arg_t *arguments)
 Clear the command lines stored in ram.
 
void sl_cli_storage_ram_list (sl_cli_command_arg_t *arguments)
 Print the contet of the command lines stored in ram.
 
void sl_cli_storage_ram_define (sl_cli_command_arg_t *arguments)
 Start defining new command lines that will be stored in ram.
 
void sl_cli_storage_ram_execute (sl_cli_command_arg_t *arguments)
 Execute command lines stored in ram.
 
size_t sl_cli_storage_ram_count (sl_cli_handle_t cli_handle)
 Get the number of command lines stored in ram.
 
void sl_cli_storage_ram_init (cli_storage_ram_handle_t handle)
 Initialize the cli_storage_ram instance.
 

Typedefs

typedef cli_storage_ram_tcli_storage_ram_handle_t
 Definition of the CLI storage RAM handle.
 

Variables

typedef MBEDTLS_PRIVATE
 

Function Documentation

◆ sl_cli_storage_ram_clear()

void sl_cli_storage_ram_clear ( sl_cli_command_arg_t arguments)

Clear the command lines stored in ram.

This function can be used directly as a cli command handler.

Parameters
[in]argumentsA pointer to the command arguments.

◆ sl_cli_storage_ram_list()

void sl_cli_storage_ram_list ( sl_cli_command_arg_t arguments)

Print the contet of the command lines stored in ram.

This function can be used directly as a cli command handler.

Parameters
[in]argumentsA pointer to the command arguments.

◆ sl_cli_storage_ram_define()

void sl_cli_storage_ram_define ( sl_cli_command_arg_t arguments)

Start defining new command lines that will be stored in ram.

This function can be used directly as a cli command handler.

Parameters
[in]argumentsA pointer to the command arguments.

◆ sl_cli_storage_ram_execute()

void sl_cli_storage_ram_execute ( sl_cli_command_arg_t arguments)

Execute command lines stored in ram.

This function can be used directly as a cli command handler.

Note
The function has a different implementation in a bare-metal vs. kernel configurations. In a bare-metal configuration, this function will signal that stored commands shall be run by the sl_cli_storage_ram_tick function. One stored command is executed for each call to the sl_cli_storage_ram_tick function. In a kernel configuration, all stored commands will be executed before this function returns.
Parameters
[in]argumentsA pointer to the command arguments.

◆ sl_cli_storage_ram_count()

size_t sl_cli_storage_ram_count ( sl_cli_handle_t  cli_handle)

Get the number of command lines stored in ram.

Parameters
[in]cli_handleHandle to the CLI where the cli_storage_ram component is connected.
Returns
The number of command lines stored in ram.

◆ sl_cli_storage_ram_init()

void sl_cli_storage_ram_init ( cli_storage_ram_handle_t  handle)

Initialize the cli_storage_ram instance.

Parameters
[in]handleA handle to the cli_storage_ram instance.

Typedef Documentation

◆ cli_storage_ram_handle_t

Definition of the CLI storage RAM handle.