sl_cli_command_entry_t Struct Reference
Struct associating a command with a string.
#include <sl_cli_types.h>
Data Fields | |
const char * | name |
String associated with command/group. | |
const sl_cli_command_info_t * | command |
Pointer to command information. | |
const bool | is_shortcut |
Indicating if the entry is a shortcut. | |
Struct associating a command with a string.
The command table should be an array of these kinds of structs.
Field Documentation
◆ name
const char* sl_cli_command_entry_t::name |
String associated with command/group.
◆ command
const sl_cli_command_info_t* sl_cli_command_entry_t::command |
Pointer to command information.
◆ is_shortcut
const bool sl_cli_command_entry_t::is_shortcut |
Indicating if the entry is a shortcut.