Silicon Labs
gecko-platform/4.1/emlib/api/efm32xg1/service/api/structsl-iostream-eusart-config-t
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
Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32xg1/service/api/structsl-iostream-eusart-config-t in 0.13 seconds
Central and Peripheral Roles | Connections | Bluetooth LE | v4.0 | Silicon Labs
https://docs.silabs.com/....
// Bluetooth LE//Version 4.0 //General ... and multi-central connections (which are part of the Bluetooth 4.1 spec) which means that a device can be simultaneously in a central and in a ...
BGAPI | BGAPI headers | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/....
A device type, class ID, message type and message ID together construct a unique ... Find out the device type from Byte 1 of the message header. ... BGAPI message header format Byte 1 Byte 2
Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
https://docs.silabs.com/.../sl-bt-adverti...
You are viewing documentation for version: 8.0.0 Advertiser# ... flags Configuration flags. Value: 0 or bitmask of Generic Advertising Configuration Flags Default : 0 Configure the legacy and ...
sl_bt_evt_scanner_scan_reportScanner | Scanner | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/.../a00...
1: Extended advertising PDUs used | | bd_addr | address | Bluetooth address of the remote device | | uint8_ ... Values:* 0: Public address 1: Random address 255: No address provided (anonymous ...
AN1302: Bluetooth Low Energy Application Security Design Considerations in SDK v3.x and Higher
https://www.silabs.com/.../an1302-bluetooth-application-security-design-considerations....
3.1.4.2 Filter Accept List and Advertisement Filtering ... 4.2.3 Application Layer Encryption Example The example accompanying this application note, available on ... Test_data 4.3 Table 4-1.
Resource TypeApplication Notes
    Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32xg1/service/api/structsl-iostream-eusart-config-t