Silicon Labs
gecko-platform/4.1/emlib/api/efm32xg23/service/api/group-device-init-clocks
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
    Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32xg23/service/api/group-device-init-clocks in 0.20 seconds
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command ... Commands Variables Examples
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    gos_result_t gos_cmd_issue (const char *fmt,.) Issue Gecko OS Command. More. ... Issue Gecko OS command, return the uint32 result. ... Issue Gecko OS command, store string result in buffer.
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    1 - an update is available, the contains the new bundle version string 2 - no update available (i.e. the device's current firmware is up-to-date) <message ... ipd 1 Input, high-impedance
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... system.cmd.buffered system.cmd.echo system.cmd.header_enabled system.cmd.prompt_enabled
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API ... <index> - the index obtained from the scan command output ... os pins can only use the strong drive strength.
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efm32xg23/service/api/group-device-init-clocks