Cpc_security_secondary
Description
CPC Security Secondary.
Overview
TODO
Initialization
TODO
Data Structures | |
struct | sl_cpc_unbind_notification_handle_t |
Enumeration representing unbind notification handle. | |
Functions | |
sl_cpc_security_state_t | sl_cpc_security_get_state (void) |
Get the setup status of the security subsystem. | |
void | sl_cpc_security_fetch_user_specified_binding_key (uint8_t **key, uint16_t *key_size_in_bytes) |
User callback to provide CPC with a binding key. | |
uint64_t | sl_cpc_security_on_unbind_request (bool is_link_encrypted) |
Authorize an unbind request. | |
sl_status_t | sl_cpc_security_unbind (void) |
Unbind device. | |
sl_status_t | sl_cpc_security_unbind_subscribe (sl_cpc_unbind_notification_handle_t *handle, sl_cpc_unbind_notification_t callback, void *data) |
Register a callback that will be called when an unbind event occurs. | |
sl_status_t | sl_cpc_security_unbind_unsubscribe (sl_cpc_unbind_notification_handle_t *handle) |
Unregister a callback that will be called when an unbind event occurs. | |
Typedefs | |
typedef void(* | sl_cpc_unbind_notification_t) (void *data) |
Typedef for the user-supplied callback function, which is called when unbinding (authorized). | |
Enumerations | |
enum | sl_cpc_security_state_t { SL_CPC_SECURITY_STATE_NOT_READY = 0x00, SL_CPC_SECURITY_STATE_DISABLED = 0x01, SL_CPC_SECURITY_STATE_INITIALIZING = 0x02, SL_CPC_SECURITY_STATE_WAITING_ON_TX_COMPLETE = 0x3, SL_CPC_SECURITY_STATE_INITIALIZED = 0x04 } |
Enumeration representing security state. | |
Function Documentation
◆ sl_cpc_security_get_state()
sl_cpc_security_state_t sl_cpc_security_get_state | ( | void |
| ) |
Get the setup status of the security subsystem.
- Returns
- The setup status of the security subsystem.
◆ sl_cpc_security_fetch_user_specified_binding_key()
void sl_cpc_security_fetch_user_specified_binding_key | ( | uint8_t ** | key, |
uint16_t * | key_size_in_bytes |
||
) |
User callback to provide CPC with a binding key.
SL_CPC_SECURITY_BINDING_KEY_METHOD config must be set to SL_CPC_SECURITY_BINDING_KEY_CUSTOMER_SPECIFIC
- Parameters
-
[out] key
The encryption key [out] key_size
The encryption key size Note: Only 16 bytes keys are supported for the moment
◆ sl_cpc_security_on_unbind_request()
uint64_t sl_cpc_security_on_unbind_request | ( | bool | is_link_encrypted | ) |
Authorize an unbind request.
- Note
- Declared as a weak symbol. If no strong definition is given by the user, unbind requests are always denied. If the user gives a definition for this function, its return value will dictate if unbind requests are accepted.
- Returns
- Whether to allow unbind or not, use SL_CPC_SECURITY_OK_TO_UNBIND as a return value to allow. Return anything else to deny.
◆ sl_cpc_security_unbind()
sl_status_t sl_cpc_security_unbind | ( | void |
| ) |
Unbind device.
- Returns
- Status code.
◆ sl_cpc_security_unbind_subscribe()
sl_status_t sl_cpc_security_unbind_subscribe | ( | sl_cpc_unbind_notification_handle_t * | handle, |
sl_cpc_unbind_notification_t | callback, |
||
void * | data |
||
) |
Register a callback that will be called when an unbind event occurs.
- Parameters
-
[in] handle
pointer to the unbind notification handle. [in] callback
pointer to the unbind notification callback. [in] data
pointer to pass to the unbind notification callback.
- Returns
- Status code.
◆ sl_cpc_security_unbind_unsubscribe()
sl_status_t sl_cpc_security_unbind_unsubscribe | ( | sl_cpc_unbind_notification_handle_t * | handle | ) |
Unregister a callback that will be called when an unbind event occurs.
- Parameters
-
[in] handle
pointer to the unbind notification handle.
- Returns
- Status code.
Typedef Documentation
◆ sl_cpc_unbind_notification_t
typedef void(* sl_cpc_unbind_notification_t) (void *data) |
Typedef for the user-supplied callback function, which is called when unbinding (authorized).
- Parameters
-
data
User-specific argument.
Enumeration Type Documentation
◆ sl_cpc_security_state_t
Enumeration representing security state.