sl_cli_instance_parameters_t Struct Reference

The structure defining the parameters for creating a CLI instance.

#include <sl_cli_types.h>

Data Fields

const char * task_name
 Task name.
 
sl_iostream_tiostream_handle
 IOstream handle.
 
sl_cli_command_group_tdefault_command_group
 Command_group.
 
osThreadId_t thread_id
 Thread ID.
 
void * thread_cb
 Thread control block.
 
void * stack
 Pointer to the stack.
 
uint32_t stack_size
 Stack size.
 
osPriority_t prio
 Task priority.
 
uint32_t start_delay_ms
 Task start delay.
 
uint32_t loop_delay_ms
 Task loop delay.
 

The structure defining the parameters for creating a CLI instance.

Field Documentation

◆ task_name

const char* sl_cli_instance_parameters_t::task_name

Task name.

◆ iostream_handle

sl_iostream_t* sl_cli_instance_parameters_t::iostream_handle

IOstream handle.

◆ default_command_group

sl_cli_command_group_t* sl_cli_instance_parameters_t::default_command_group

Command_group.

◆ thread_id

osThreadId_t sl_cli_instance_parameters_t::thread_id

Thread ID.

◆ thread_cb

void* sl_cli_instance_parameters_t::thread_cb

Thread control block.

Can be set to NULL for dynamic allocation.

◆ stack

void* sl_cli_instance_parameters_t::stack

Pointer to the stack.

Can be set to NULL for dynamic allocation.

◆ stack_size

uint32_t sl_cli_instance_parameters_t::stack_size

Stack size.

◆ prio

osPriority_t sl_cli_instance_parameters_t::prio

Task priority.

◆ start_delay_ms

uint32_t sl_cli_instance_parameters_t::start_delay_ms

Task start delay.

◆ loop_delay_ms

uint32_t sl_cli_instance_parameters_t::loop_delay_ms

Task loop delay.