// Platform//Version 5.1.0 //Drivers ... You are viewing documentation for version: 5.1.0 Simple Button Driver# ... The Simple Button driver is a module of the button driver that provides the ...
// Set to 1 to enable hardware flow control. ... is not required, make sure that EMDRV_UARTDRV_FLOW_CONTROL_ENABLE is set to 0. ... { \ .head = 0, \ .tail = 0, \ .used = 0, \ .size = qSize, \
ProductMicrocontrollersResource TypeSoftware API documentation
Simplicity Studio 5 Users Guide//Version 5.9.1 ... The base Simplicity Studio platform (not an installer) is delivered in a tar file that should be expanded into the desired installation ...
Home Training ... You are viewing documentation for version: 5.5.0 Simplicity Studio® 5 User's Guide# Simplicity Studio is the core development environment designed to support the Silicon ...
ProductSimplicity StudioResource TypeSoftware API Documentation
You are viewing documentation for version: 4.0 Central and Peripheral Roles# ... and multi-central connections (which are part of the Bluetooth 4.1 spec) which means that a device can be ...
Results 1-5 of 5 for gecko-platform/5.0.1/platform-middleware/usb-host