The static part of an event.
Each event can be used with only one event queue.
Public Attributes#
struct EventQueue_s *
the queue this event goes on
void(*
called when the event fires
void(*
marking fuction, can be NULL
const char *
event name for debugging purposes
Public Attribute Documentation#
queue#
struct EventQueue_s* EventActions::queue
the queue this event goes on
Definition at line
478
of file platform/service/token_manager/test/stack/include/sl_zigbee_types.h
handler#
void(* EventActions::handler) (struct Event_s *)
called when the event fires
Definition at line
479
of file platform/service/token_manager/test/stack/include/sl_zigbee_types.h
marker#
void(* EventActions::marker) (struct Event_s *)
marking fuction, can be NULL
Definition at line
480
of file platform/service/token_manager/test/stack/include/sl_zigbee_types.h
name#
const char* EventActions::name
event name for debugging purposes
Definition at line
481
of file platform/service/token_manager/test/stack/include/sl_zigbee_types.h