// Gecko Platform//Version 4.4.1 //Services ... The hardware timer peripheral must be properly clocked from the application. ... All API functions can be called from within interrupt handlers.
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Hardware block inside the SE used for generating random numbers.
You are viewing documentation for version: 4.2 | Version History ... The control block references a ring buffer for each configured channel. ... You should avoid using it in production.
ProductMicrocontrollersResource TypeSoftware API documentation
The SE Manager API document can be found at https://docs.silabs.com/gecko-platform/latest/service/api/group-sl-se-manager. ... (Note that this API is not available for EFR32xG21B-based parts).
Resource TypeApplication Notes
Results 1-5 of 5 for gecko-platform/5.0.2/platform-security-api/psa-builtin-keys