Overview#

The programming model applies only to projects that are generated by Simplicity Studio v5's project configuration tool. As of this release this is only applicable to Bluetooth and Proprietary SDKs. This section explains the details of how a project generated by Simplicity Studio v5's project configuration tool works, and how you integrate your application to it. This covers both new projects and projects that are migrated to the new SDK version.

The programming model covers several important areas such as hardware initialization, software initialization, and periodic action processing. It covers both bare metal and kernel based applications. For instance, in case of a bare metal application, this programming model will allow you to add processing action functions to the main loop.

If you are migrating an existing application to this new version, be aware that this programming model now handles some hardware initializations (hardware clocks, DCDC, etc) and some software initializations (kernel, stacks, etc) that you may have had to do manually with previous versions.

Using this programming model for your application is important as it will ensure proper hardware initialization and proper SDK software modules initialization. Using this programming model will also ensure proper power management, as power management has to be a centralized service (power requirements can come from different requesters). For more information on power management, refer to Power Manager section.

Note: The SDK Programming model is compatible with SiSDK 2025.6 and greater versions.

Features#

Initialization#

In a bare metal application, a single function, sl_main_init(), is provided to you. This function initializes all the SDK modules that are selected in your project.

With a RTOS kernel, the main() function is executed as a task. The function sl_main_second_stage_init() is used to initialize the SDK modules present in your project.

Note: System Setup (sl_main) is the new standard for the initialization sequence replacing System Setup (sl_system), differing in some points. If you want to migrate an sl_system application to sl_main, refer to the SL System to SL Main Migration Guide.

Action Processing#

Some of the SDK modules (mostly services and wireless stacks) have actions to process periodically. Functions are also provided to help you with that. The action processing however differs depending on if you are using a kernel or if you have a bare metal application.

Bare Metal#

If your application is bare metal, a function called sl_main_process_action() is provided to you. This function contains all the SDK modules "step" functions that must be called in every iteration of the super loop. You must call this function from your super loop.

Note: For series 3 devices, bare metal is not supported. A RTOS is mandatory for the SiSDK.

When Using a Kernel (RTOS)#

If you selected a kernel in your project, the SDK modules that have to process periodic actions will automatically create task(s) during initialization. Your main() function is called in the start task as the kernel is already started. The start task priority is set to the maximum during initialization`. The start task will terminate by default, but it can be used if desired.

You should do your permanent memory allocations in app_permanent_memory_alloc(), which is called before the kernel is started but after it was initialized. This will improve the memory placement and could lead to lower power consumption. Then, you can create the tasks for your application in app_init().

SDK Component Catalog#

The SDK component catalog is a simple header file named sl_component_catalog.h that you can include from anywhere in your project. This file contains #define entries for the different SDK components available in your project. This allows you to enable/disable portions of code depending on whether a SDK component is present in your project or not.

Usage Examples#

These are examples of main functions that use the functions described above that you can use as a reference. A main.c template file is added automatically to the project during the first generation, but it can be freely be customized without any risk of being overridden.

Bare Metal#

#include "sl_main_init.h"
#include "sl_main_process_action.h"
#include "sl_component_catalog.h"

#ifdef SL_CATALOG_POWER_MANAGER_PRESENT
#include "sl_power_manager.h"
#endif

void app_init(void)
{
  // TODO: Add required initializations for your application.
}

void app_process_action(void)
{
  // TODO: Add required "step" actions for your application.
}

int main(void)
{
  // Initialize Silicon Labs SDK modules.
  sl_main_init();

  // Initialization for your application.
  app_init();

  while (1) {
    // Process periodic actions of your application.
    app_process_action();

    // Process periodic actions of Silicon Labs SDK modules.
    sl_main_process_action();

#ifdef SL_CATALOG_POWER_MANAGER_PRESENT
    // Let the CPU go to sleep if the system allows it.
    sl_power_manager_sleep();
#endif
  }
}

When Using a Kernel (RTOS)#

#include "sl_main_init.h"
#include "sl_main_init_memory.h"
#include "sl_main_kernel.h"

void app_init_early(void)
{
  // This function is called before the kernel is initialized.

  // TODO: Add required initializations for your application.
}

void app_permanent_memory_alloc(void)
{
  // This function is called before the kernel is started,
  // but after the kernel is initialized.

  // TODO: Do the permanent memory allocations for your application.

  // TODO: Create permanent kernel objects for your application.
}

void app_init(void)
{
  // TODO: Add required initializations for your application.

  // TODO: Create kernel tasks for your application.
}

int main(void)
{
  // Initialize Silicon Labs SDK modules.
  sl_main_second_stage_init();

  // Initialization for your application.
  app_init();

  // The start task is deleted when exiting this function.
  // You can also not let this task end and use it.
}

Initializing your Device#

When generating your project on a Silicon Labs kit, the project configuration tools will automatically add two components called Automatic Device Initialization and Clock Manager. These components provide basic hardware configuration functionalities. These functions will automatically be called by sl_main_init().

When generating a project for a custom board, the Automatic Device Initialization and Clock Manager modules can be manually selected.

You can customize these basic configurations by modifying the configurations available in the Device Initialization software component. For more information on this component, see Device Initialization. The Clock Manager is also fully configurable, refer to Clock Manager.

Atomic Section General Considerations#

Overview#

The sl_core module provides two types of basic critical sections (interrupt masking), the critical sections, and the atomic sections. The critical sections will always mask all the interrupts (except the non-maskable ones) by using the PRIMASK register. On the other hand, the atomic sections can mask the interrupts by using either the PRIMASK or BASEPRI register.

Using the BASEPRI register allows you to only mask interrupts based on their interrupt priority. That is to say, only interrupts with equal or lower priority (higher number) than the BASEPRI register value will be masked in an atomic section.

The default value for the BASEPRI register used to mask interrupts in an atomic section is 3. Otherwise, the BASEPRI value is kept to 0 to allow all interrupts.

The benefit of the atomic sections over the critical sections is that it won't mask interrupts that you would consider of very high priority and for which you want to have minimal latency. However, the atomic sections can obviously not be used to protect access to resources that would be accessed by these very high priority interrupt's handlers.

Kernel-aware vs. non kernel-aware interrupt considerations#

The RTOSs currently provided (Micrium OS and FreeRTOS, for example) implement the principle of kernel aware vs non kernel-aware interrupts. The threshold is defined by the BASEPRI register value. That is, when having to protect its internal resources, the kernel will always mask the interrupts using atomic sections. This means any very high priority interrupts will be able to interrupt the kernel. That also means you CANNOT use any kernel API from these very hight interrupt's handlers (you cannot post a semaphore, for instance).

When using FreeRTOS, interrupts priorities MUST be configured either manually or automatically using the Interrupt manager module. This is because when an MCU supports BASEPRI, FreeRTOS will use the configMAX_SYSCALL_INTERRUPT_PRIORITY setting to configure BASEPRI to protect its internal resources from concurrent access.

Interrupt Manager Module#

The Interrupt Manager component initializes all interrupt handler priorities via the sl_interrupt_manager_init() function. The Interrupt Manager module is a dependency of the sl_main module and is added automatically to your project if the sl_main module is selected.

Silicon labs devices with Cortex-M33 core have 4 bits in the NVIC register to encode a priority, therefore the priority range is 0-15.

The Interrupt manager module defines the following value:

Define

Value for Cortex M33

SL_INTERRUPT_MANAGER_DEFAULT_PRIORITY

5

sl_interrupt_manager_init() will therefore initialize all interrupt priorities (except fault handler) to SL_INTERRUPT_MANAGER_DEFAULT_PRIORITY. Since the default priority is lower than the BASEPRI value used in atomic sections, every interrupt is disabled by default during an atomic section. When the interrupt manager service initialization has finished, it is up to your application to call sl_interrupt_manager_set_irq_priority() to change the default priority of an Interrupt Handler according to its needs.

Any modification to an interrupt priority should be done carefully since it can introduce behavior changes in your application difficult to pinpoint.

Memory considerations#

The interrupt manager can relocate the interrupt vector table in RAM and switch the interrupt vector table base address of the core to point to it. This can be achieved by adding the component Interrupt Manager: Interrupt Vector Table in RAM to your project.

The interrupt vector table is always in RAM for Series 3 because the latency of the external FLASH can slow down the execution if the instruction cache misses. For this reason, it is also recommended to place your interrupt routines and time-critical code in RAM using the macro SL_CODE_RAM. The component ICACHE Disable can be used to disable the instruction cache in testing. This can help to identify what code fails when a cache miss happens and would need to be put in RAM.