You are viewing documentation for version:6.1.2 (latest)Public Attributes#sli_cpc_system_cmd_id_tcommand_idIdentifier of the command. uint8_tseqCommand sequence number. uint16_tlengthLength of the payload in bytes. uint8_tpayloadCommand payload. Public Attribute Documentation#command_id#sli_cpc_system_cmd_id_t sli_cpc_system_cmd_t::command_idIdentifier of the command. seq#uint8_t sli_cpc_system_cmd_t::seqCommand sequence number. length#uint16_t sli_cpc_system_cmd_t::lengthLength of the payload in bytes. payload#uint8_t sli_cpc_system_cmd_t::payload[PAYLOAD_LENGTH_MAX]Command payload.