Silicon Labs
gecko-platform/driver/api/struct-u-a-r-t-d-r-v-init-euart-t
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
Results 1-5 of 5 for gecko-platform/driver/api/struct-u-a-r-t-d-r-v-init-euart-t in 0.17 seconds
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... A pointer to this function is passed to sl_sleeptimer_start_timer().
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
// Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... A counter in the tamper filter is increased. ... sl_se_otp_init_t otp_settings_init = SL_SE_OTP_INIT_DEFAULT;
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
... and supports multiple driver instances. The driver does not buffer or queue data. However, it queues UART ... A receiver should set RTS high when it is no longer capable of receiving data.
ProductMicrocontrollers Resource TypeSoftware API documentation
CLI Commands in NVM3 - v3.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-cli-storage-n...
Data Structures struct cli_storage_nvm3_t Struct representing an instance of the CLI storage NVM3. ... A boolean that is true if there are more stored commands to execute, else false.
ProductMicrocontrollers Resource TypeSoftware API documentation
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
P L AT F O R M A N D M C U A P P S | N O V E M B E R 2 0 2 0 ... Driver for the Silicon Labs Si1133 ambient light and UV sensor ... Platform Services Detail Device Initialization
    Results 1-5 of 5 for gecko-platform/driver/api/struct-u-a-r-t-d-r-v-init-euart-t