Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... Command configuration, see gos_cmd_operation_config_t for more details.
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... to update the firmware, or switch back to Gecko OS using the faults_reset command.
ProductWirelessResource TypeSoftware API documentation
BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of how to use each command. ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
. 20 4.1.1 4.1.2 4.1.3 ... 1.3.3 Debug This component provides the bootloader with support for debugging output ... Gecko Bootloader has been built using GSDK v4.0, it is recommended that the ...
Resource TypeUser's Guides
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg/group-usart