Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... reboot ... tcp.client.local_port tcp.client.retries tcp.client.retry_period uart.baud
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
... is the recommended device independent crypto API and should be used whenever possible ... Read SE OTP contents Read SE firmware version Read provisioned certificates Multi-thread safe APIs for ...
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg/middleware/api/group-usb-common