// Bluetooth LE//Version 5.0 //General //System & Performance ... Bluetooth functions in the 2.4 GHz frequency range. ... Bluetooth Low Energy has two channel selection algorithms.
// Bluetooth LE//Version 3.1 //General //System & Performance ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm in those cases when AFH is not enabled ...
// Bluetooth LE//Version 3.1 //General //Advertising and Scanning ... Bluetooth Core Specification - This is the golden reference, but not that easy to digest.
... att_errorcode| Attribute protocol error code 0: No error Non-zero: See Bluetooth specification, ... the request is a reliable write (by Bluetooth Core Specification Volume 3, Part G, 4.9.5).
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32gg11/struct-q-s-p-i-write-config-type-def