Acknowledge for i2c was not received. ... crypto Error using crypto functions 0x0194 ... Errors from Attribute Protocol Bluetooth Mesh errors Bluetooth Mesh foundation errors Filesystem errors
... client configuration was changed or whether a characteristic confirmation was received. Functions# sl_status_t | sl_bt_gatt_ ... See Bluetooth specification Vol 3, Part G, 7.2 for the values.
From a Bluetooth perspective, the tools that were found in Simplicity Studio v4 are now different in Simplicity ... Both functions are very similar internally and differ in the variables used.
Training ... // Bluetooth LE//Version 8.0.0 //Getting Started ... The Bluetooth SDK comes with a number of example application that you can then modify to create your own applications.
Training ... Register // Bluetooth LE//Version 9.0.0 //Developer's Guide ... 9.0.0 Bluetooth LE Developers Guide# The Developer's Guide content is organized in the following groups:
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32xg12/driver/api/struct-s-p-i-d-r-v-init