Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Core Functions for issuing Gecko OS commands. More. ... Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... See Device Firmware Update . The Device Management Server (DMS) To update a Gecko OS ...
ProductWirelessResource TypeSoftware API documentation
... ., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks). ... dependencies on external functions, such as functions from the C standard library, EMLIB, and CMSIS.
Example Example usage. Alphabetical List of Commands ... <index> - the index obtained from the scan command output ... os pins can only use the strong drive strength. ... > gges Example > gges
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32xg12/service/api/group-diagnostics