Training ... // Gecko Platform//Version 4.4.1 //Services ... This driver works with a configurable time unit called tick. ... All API functions can be called from within interrupt handlers.
Driver for the Silicon Labs Si1133 ambient light and UV sensor ... Driver for the Silicon Labs Si7210 Hall effect sensor ... Platform Services Detail Device Initialization
Login ... // Platform//Version 5.0.1 //Security //API Documentation //SE Manager ... Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible.
You are viewing documentation for version: 3.2 | Version History ... Support for CLI commands stored in and executed from NVM3. ... sl_cli_storage_nvm3_clear ( sl_cli_command_arg_t *arguments)
ProductMicrocontrollersResource TypeSoftware API documentation
... Version 2 for the EFR32 SoC Series 1 Platform AN1135: Using Third Generation Non-Volatile ... on NVM3 is documented in the EMDRV->NVM3 section of the Gecko HAL & Driver API Reference Guide.
Resource TypeUser's Guides
Results 1-5 of 5 for gecko-platform/latest/emlib/api/efm32xg12/struct-u-s-a-r-t-init-sync-type-def