LDMA - Linked DMA

Description

Linked Direct Memory Access (LDMA) Peripheral API.

LDMA API functions provide full support for the LDMA peripheral.

LDMA supports these DMA transfer types:

  • Memory to memory.
  • Memory to peripheral.
  • Peripheral to memory.
  • Peripheral to peripheral.
  • Constant value to memory.

LDMA supports linked lists of DMA descriptors allowing:

  • Circular and ping-pong buffer transfers.
  • Scatter-gather transfers.
  • Looped transfers.

LDMA has some advanced features:

  • Intra-channel synchronization (SYNC), allowing hardware events to pause and restart a DMA sequence.
  • Immediate-write (WRI), allowing DMA to write a constant anywhere in the memory map.
  • Complex flow control allowing if-else constructs.

Basic understanding of LDMA controller is assumed. Please refer to the reference manual for further details. The LDMA examples described in the reference manual are particularly helpful in understanding LDMA operations.

In order to use the DMA controller, the initialization function LDMA_Init() must have been executed once (normally during system initialization).

DMA transfers are initiated by a call to LDMA_StartTransfer(), transfer properties are controlled by the contents of LDMA_TransferCfg_t and LDMA_Descriptor_t structure parameters. The LDMA_Descriptor_t structure parameter may be a pointer to an array of descriptors, descriptors in array should be linked together as needed.

Transfer and descriptor initialization macros are provided for the most common transfer types. Due to the flexibility of LDMA peripheral, only a small subset of all possible initializer macros are provided, users should create new ones when needed.

Examples of LDMA usage:

A simple memory to memory transfer:

/* A single transfer of 4 half words. */
static const LDMA_TransferCfg_t transferCfg = LDMA_TRANSFER_CFG_MEMORY();
static const LDMA_Descriptor_t desc = LDMA_DESCRIPTOR_SINGLE_M2M_HALF(src, dst, 4);
void ldmaTransfer(void)
{
/* Initialize the LDMA with default values. */
LDMA_Init(&init);
/* Start the memory transfer */
LDMA_StartTransfer(0, &transferCfg, &desc);
}


A linked list of three memory to memory transfers:

/* A transfer consisting of 3 descriptors linked together and each descriptor
* transfers 4 words from the source to the destination. */
static const LDMA_TransferCfg_t transferCfg1 = LDMA_TRANSFER_CFG_MEMORY();
static const LDMA_Descriptor_t descList[] =
{
LDMA_DESCRIPTOR_LINKREL_M2M_WORD(src + 4, dst + 4, 4, 1),
LDMA_DESCRIPTOR_SINGLE_M2M_WORD(src + 8, dst + 8, 4)
};
void ldmaLinkedTransfer(void)
{
/* Initialize the LDMA with default values. */
LDMA_Init(&init);
/* Start the linked memory transfer */
LDMA_StartTransfer(0, &transferCfg1, &descList[0]);
}


DMA from serial port peripheral to memory:

/* The LDMA transfer should be triggered by the USART1 RX data available signal. */
static const LDMA_TransferCfg_t usart1RxTransfer =
/* Transfer 4 bytes from the USART1 RX FIFO to memory. */
static const LDMA_Descriptor_t usart1RxDesc =
LDMA_DESCRIPTOR_SINGLE_P2M_BYTE(&USART1->RXDATA, // Peripheral address
dst, // Destination (SRAM)
4); // Number of byte transfers
void ldmaPeripheralTransfer(void)
{
/* Initialize the LDMA with default values. */
LDMA_Init(&init);
/* Start the peripheral transfer which is triggered by the USART1
* peripheral RXDATAV signal. */
LDMA_StartTransfer(0, &usart1RxTransfer, &usart1RxDesc);
}


Ping-pong DMA from serial port peripheral to memory:

/* Two buffers used in the ping-pong transfer from USART1. */
static volatile uint8_t buffer0[5];
static volatile uint8_t buffer1[5];
/* The LDMA transfer should be triggered by the USART1 RX data available signal. */
static const LDMA_TransferCfg_t usart1Transfer =
/* Both descriptors transfer 5 bytes from the USART1 rx data register into
* one of the buffers. Note that the first descriptor uses a relative address
* of 1 to link to the next descriptor, while the last descriptor uses a
* relative address of -1 to link to the first descriptor. */
static const LDMA_Descriptor_t rxLoop[] =
{
LDMA_DESCRIPTOR_LINKREL_P2M_BYTE(&USART1->RXDATA, buffer0, 5, 1),
LDMA_DESCRIPTOR_LINKREL_P2M_BYTE(&USART1->RXDATA, buffer1, 5, -1)
};
void ldmaPingPongTransfer(void)
{
/* Initialize the LDMA with default values. */
LDMA_Init(&init);
/* Start the peripheral transfer which is triggered by the USART1
* peripheral RXDATAV signal. */
LDMA_StartTransfer(0, &usart1Transfer, &rxLoop[0]);
}
Note
LDMA module does not implement LDMA interrupt handler. A template for an LDMA IRQ handler is included here as an example.
/* Template for an LDMA IRQ handler. */
void LDMA_IRQHandler(void)
{
uint32_t ch;
/* Get all pending and enabled interrupts. */
uint32_t pending = LDMA_IntGetEnabled();
/* Loop here on an LDMA error to enable debugging. */
while (pending & LDMA_IF_ERROR) {
}
/* Iterate over all LDMA channels. */
for (ch = 0; ch < DMA_CHAN_COUNT; ch++) {
uint32_t mask = 0x1 << ch;
if (pending & mask) {
/* Clear interrupt flag. */
#if defined (LDMA_HAS_SET_CLEAR)
LDMA->IF_CLR = mask;
#else
LDMA->IFC = mask;
#endif
/* Do more stuff here, execute callbacks etc. */
}
}
}

Data Structures

union  LDMA_Descriptor_t
 DMA descriptor.
 
struct  LDMA_Init_t
 LDMA initialization configuration structure.
 
struct  LDMA_TransferCfg_t
 DMA transfer configuration structure.
 

Functions

void LDMA_DeInit (void)
 De-initialize the LDMA controller.
 
void LDMA_EnableChannelRequest (int ch, bool enable)
 Enable or disable an LDMA channel request.
 
void LDMA_Init (const LDMA_Init_t *init)
 Initialize the LDMA controller.
 
void LDMA_StartTransfer (int ch, const LDMA_TransferCfg_t *transfer, const LDMA_Descriptor_t *descriptor)
 Start a DMA transfer.
 
void LDMA_StopTransfer (int ch)
 Stop a DMA transfer.
 
bool LDMA_TransferDone (int ch)
 Check if a DMA transfer has completed.
 
uint32_t LDMA_TransferRemainingCount (int ch)
 Get the number of items remaining in a transfer.
 
bool LDMA_ChannelEnabled (int ch)
 Check if a certain channel is enabled.
 
void LDMA_IntClear (uint32_t flags)
 Clear one or more pending LDMA interrupts.
 
void LDMA_IntDisable (uint32_t flags)
 Disable one or more LDMA interrupts.
 
void LDMA_IntEnable (uint32_t flags)
 Enable one or more LDMA interrupts.
 
uint32_t LDMA_IntGet (void)
 Get pending LDMA interrupt flags.
 
uint32_t LDMA_IntGetEnabled (void)
 Get enabled and pending LDMA interrupt flags.
 
void LDMA_IntSet (uint32_t flags)
 Set one or more pending LDMA interrupts.
 

Macros

#define LDMA_INIT_DEFAULT
 Default DMA initialization structure.
 
#define LDMA_TRANSFER_CFG_MEMORY()
 Generic DMA transfer configuration for memory to memory transfers.
 
#define LDMA_TRANSFER_CFG_MEMORY_LOOP(loopCnt)
 Generic DMA transfer configuration for looped memory to memory transfers.
 
#define LDMA_TRANSFER_CFG_PERIPHERAL(signal)
 Generic DMA transfer configuration for memory to/from peripheral transfers.
 
#define LDMA_TRANSFER_CFG_PERIPHERAL_LOOP(signal, loopCnt)
 Generic DMA transfer configuration for looped memory to/from peripheral transfers.
 
#define LDMA_DESCRIPTOR_SINGLE_M2M_WORD(src, dest, count)
 DMA descriptor initializer for single memory to memory word transfer.
 
#define LDMA_DESCRIPTOR_SINGLE_M2M_HALF(src, dest, count)
 DMA descriptor initializer for single memory to memory half-word transfer.
 
#define LDMA_DESCRIPTOR_SINGLE_M2M_BYTE(src, dest, count)
 DMA descriptor initializer for single memory to memory byte transfer.
 
#define LDMA_DESCRIPTOR_LINKABS_M2M_WORD(src, dest, count)
 DMA descriptor initializer for linked memory to memory word transfer.
 
#define LDMA_DESCRIPTOR_LINKABS_M2M_HALF(src, dest, count)
 DMA descriptor initializer for linked memory to memory half-word transfer.
 
#define LDMA_DESCRIPTOR_LINKABS_M2M_BYTE(src, dest, count)
 DMA descriptor initializer for linked memory to memory byte transfer.
 
#define LDMA_DESCRIPTOR_LINKREL_M2M_WORD(src, dest, count, linkjmp)
 DMA descriptor initializer for linked memory to memory word transfer.
 
#define LDMA_DESCRIPTOR_LINKREL_M2M_HALF(src, dest, count, linkjmp)
 DMA descriptor initializer for linked memory to memory half-word transfer.
 
#define LDMA_DESCRIPTOR_LINKREL_M2M_BYTE(src, dest, count, linkjmp)
 DMA descriptor initializer for linked memory to memory byte transfer.
 
#define LDMA_DESCRIPTOR_SINGLE_P2M_BYTE(src, dest, count)
 DMA descriptor initializer for byte transfers from a peripheral to memory.
 
#define LDMA_DESCRIPTOR_SINGLE_P2P_BYTE(src, dest, count)
 DMA descriptor initializer for byte transfers from a peripheral to a peripheral.
 
#define LDMA_DESCRIPTOR_SINGLE_M2P_BYTE(src, dest, count)
 DMA descriptor initializer for byte transfers from memory to a peripheral.
 
#define LDMA_DESCRIPTOR_LINKREL_P2M_BYTE(src, dest, count, linkjmp)
 DMA descriptor initializer for byte transfers from a peripheral to memory.
 
#define LDMA_DESCRIPTOR_LINKREL_P2M_WORD(src, dest, count, linkjmp)
 DMA descriptor initializer for word transfers from a peripheral to memory.
 
#define LDMA_DESCRIPTOR_LINKREL_M2P_BYTE(src, dest, count, linkjmp)
 DMA descriptor initializer for byte transfers from memory to a peripheral.
 
#define LDMA_DESCRIPTOR_SINGLE_WRITE(value, address)
 DMA descriptor initializer for Immediate WRITE transfer.
 
#define LDMA_DESCRIPTOR_LINKABS_WRITE(value, address)
 DMA descriptor initializer for Immediate WRITE transfer.
 
#define LDMA_DESCRIPTOR_LINKREL_WRITE(value, address, linkjmp)
 DMA descriptor initializer for Immediate WRITE transfer.
 
#define LDMA_DESCRIPTOR_SINGLE_SYNC(set, clr, matchValue, matchEnable)
 DMA descriptor initializer for SYNC transfer.
 
#define LDMA_DESCRIPTOR_LINKABS_SYNC(set, clr, matchValue, matchEnable)
 DMA descriptor initializer for SYNC transfer.
 
#define LDMA_DESCRIPTOR_LINKREL_SYNC(set, clr, matchValue, matchEnable, linkjmp)
 DMA descriptor initializer for SYNC transfer.
 

Enumerations

enum  LDMA_CtrlBlockSize_t {
  ldmaCtrlBlockSizeUnit1 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT1,
  ldmaCtrlBlockSizeUnit2 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT2,
  ldmaCtrlBlockSizeUnit3 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT3,
  ldmaCtrlBlockSizeUnit4 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT4,
  ldmaCtrlBlockSizeUnit6 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT6,
  ldmaCtrlBlockSizeUnit8 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT8,
  ldmaCtrlBlockSizeUnit16 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT16,
  ldmaCtrlBlockSizeUnit32 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT32,
  ldmaCtrlBlockSizeUnit64 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT64,
  ldmaCtrlBlockSizeUnit128 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT128,
  ldmaCtrlBlockSizeUnit256 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT256,
  ldmaCtrlBlockSizeUnit512 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT512,
  ldmaCtrlBlockSizeUnit1024 = _LDMA_CH_CTRL_BLOCKSIZE_UNIT1024,
  ldmaCtrlBlockSizeAll = _LDMA_CH_CTRL_BLOCKSIZE_ALL
}
 Controls the number of unit data transfers per arbitration cycle, providing a means to balance DMA channels' load on the controller.
 
enum  LDMA_CtrlStructType_t {
  ldmaCtrlStructTypeXfer = _LDMA_CH_CTRL_STRUCTTYPE_TRANSFER,
  ldmaCtrlStructTypeSync = _LDMA_CH_CTRL_STRUCTTYPE_SYNCHRONIZE,
  ldmaCtrlStructTypeWrite = _LDMA_CH_CTRL_STRUCTTYPE_WRITE
}
 DMA structure type.
 
enum  LDMA_CtrlReqMode_t {
  ldmaCtrlReqModeBlock = _LDMA_CH_CTRL_REQMODE_BLOCK,
  ldmaCtrlReqModeAll = _LDMA_CH_CTRL_REQMODE_ALL
}
 DMA transfer block or cycle selector.
 
enum  LDMA_CtrlSrcInc_t {
  ldmaCtrlSrcIncOne = _LDMA_CH_CTRL_SRCINC_ONE,
  ldmaCtrlSrcIncTwo = _LDMA_CH_CTRL_SRCINC_TWO,
  ldmaCtrlSrcIncFour = _LDMA_CH_CTRL_SRCINC_FOUR,
  ldmaCtrlSrcIncNone = _LDMA_CH_CTRL_SRCINC_NONE
}
 Source address increment unit size.
 
enum  LDMA_CtrlSize_t {
  ldmaCtrlSizeByte = _LDMA_CH_CTRL_SIZE_BYTE,
  ldmaCtrlSizeHalf = _LDMA_CH_CTRL_SIZE_HALFWORD,
  ldmaCtrlSizeWord = _LDMA_CH_CTRL_SIZE_WORD
}
 DMA transfer unit size.
 
enum  LDMA_CtrlDstInc_t {
  ldmaCtrlDstIncOne = _LDMA_CH_CTRL_DSTINC_ONE,
  ldmaCtrlDstIncTwo = _LDMA_CH_CTRL_DSTINC_TWO,
  ldmaCtrlDstIncFour = _LDMA_CH_CTRL_DSTINC_FOUR,
  ldmaCtrlDstIncNone = _LDMA_CH_CTRL_DSTINC_NONE
}
 Destination address increment unit size.
 
enum  LDMA_CtrlSrcAddrMode_t {
  ldmaCtrlSrcAddrModeAbs = _LDMA_CH_CTRL_SRCMODE_ABSOLUTE,
  ldmaCtrlSrcAddrModeRel = _LDMA_CH_CTRL_SRCMODE_RELATIVE
}
 Source addressing mode.
 
enum  LDMA_CtrlDstAddrMode_t {
  ldmaCtrlDstAddrModeAbs = _LDMA_CH_CTRL_DSTMODE_ABSOLUTE,
  ldmaCtrlDstAddrModeRel = _LDMA_CH_CTRL_DSTMODE_RELATIVE
}
 Destination addressing mode.
 
enum  LDMA_LinkMode_t {
  ldmaLinkModeAbs = _LDMA_CH_LINK_LINKMODE_ABSOLUTE,
  ldmaLinkModeRel = _LDMA_CH_LINK_LINKMODE_RELATIVE
}
 DMA link load address mode.
 
enum  LDMA_CfgArbSlots_t {
  ldmaCfgArbSlotsAs1 = _LDMA_CH_CFG_ARBSLOTS_ONE,
  ldmaCfgArbSlotsAs2 = _LDMA_CH_CFG_ARBSLOTS_TWO,
  ldmaCfgArbSlotsAs4 = _LDMA_CH_CFG_ARBSLOTS_FOUR,
  ldmaCfgArbSlotsAs8 = _LDMA_CH_CFG_ARBSLOTS_EIGHT
}
 Insert extra arbitration slots to increase channel arbitration priority.
 
enum  LDMA_CfgSrcIncSign_t {
  ldmaCfgSrcIncSignPos = _LDMA_CH_CFG_SRCINCSIGN_POSITIVE,
  ldmaCfgSrcIncSignNeg = _LDMA_CH_CFG_SRCINCSIGN_NEGATIVE
}
 Source address increment sign.
 
enum  LDMA_CfgDstIncSign_t {
  ldmaCfgDstIncSignPos = _LDMA_CH_CFG_DSTINCSIGN_POSITIVE,
  ldmaCfgDstIncSignNeg = _LDMA_CH_CFG_DSTINCSIGN_NEGATIVE
}
 Destination address increment sign.
 
enum  LDMA_PeripheralSignal_t {
  ldmaPeripheralSignal_NONE = LDMAXBAR_CH_REQSEL_SOURCESEL_NONE,
  ldmaPeripheralSignal_LDMAXBAR_PRSREQ0 = LDMAXBAR_CH_REQSEL_SIGSEL_LDMAXBARPRSREQ0 | LDMAXBAR_CH_REQSEL_SOURCESEL_LDMAXBAR,
  ldmaPeripheralSignal_LDMAXBAR_PRSREQ1 = LDMAXBAR_CH_REQSEL_SIGSEL_LDMAXBARPRSREQ1 | LDMAXBAR_CH_REQSEL_SOURCESEL_LDMAXBAR,
  ldmaPeripheralSignal_TIMER0_CC0 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER0CC0 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER0,
  ldmaPeripheralSignal_TIMER0_CC1 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER0CC1 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER0,
  ldmaPeripheralSignal_TIMER0_CC2 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER0CC2 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER0,
  ldmaPeripheralSignal_TIMER0_UFOF = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER0UFOF | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER0,
  ldmaPeripheralSignal_TIMER1_CC0 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER1CC0 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER1,
  ldmaPeripheralSignal_TIMER1_CC1 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER1CC1 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER1,
  ldmaPeripheralSignal_TIMER1_CC2 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER1CC2 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER1,
  ldmaPeripheralSignal_TIMER1_UFOF = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER1UFOF | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER1,
  ldmaPeripheralSignal_USART0_RXDATAV = LDMAXBAR_CH_REQSEL_SIGSEL_USART0RXDATAV | LDMAXBAR_CH_REQSEL_SOURCESEL_USART0,
  ldmaPeripheralSignal_USART0_RXDATAVRIGHT = LDMAXBAR_CH_REQSEL_SIGSEL_USART0RXDATAVRIGHT | LDMAXBAR_CH_REQSEL_SOURCESEL_USART0,
  ldmaPeripheralSignal_USART0_TXBL = LDMAXBAR_CH_REQSEL_SIGSEL_USART0TXBL | LDMAXBAR_CH_REQSEL_SOURCESEL_USART0,
  ldmaPeripheralSignal_USART0_TXBLRIGHT = LDMAXBAR_CH_REQSEL_SIGSEL_USART0TXBLRIGHT | LDMAXBAR_CH_REQSEL_SOURCESEL_USART0,
  ldmaPeripheralSignal_USART0_TXEMPTY = LDMAXBAR_CH_REQSEL_SIGSEL_USART0TXEMPTY | LDMAXBAR_CH_REQSEL_SOURCESEL_USART0,
  ldmaPeripheralSignal_USART1_RXDATAV = LDMAXBAR_CH_REQSEL_SIGSEL_USART1RXDATAV | LDMAXBAR_CH_REQSEL_SOURCESEL_USART1,
  ldmaPeripheralSignal_USART1_RXDATAVRIGHT = LDMAXBAR_CH_REQSEL_SIGSEL_USART1RXDATAVRIGHT | LDMAXBAR_CH_REQSEL_SOURCESEL_USART1,
  ldmaPeripheralSignal_USART1_TXBL = LDMAXBAR_CH_REQSEL_SIGSEL_USART1TXBL | LDMAXBAR_CH_REQSEL_SOURCESEL_USART1,
  ldmaPeripheralSignal_USART1_TXBLRIGHT = LDMAXBAR_CH_REQSEL_SIGSEL_USART1TXBLRIGHT | LDMAXBAR_CH_REQSEL_SOURCESEL_USART1,
  ldmaPeripheralSignal_USART1_TXEMPTY = LDMAXBAR_CH_REQSEL_SIGSEL_USART1TXEMPTY | LDMAXBAR_CH_REQSEL_SOURCESEL_USART1,
  ldmaPeripheralSignal_USART2_RXDATAV = LDMAXBAR_CH_REQSEL_SIGSEL_USART2RXDATAV | LDMAXBAR_CH_REQSEL_SOURCESEL_USART2,
  ldmaPeripheralSignal_USART2_RXDATAVRIGHT = LDMAXBAR_CH_REQSEL_SIGSEL_USART2RXDATAVRIGHT | LDMAXBAR_CH_REQSEL_SOURCESEL_USART2,
  ldmaPeripheralSignal_USART2_TXBL = LDMAXBAR_CH_REQSEL_SIGSEL_USART2TXBL | LDMAXBAR_CH_REQSEL_SOURCESEL_USART2,
  ldmaPeripheralSignal_USART2_TXBLRIGHT = LDMAXBAR_CH_REQSEL_SIGSEL_USART2TXBLRIGHT | LDMAXBAR_CH_REQSEL_SOURCESEL_USART2,
  ldmaPeripheralSignal_USART2_TXEMPTY = LDMAXBAR_CH_REQSEL_SIGSEL_USART2TXEMPTY | LDMAXBAR_CH_REQSEL_SOURCESEL_USART2,
  ldmaPeripheralSignal_I2C0_RXDATAV = LDMAXBAR_CH_REQSEL_SIGSEL_I2C0RXDATAV | LDMAXBAR_CH_REQSEL_SOURCESEL_I2C0,
  ldmaPeripheralSignal_I2C0_TXBL = LDMAXBAR_CH_REQSEL_SIGSEL_I2C0TXBL | LDMAXBAR_CH_REQSEL_SOURCESEL_I2C0,
  ldmaPeripheralSignal_I2C1_RXDATAV = LDMAXBAR_CH_REQSEL_SIGSEL_I2C1RXDATAV | LDMAXBAR_CH_REQSEL_SOURCESEL_I2C1,
  ldmaPeripheralSignal_I2C1_TXBL = LDMAXBAR_CH_REQSEL_SIGSEL_I2C1TXBL | LDMAXBAR_CH_REQSEL_SOURCESEL_I2C1,
  ldmaPeripheralSignal_AGC_RSSI = LDMAXBAR_CH_REQSEL_SIGSEL_AGCRSSI | LDMAXBAR_CH_REQSEL_SOURCESEL_AGC,
  ldmaPeripheralSignal_PROTIMER_BOF = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERBOF | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_CC0 = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERCC0 | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_CC1 = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERCC1 | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_CC2 = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERCC2 | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_CC3 = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERCC3 | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_CC4 = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERCC4 | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_POF = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERPOF | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_PROTIMER_WOF = LDMAXBAR_CH_REQSEL_SIGSEL_PROTIMERWOF | LDMAXBAR_CH_REQSEL_SOURCESEL_PROTIMER,
  ldmaPeripheralSignal_MODEM_DEBUG = LDMAXBAR_CH_REQSEL_SIGSEL_MODEMDEBUG | LDMAXBAR_CH_REQSEL_SOURCESEL_MODEM,
  ldmaPeripheralSignal_IADC0_IADC_SCAN = LDMAXBAR_CH_REQSEL_SIGSEL_IADC0IADC_SCAN | LDMAXBAR_CH_REQSEL_SOURCESEL_IADC0,
  ldmaPeripheralSignal_IADC0_IADC_SINGLE = LDMAXBAR_CH_REQSEL_SIGSEL_IADC0IADC_SINGLE | LDMAXBAR_CH_REQSEL_SOURCESEL_IADC0,
  ldmaPeripheralSignal_MSC_WDATA = LDMAXBAR_CH_REQSEL_SIGSEL_MSCWDATA | LDMAXBAR_CH_REQSEL_SOURCESEL_MSC,
  ldmaPeripheralSignal_TIMER2_CC0 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER2CC0 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER2,
  ldmaPeripheralSignal_TIMER2_CC1 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER2CC1 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER2,
  ldmaPeripheralSignal_TIMER2_CC2 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER2CC2 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER2,
  ldmaPeripheralSignal_TIMER2_UFOF = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER2UFOF | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER2,
  ldmaPeripheralSignal_TIMER3_CC0 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER3CC0 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER3,
  ldmaPeripheralSignal_TIMER3_CC1 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER3CC1 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER3,
  ldmaPeripheralSignal_TIMER3_CC2 = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER3CC2 | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER3,
  ldmaPeripheralSignal_TIMER3_UFOF = LDMAXBAR_CH_REQSEL_SIGSEL_TIMER3UFOF | LDMAXBAR_CH_REQSEL_SOURCESEL_TIMER3
}
 Peripherals that can trigger LDMA transfers.
 

Function Documentation

◆ LDMA_DeInit()

void LDMA_DeInit ( void  )

De-initialize the LDMA controller.

LDMA interrupts are disabled and the LDMA clock is stopped.

◆ LDMA_EnableChannelRequest()

void LDMA_EnableChannelRequest ( int  ch,
bool  enable 
)

Enable or disable an LDMA channel request.

Use this function to enable or disable an LDMA channel request. This will prevent the LDMA from proceeding after its current transaction if disabled.

Parameters
[in]chLDMA channel to enable or disable requests.
[in]enableIf 'true', the request will be enabled. If 'false', the request will be disabled.

◆ LDMA_Init()

void LDMA_Init ( const LDMA_Init_t init)

Initialize the LDMA controller.

This function will disable all the LDMA channels and enable the LDMA bus clock in the CMU. This function will also enable the LDMA IRQ in the NVIC and set the LDMA IRQ priority to a user-configurable priority. The LDMA interrupt priority is configured using the LDMA_Init_t structure.

Note
Since this function enables the LDMA IRQ, always add a custom LDMA_IRQHandler to the application to handle any interrupts from LDMA.
Parameters
[in]initA pointer to the initialization structure used to configure the LDMA.

◆ LDMA_StartTransfer()

void LDMA_StartTransfer ( int  ch,
const LDMA_TransferCfg_t transfer,
const LDMA_Descriptor_t descriptor 
)

Start a DMA transfer.

Parameters
[in]chA DMA channel.
[in]transferThe initialization structure used to configure the transfer.
[in]descriptorThe transfer descriptor, which can be an array of descriptors linked together.

◆ LDMA_StopTransfer()

void LDMA_StopTransfer ( int  ch)

Stop a DMA transfer.

Note
The DMA will complete the current AHB burst transfer before stopping.
Parameters
[in]chA DMA channel to stop.

◆ LDMA_TransferDone()

bool LDMA_TransferDone ( int  ch)

Check if a DMA transfer has completed.

Parameters
[in]chA DMA channel to check.
Returns
True if transfer has completed, false if not.

◆ LDMA_TransferRemainingCount()

uint32_t LDMA_TransferRemainingCount ( int  ch)

Get the number of items remaining in a transfer.

Note
This function does not take into account that a DMA transfer with a chain of linked transfers might be ongoing. It will only check the count for the current transfer.
Parameters
[in]chThe channel number of the transfer to check.
Returns
A number of items remaining in the transfer.

◆ LDMA_ChannelEnabled()

bool LDMA_ChannelEnabled ( int  ch)
inline

Check if a certain channel is enabled.

Parameters
[in]chLDMA channel to check.
Returns
return true if the LDMA channel is enabled and false if the channel is not enabled.

◆ LDMA_IntClear()

void LDMA_IntClear ( uint32_t  flags)
inline

Clear one or more pending LDMA interrupts.

Parameters
[in]flagsPending LDMA interrupt sources to clear. Use one or more valid interrupt flags for the LDMA module. The flags are LDMA_IFC_ERROR and one done flag for each channel.

◆ LDMA_IntDisable()

void LDMA_IntDisable ( uint32_t  flags)
inline

Disable one or more LDMA interrupts.

Parameters
[in]flagsLDMA interrupt sources to disable. Use one or more valid interrupt flags for LDMA module. The flags are LDMA_IEN_ERROR and one done flag for each channel.

◆ LDMA_IntEnable()

void LDMA_IntEnable ( uint32_t  flags)
inline

Enable one or more LDMA interrupts.

Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using LDMA_IntClear() prior to enabling the interrupt.
Parameters
[in]flagsLDMA interrupt sources to enable. Use one or more valid interrupt flags for LDMA module. The flags are LDMA_IEN_ERROR and one done flag for each channel.

◆ LDMA_IntGet()

uint32_t LDMA_IntGet ( void  )
inline

Get pending LDMA interrupt flags.

Note
Event bits are not cleared by the use of this function.
Returns
LDMA interrupt sources pending. Returns one or more valid interrupt flags for LDMA module. The flags are LDMA_IF_ERROR and one flag for each LDMA channel.

◆ LDMA_IntGetEnabled()

uint32_t LDMA_IntGetEnabled ( void  )
inline

Get enabled and pending LDMA interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled LDMA interrupt sources Return value is the bitwise AND of
  • the enabled interrupt sources in LDMA_IEN and
  • the pending interrupt flags LDMA_IF

◆ LDMA_IntSet()

void LDMA_IntSet ( uint32_t  flags)
inline

Set one or more pending LDMA interrupts.

Parameters
[in]flagsLDMA interrupt sources to set to pending. Use one or more valid interrupt flags for LDMA module. The flags are LDMA_IFS_ERROR and one done flag for each LDMA channel.

Macro Definition Documentation

◆ LDMA_INIT_DEFAULT

#define LDMA_INIT_DEFAULT
Value:
{ \
.ldmaInitCtrlNumFixed = _LDMA_CTRL_NUMFIXED_DEFAULT,/* Fixed priority arbitration.*/ \
.ldmaInitCtrlSyncPrsClrEn = 0, /* No PRS Synctrig clear enable*/ \
.ldmaInitCtrlSyncPrsSetEn = 0, /* No PRS Synctrig set enable. */ \
.ldmaInitIrqPriority = 3 /* IRQ priority level 3. */ \
}

Default DMA initialization structure.

◆ LDMA_TRANSFER_CFG_MEMORY

#define LDMA_TRANSFER_CFG_MEMORY ( )
Value:
{ \
0, 0, 0, 0, 0, \
false, false, ldmaCfgArbSlotsAs1, \
ldmaCfgSrcIncSignPos, ldmaCfgDstIncSignPos, 0 \
}

Generic DMA transfer configuration for memory to memory transfers.

◆ LDMA_TRANSFER_CFG_MEMORY_LOOP

#define LDMA_TRANSFER_CFG_MEMORY_LOOP (   loopCnt)
Value:
{ \
0, 0, 0, 0, 0, \
false, false, ldmaCfgArbSlotsAs1, \
ldmaCfgSrcIncSignPos, ldmaCfgDstIncSignPos, \
loopCnt \
}

Generic DMA transfer configuration for looped memory to memory transfers.

◆ LDMA_TRANSFER_CFG_PERIPHERAL

#define LDMA_TRANSFER_CFG_PERIPHERAL (   signal)
Value:
{ \
signal, 0, 0, 0, 0, \
false, false, ldmaCfgArbSlotsAs1, \
ldmaCfgSrcIncSignPos, ldmaCfgDstIncSignPos, 0 \
}

Generic DMA transfer configuration for memory to/from peripheral transfers.

◆ LDMA_TRANSFER_CFG_PERIPHERAL_LOOP

#define LDMA_TRANSFER_CFG_PERIPHERAL_LOOP (   signal,
  loopCnt 
)
Value:
{ \
signal, 0, 0, 0, 0, \
false, false, ldmaCfgArbSlotsAs1, \
ldmaCfgSrcIncSignPos, ldmaCfgDstIncSignPos, loopCnt \
}

Generic DMA transfer configuration for looped memory to/from peripheral transfers.

◆ LDMA_DESCRIPTOR_SINGLE_M2M_WORD

#define LDMA_DESCRIPTOR_SINGLE_M2M_WORD (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeWord, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for single memory to memory word transfer.

Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of words to transfer.

◆ LDMA_DESCRIPTOR_SINGLE_M2M_HALF

#define LDMA_DESCRIPTOR_SINGLE_M2M_HALF (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeHalf, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for single memory to memory half-word transfer.

Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of half-words to transfer.

◆ LDMA_DESCRIPTOR_SINGLE_M2M_BYTE

#define LDMA_DESCRIPTOR_SINGLE_M2M_BYTE (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for single memory to memory byte transfer.

Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of bytes to transfer.

◆ LDMA_DESCRIPTOR_LINKABS_M2M_WORD

#define LDMA_DESCRIPTOR_LINKABS_M2M_WORD (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 0, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeWord, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeAbs, \
.link = 1, \
.linkAddr = 0 /* Must be set runtime ! */ \
} \
}

DMA descriptor initializer for linked memory to memory word transfer.

Link address must be an absolute address.

Note
The linkAddr member of the transfer descriptor is not initialized.
Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of words to transfer.

◆ LDMA_DESCRIPTOR_LINKABS_M2M_HALF

#define LDMA_DESCRIPTOR_LINKABS_M2M_HALF (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 0, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeHalf, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeAbs, \
.link = 1, \
.linkAddr = 0 /* Must be set runtime ! */ \
} \
}

DMA descriptor initializer for linked memory to memory half-word transfer.

Link address must be an absolute address.

Note
The linkAddr member of the transfer descriptor is not initialized.
Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of half-words to transfer.

◆ LDMA_DESCRIPTOR_LINKABS_M2M_BYTE

#define LDMA_DESCRIPTOR_LINKABS_M2M_BYTE (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 0, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeAbs, \
.link = 1, \
.linkAddr = 0 /* Must be set runtime ! */ \
} \
}

DMA descriptor initializer for linked memory to memory byte transfer.

Link address must be an absolute address.

Note
The linkAddr member of the transfer descriptor is not initialized.
Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of bytes to transfer.

◆ LDMA_DESCRIPTOR_LINKREL_M2M_WORD

#define LDMA_DESCRIPTOR_LINKREL_M2M_WORD (   src,
  dest,
  count,
  linkjmp 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 0, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeWord, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for linked memory to memory word transfer.

Link address is a relative address.

Note
The linkAddr member of the transfer descriptor is initialized to 4, assuming that the next descriptor immediately follows this descriptor (in memory).
Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of words to transfer.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_LINKREL_M2M_HALF

#define LDMA_DESCRIPTOR_LINKREL_M2M_HALF (   src,
  dest,
  count,
  linkjmp 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 0, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeHalf, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for linked memory to memory half-word transfer.

Link address is a relative address.

Note
The linkAddr member of transfer descriptor is initialized to 4, assuming that the next descriptor immediately follows this descriptor (in memory).
Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of half-words to transfer.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_LINKREL_M2M_BYTE

#define LDMA_DESCRIPTOR_LINKREL_M2M_BYTE (   src,
  dest,
  count,
  linkjmp 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 1, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 0, \
.reqMode = ldmaCtrlReqModeAll, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for linked memory to memory byte transfer.

Link address is a relative address.

Note
The linkAddr member of transfer descriptor is initialized to 4, assuming that the next descriptor immediately follows this descriptor (in memory).
Parameters
[in]srcSource data address.
[in]destDestination data address.
[in]countNumber of bytes to transfer.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_SINGLE_P2M_BYTE

#define LDMA_DESCRIPTOR_SINGLE_P2M_BYTE (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 0, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeBlock, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncNone, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for byte transfers from a peripheral to memory.

Parameters
[in]srcPeripheral data source register address.
[in]destDestination data address.
[in]countNumber of bytes to transfer.

◆ LDMA_DESCRIPTOR_SINGLE_P2P_BYTE

#define LDMA_DESCRIPTOR_SINGLE_P2P_BYTE (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 0, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeBlock, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncNone, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncNone, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for byte transfers from a peripheral to a peripheral.

Parameters
[in]srcPeripheral data source register address.
[in]destPeripheral data destination register address.
[in]countNumber of bytes to transfer.

◆ LDMA_DESCRIPTOR_SINGLE_M2P_BYTE

#define LDMA_DESCRIPTOR_SINGLE_M2P_BYTE (   src,
  dest,
  count 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 0, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeBlock, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncNone, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for byte transfers from memory to a peripheral.

Parameters
[in]srcSource data address.
[in]destPeripheral data register destination address.
[in]countNumber of bytes to transfer.

◆ LDMA_DESCRIPTOR_LINKREL_P2M_BYTE

#define LDMA_DESCRIPTOR_LINKREL_P2M_BYTE (   src,
  dest,
  count,
  linkjmp 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 0, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeBlock, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncNone, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for byte transfers from a peripheral to memory.

Parameters
[in]srcPeripheral data source register address.
[in]destDestination data address.
[in]countNumber of bytes to transfer.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_LINKREL_P2M_WORD

#define LDMA_DESCRIPTOR_LINKREL_P2M_WORD (   src,
  dest,
  count,
  linkjmp 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 0, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeBlock, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncNone, \
.size = ldmaCtrlSizeWord, \
.dstInc = ldmaCtrlDstIncOne, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for word transfers from a peripheral to memory.

Parameters
[in]srcPeripheral data source register address.
[in]destDestination data address.
[in]countNumber of words to transfer.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_LINKREL_M2P_BYTE

#define LDMA_DESCRIPTOR_LINKREL_M2P_BYTE (   src,
  dest,
  count,
  linkjmp 
)
Value:
{ \
.xfer = \
{ \
.structType = ldmaCtrlStructTypeXfer, \
.structReq = 0, \
.xferCnt = (count) - 1, \
.byteSwap = 0, \
.blockSize = ldmaCtrlBlockSizeUnit1, \
.doneIfs = 1, \
.reqMode = ldmaCtrlReqModeBlock, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = ldmaCtrlSrcIncOne, \
.size = ldmaCtrlSizeByte, \
.dstInc = ldmaCtrlDstIncNone, \
.srcAddrMode = ldmaCtrlSrcAddrModeAbs, \
.dstAddrMode = ldmaCtrlDstAddrModeAbs, \
.srcAddr = (uint32_t)(src), \
.dstAddr = (uint32_t)(dest), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for byte transfers from memory to a peripheral.

Parameters
[in]srcSource data address.
[in]destPeripheral data register destination address.
[in]countNumber of bytes to transfer.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_SINGLE_WRITE

#define LDMA_DESCRIPTOR_SINGLE_WRITE (   value,
  address 
)
Value:
{ \
.wri = \
{ \
.structType = ldmaCtrlStructTypeWrite, \
.structReq = 1, \
.xferCnt = 0, \
.byteSwap = 0, \
.blockSize = 0, \
.doneIfs = 1, \
.reqMode = 0, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = 0, \
.size = 0, \
.dstInc = 0, \
.srcAddrMode = 0, \
.dstAddrMode = 0, \
.immVal = (value), \
.dstAddr = (uint32_t)(address), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for Immediate WRITE transfer.

Parameters
[in]valueImmediate value to write.
[in]addressWrite address.

◆ LDMA_DESCRIPTOR_LINKABS_WRITE

#define LDMA_DESCRIPTOR_LINKABS_WRITE (   value,
  address 
)
Value:
{ \
.wri = \
{ \
.structType = ldmaCtrlStructTypeWrite, \
.structReq = 1, \
.xferCnt = 0, \
.byteSwap = 0, \
.blockSize = 0, \
.doneIfs = 0, \
.reqMode = 0, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = 0, \
.size = 0, \
.dstInc = 0, \
.srcAddrMode = 0, \
.dstAddrMode = 0, \
.immVal = (value), \
.dstAddr = (uint32_t)(address), \
.linkMode = ldmaLinkModeAbs, \
.link = 1, \
.linkAddr = 0 /* Must be set runtime ! */ \
} \
}

DMA descriptor initializer for Immediate WRITE transfer.

Link address must be an absolute address.

Note
The linkAddr member of the transfer descriptor is not initialized.
Parameters
[in]valueImmediate value to write.
[in]addressWrite address.

◆ LDMA_DESCRIPTOR_LINKREL_WRITE

#define LDMA_DESCRIPTOR_LINKREL_WRITE (   value,
  address,
  linkjmp 
)
Value:
{ \
.wri = \
{ \
.structType = ldmaCtrlStructTypeWrite, \
.structReq = 1, \
.xferCnt = 0, \
.byteSwap = 0, \
.blockSize = 0, \
.doneIfs = 0, \
.reqMode = 0, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = 0, \
.size = 0, \
.dstInc = 0, \
.srcAddrMode = 0, \
.dstAddrMode = 0, \
.immVal = (value), \
.dstAddr = (uint32_t)(address), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for Immediate WRITE transfer.

Parameters
[in]valueImmediate value to write.
[in]addressWrite address.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

◆ LDMA_DESCRIPTOR_SINGLE_SYNC

#define LDMA_DESCRIPTOR_SINGLE_SYNC (   set,
  clr,
  matchValue,
  matchEnable 
)
Value:
{ \
.sync = \
{ \
.structType = ldmaCtrlStructTypeSync, \
.structReq = 1, \
.xferCnt = 0, \
.byteSwap = 0, \
.blockSize = 0, \
.doneIfs = 1, \
.reqMode = 0, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = 0, \
.size = 0, \
.dstInc = 0, \
.srcAddrMode = 0, \
.dstAddrMode = 0, \
.syncSet = (set), \
.syncClr = (clr), \
.matchVal = (matchValue), \
.matchEn = (matchEnable), \
.linkMode = 0, \
.link = 0, \
.linkAddr = 0 \
} \
}

DMA descriptor initializer for SYNC transfer.

Parameters
[in]setSync pattern bits to set.
[in]clrSync pattern bits to clear.
[in]matchValueSync pattern to match.
[in]matchEnableSync pattern bits to enable for match.

◆ LDMA_DESCRIPTOR_LINKABS_SYNC

#define LDMA_DESCRIPTOR_LINKABS_SYNC (   set,
  clr,
  matchValue,
  matchEnable 
)
Value:
{ \
.sync = \
{ \
.structType = ldmaCtrlStructTypeSync, \
.structReq = 1, \
.xferCnt = 0, \
.byteSwap = 0, \
.blockSize = 0, \
.doneIfs = 0, \
.reqMode = 0, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = 0, \
.size = 0, \
.dstInc = 0, \
.srcAddrMode = 0, \
.dstAddrMode = 0, \
.syncSet = (set), \
.syncClr = (clr), \
.matchVal = (matchValue), \
.matchEn = (matchEnable), \
.linkMode = ldmaLinkModeAbs, \
.link = 1, \
.linkAddr = 0 /* Must be set runtime ! */ \
} \
}

DMA descriptor initializer for SYNC transfer.

Link address must be an absolute address.

Note
The linkAddr member of the transfer descriptor is not initialized.
Parameters
[in]setSync pattern bits to set.
[in]clrSync pattern bits to clear.
[in]matchValueSync pattern to match.
[in]matchEnableSync pattern bits to enable for match.

◆ LDMA_DESCRIPTOR_LINKREL_SYNC

#define LDMA_DESCRIPTOR_LINKREL_SYNC (   set,
  clr,
  matchValue,
  matchEnable,
  linkjmp 
)
Value:
{ \
.sync = \
{ \
.structType = ldmaCtrlStructTypeSync, \
.structReq = 1, \
.xferCnt = 0, \
.byteSwap = 0, \
.blockSize = 0, \
.doneIfs = 0, \
.reqMode = 0, \
.decLoopCnt = 0, \
.ignoreSrec = 0, \
.srcInc = 0, \
.size = 0, \
.dstInc = 0, \
.srcAddrMode = 0, \
.dstAddrMode = 0, \
.syncSet = (set), \
.syncClr = (clr), \
.matchVal = (matchValue), \
.matchEn = (matchEnable), \
.linkMode = ldmaLinkModeRel, \
.link = 1, \
.linkAddr = (linkjmp) * 4 \
} \
}

DMA descriptor initializer for SYNC transfer.

Parameters
[in]setSync pattern bits to set.
[in]clrSync pattern bits to clear.
[in]matchValueSync pattern to match.
[in]matchEnableSync pattern bits to enable for match.
[in]linkjmpAddress of descriptor to link to, expressed as a signed number of descriptors from "here". 1=one descriptor forward in memory, 0=this descriptor, -1=one descriptor back in memory.

Enumeration Type Documentation

◆ LDMA_CtrlBlockSize_t

Controls the number of unit data transfers per arbitration cycle, providing a means to balance DMA channels' load on the controller.

Enumerator
ldmaCtrlBlockSizeUnit1 

One transfer per arbitration.


ldmaCtrlBlockSizeUnit2 

Two transfers per arbitration.


ldmaCtrlBlockSizeUnit3 

Three transfers per arbitration.


ldmaCtrlBlockSizeUnit4 

Four transfers per arbitration.


ldmaCtrlBlockSizeUnit6 

Six transfers per arbitration.


ldmaCtrlBlockSizeUnit8 

Eight transfers per arbitration.


ldmaCtrlBlockSizeUnit16 

16 transfers per arbitration.


ldmaCtrlBlockSizeUnit32 

32 transfers per arbitration.


ldmaCtrlBlockSizeUnit64 

64 transfers per arbitration.


ldmaCtrlBlockSizeUnit128 

128 transfers per arbitration.


ldmaCtrlBlockSizeUnit256 

256 transfers per arbitration.


ldmaCtrlBlockSizeUnit512 

512 transfers per arbitration.


ldmaCtrlBlockSizeUnit1024 

1024 transfers per arbitration.


ldmaCtrlBlockSizeAll 

Lock arbitration during transfer.

◆ LDMA_CtrlStructType_t

DMA structure type.

Enumerator
ldmaCtrlStructTypeXfer 

TRANSFER transfer type.


ldmaCtrlStructTypeSync 

SYNCHRONIZE transfer type.

ldmaCtrlStructTypeWrite 

WRITE transfer type.


◆ LDMA_CtrlReqMode_t

DMA transfer block or cycle selector.

Enumerator
ldmaCtrlReqModeBlock 

Each DMA request trigger transfer of one block.


ldmaCtrlReqModeAll 

A DMA request trigger transfer of a complete cycle.

◆ LDMA_CtrlSrcInc_t

Source address increment unit size.

Enumerator
ldmaCtrlSrcIncOne 

Increment source address by one unit data size.


ldmaCtrlSrcIncTwo 

Increment source address by two unit data sizes.


ldmaCtrlSrcIncFour 

Increment source address by four unit data sizes.

ldmaCtrlSrcIncNone 

Do not increment source address.


◆ LDMA_CtrlSize_t

DMA transfer unit size.

Enumerator
ldmaCtrlSizeByte 

Each unit transfer is a byte.


ldmaCtrlSizeHalf 

Each unit transfer is a half-word.

ldmaCtrlSizeWord 

Each unit transfer is a word.


◆ LDMA_CtrlDstInc_t

Destination address increment unit size.

Enumerator
ldmaCtrlDstIncOne 

Increment destination address by one unit data size.


ldmaCtrlDstIncTwo 

Increment destination address by two unit data sizes.


ldmaCtrlDstIncFour 

Increment destination address by four unit data sizes.

ldmaCtrlDstIncNone 

Do not increment destination address.


◆ LDMA_CtrlSrcAddrMode_t

Source addressing mode.

Enumerator
ldmaCtrlSrcAddrModeAbs 

Address fetched from a linked structure is absolute.


ldmaCtrlSrcAddrModeRel 

Address fetched from a linked structure is relative.


◆ LDMA_CtrlDstAddrMode_t

Destination addressing mode.

Enumerator
ldmaCtrlDstAddrModeAbs 

Address fetched from a linked structure is absolute.


ldmaCtrlDstAddrModeRel 

Address fetched from a linked structure is relative.


◆ LDMA_LinkMode_t

DMA link load address mode.

Enumerator
ldmaLinkModeAbs 

Link address is an absolute address value.


ldmaLinkModeRel 

Link address is a two's complement relative address.


◆ LDMA_CfgArbSlots_t

Insert extra arbitration slots to increase channel arbitration priority.

Enumerator
ldmaCfgArbSlotsAs1 

One arbitration slot selected.


ldmaCfgArbSlotsAs2 

Two arbitration slots selected.


ldmaCfgArbSlotsAs4 

Four arbitration slots selected.


ldmaCfgArbSlotsAs8 

Eight arbitration slots selected.

◆ LDMA_CfgSrcIncSign_t

Source address increment sign.

Enumerator
ldmaCfgSrcIncSignPos 

Increment source address.

ldmaCfgSrcIncSignNeg 

Decrement source address.

◆ LDMA_CfgDstIncSign_t

Destination address increment sign.

Enumerator
ldmaCfgDstIncSignPos 

Increment destination address.

ldmaCfgDstIncSignNeg 

Decrement destination address.

◆ LDMA_PeripheralSignal_t

Peripherals that can trigger LDMA transfers.

Enumerator
ldmaPeripheralSignal_NONE 

No peripheral selected for DMA triggering.

ldmaPeripheralSignal_LDMAXBAR_PRSREQ0 

Trigger on PRS REQ0.

ldmaPeripheralSignal_LDMAXBAR_PRSREQ1 

Trigger on PRS REQ1.

ldmaPeripheralSignal_TIMER0_CC0 

Trigger on TIMER0_CC0.

ldmaPeripheralSignal_TIMER0_CC1 

Trigger on TIMER0_CC1.

ldmaPeripheralSignal_TIMER0_CC2 

Trigger on TIMER0_CC2.

ldmaPeripheralSignal_TIMER0_UFOF 

Trigger on TIMER0_UFOF.

ldmaPeripheralSignal_TIMER1_CC0 

Trigger on TIMER1_CC0.

ldmaPeripheralSignal_TIMER1_CC1 

Trigger on TIMER1_CC1.

ldmaPeripheralSignal_TIMER1_CC2 

Trigger on TIMER1_CC2.

ldmaPeripheralSignal_TIMER1_UFOF 

Trigger on TIMER1_UFOF.

ldmaPeripheralSignal_USART0_RXDATAV 

Trigger on USART0_RXDATAV.

ldmaPeripheralSignal_USART0_RXDATAVRIGHT 

Trigger on USART0_RXDATAVRIGHT.

ldmaPeripheralSignal_USART0_TXBL 

Trigger on USART0_TXBL.

ldmaPeripheralSignal_USART0_TXBLRIGHT 

Trigger on USART0_TXBLRIGHT.

ldmaPeripheralSignal_USART0_TXEMPTY 

Trigger on USART0_TXEMPTY.

ldmaPeripheralSignal_USART1_RXDATAV 

Trigger on USART1_RXDATAV.

ldmaPeripheralSignal_USART1_RXDATAVRIGHT 

Trigger on USART1_RXDATAVRIGHT.

ldmaPeripheralSignal_USART1_TXBL 

Trigger on USART1_TXBL.

ldmaPeripheralSignal_USART1_TXBLRIGHT 

Trigger on USART1_TXBLRIGHT.

ldmaPeripheralSignal_USART1_TXEMPTY 

Trigger on USART1_TXEMPTY.

ldmaPeripheralSignal_USART2_RXDATAV 

Trigger on USART2_RXDATAV.

ldmaPeripheralSignal_USART2_RXDATAVRIGHT 

Trigger on USART2_RXDATAVRIGHT.

ldmaPeripheralSignal_USART2_TXBL 

Trigger on USART2_TXBL.

ldmaPeripheralSignal_USART2_TXBLRIGHT 

Trigger on USART2_TXBLRIGHT.

ldmaPeripheralSignal_USART2_TXEMPTY 

Trigger on USART2_TXEMPTY.

ldmaPeripheralSignal_I2C0_RXDATAV 

Trigger on I2C0_RXDATAV.

ldmaPeripheralSignal_I2C0_TXBL 

Trigger on I2C0_TXBL.

ldmaPeripheralSignal_I2C1_RXDATAV 

Trigger on I2C1_RXDATAV.

ldmaPeripheralSignal_I2C1_TXBL 

Trigger on I2C1_TXBL.

ldmaPeripheralSignal_AGC_RSSI 

Trigger on AGC_RSSI.

ldmaPeripheralSignal_PROTIMER_BOF 

Trigger on PROTIMER_BOF.

ldmaPeripheralSignal_PROTIMER_CC0 

Trigger on PROTIMER_CC0.

ldmaPeripheralSignal_PROTIMER_CC1 

Trigger on PROTIMER_CC1.

ldmaPeripheralSignal_PROTIMER_CC2 

Trigger on PROTIMER_CC2.

ldmaPeripheralSignal_PROTIMER_CC3 

Trigger on PROTIMER_CC3.

ldmaPeripheralSignal_PROTIMER_CC4 

Trigger on PROTIMER_CC4.

ldmaPeripheralSignal_PROTIMER_POF 

Trigger on PROTIMER_POF.

ldmaPeripheralSignal_PROTIMER_WOF 

Trigger on PROTIMER_WOF.

ldmaPeripheralSignal_MODEM_DEBUG 

Trigger on MODEM_DEBUG.

ldmaPeripheralSignal_IADC0_IADC_SCAN 

Trigger on IADC0_IADC_SCAN.

ldmaPeripheralSignal_IADC0_IADC_SINGLE 

Trigger on IADC0_IADC_SINGLE.

ldmaPeripheralSignal_MSC_WDATA 

Trigger on MSC_WDATA.

ldmaPeripheralSignal_TIMER2_CC0 

Trigger on TIMER2_CC0.

ldmaPeripheralSignal_TIMER2_CC1 

Trigger on TIMER2_CC1.

ldmaPeripheralSignal_TIMER2_CC2 

Trigger on TIMER2_CC2.

ldmaPeripheralSignal_TIMER2_UFOF 

Trigger on TIMER2_UFOF.

ldmaPeripheralSignal_TIMER3_CC0 

Trigger on TIMER3_CC0.

ldmaPeripheralSignal_TIMER3_CC1 

Trigger on TIMER3_CC1.

ldmaPeripheralSignal_TIMER3_CC2 

Trigger on TIMER3_CC2.

ldmaPeripheralSignal_TIMER3_UFOF 

Trigger on TIMER3_UFOF.