// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
You should avoid using it in production. ... Functions sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables sl_iostream_t * sl_iostream_rtt_handle ... ) RTT Stream init. Returns
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... is the recommended device independent crypto API and should be used whenever possible ... sl_se_otp_init_t otp_settings_init = SL_SE_OTP_INIT_DEFAULT;
The ZG28 is an ideal platform for Z-Wave applications that require more Flash, RAM and ... names in our industry share and discover the latest trends and technologies that are making our lives ...
ProductWirelessResource TypeProduct Category Page
Results 1-5 of 5 for gecko-platform/latest/middleware/api/struct-b-m-p-header