// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Note that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... Device configuration and utilities (Utilities) ... Reset The device is reset. 7
You can configure the number and size of the ring buffers at compile-time in SEGGER_RTT_Conf.h configuration file. Please refer to Segger's documentation for further information on RTT.
ProductMicrocontrollersResource TypeSoftware API documentation
https://docs.silabs.com/gecko-platform/latest/middleware/api/group-glib https://docs.silabs.com/gecko-platform/ ... Device Init component adds autogen files and function calls to project:
Configuration Options The API Flow Control Support ... [in] type Abort type – whether to abort only Tx, only Rx, or both. ... The UARTDRV device handle used to start the transfer.
ProductMicrocontrollersResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/latest/middleware/api/struct-u-s-b-h-device-type-def