Legacy HAL

Description

Legacy HAL API.

Modules

Application Bootloader Interface
Definition of the application bootloader interface.
 
Common Bootloader
Common bootloader interface defines and functions.
 
Cyclic Redundancy Check
Functions that provide access to cyclic redundancy code (CRC) calculation. See crc.h for source code.
 
Diagnostics
Crash and watchdog diagnostic functions.
 
LED
Sample API funtions for controlling LEDs.
 
Microcontroller functions
Microcontroller functions.
 
Random Numbers
Functions that provide access to random numbers.
 
Reset Cause Definitions
Definitions for all the reset cause types.
 
SimEE2 to NVM3 Upgrade
 
Simulated EEPROM 1 and 2
Simulated EEPROM 1 and 2 legacy storage.
 
Standalone Bootloader
Definition of the standalone bootloader interface.
 

Data Structures

struct  HalEepromInformationType
 This structure defines a variety of information about the attached external EEPROM device.
 
struct  EepromStateType
 

Functions

const HalEepromInformationTypehalEepromInfo (void)
 Call this function to get information about the external EEPROM and its capabilities.
 
uint16_t halCommonGetInt16uMillisecondTick (void)
 
uint32_t halCommonGetInt32uMillisecondTick (void)
 
uint64_t halCommonGetInt64uMillisecondTick (void)
 
uint16_t halCommonGetInt16uQuarterSecondTick (void)
 
uint16_t halInternalStartSystemTimer (void)
 
void halCommonDelayMicroseconds (uint16_t us)
 
void halCommonDelayMilliseconds (uint16_t ms)
 
void halStackSymbolDelayAIsr (void)
 
void halStackRadioPowerMainControl (bool powerUp)
 
void halStackRadioPowerUpBoard (void)
 
void halStackRadioPowerDownBoard (void)
 
void halStackProcessBootCount (void)
 
EmberStatus emDebugInit (void)
 
void emRadioSeedRandom (void)
 

Macros

#define EEPROM_PAGE_SIZE   (128ul)
 Definition of an EEPROM page size, in bytes.
 
#define EEPROM_FIRST_PAGE   (0)
 Define the location of the first page in EEPROM.
 
#define EEPROM_IMAGE_START   (EEPROM_FIRST_PAGE * EEPROM_PAGE_SIZE)
 Define the location of the image start in EEPROM as a function of the EEPROM_FIRST_PAGE and EEPROM_PAGE_SIZE.
 
#define EEPROM_SUCCESS   0U
 Define EEPROM success status.
 
#define EEPROM_ERR   1U
 Define EEPROM error status.
 
#define EEPROM_ERR_MASK   0x80U
 Define EEPROM error mask.
 
#define EEPROM_ERR_PG_BOUNDARY   0x81U
 Define EEPROM page boundary error.
 
#define EEPROM_ERR_PG_SZ   0x82U
 Define EEPROM page size error.
 
#define EEPROM_ERR_WRT_DATA   0x83U
 Define EEPROM write data error.
 
#define EEPROM_ERR_IMG_SZ   0x84U
 Define EEPROM image too large error.
 
#define EEPROM_ERR_ADDR   0x85U
 Define EEPROM invalid address error.
 
#define EEPROM_ERR_INVALID_CHIP   0x86U
 Define EEPROM chip initialization error.
 
#define EEPROM_ERR_ERASE_REQUIRED   0x87U
 Define EEPROM erase required error.
 
#define EEPROM_ERR_NO_ERASE_SUPPORT   0x88U
 Define EEPROM error for no erase support.
 
#define EEPROM_INFO_VERSION   (0x0202)
 The current version of the HalEepromInformationType data structure.
 
#define EEPROM_INFO_MAJOR_VERSION   (0x0200)
 
#define EEPROM_INFO_MAJOR_VERSION_MASK   (0xFF00)
 
#define EEPROM_INFO_MIN_VERSION_WITH_WORD_SIZE_SUPPORT   0x0102U
 
#define EEPROM_CAPABILITIES_ERASE_SUPPORTED   (0x0001U)
 Eeprom capabilites mask that indicates the erase API is supported.
 
#define EEPROM_CAPABILITIES_PAGE_ERASE_REQD   (0x0002U)
 Eeprom capabilites mask that indicates page erasing is required before new data can be written to a device.
 
#define EEPROM_CAPABILITIES_BLOCKING_WRITE   (0x0004U)
 Eeprom capabilites mask that indicates that the write routine is blocking on this device.
 
#define EEPROM_CAPABILITIES_BLOCKING_ERASE   (0x0008U)
 Eeprom capabilites mask that indicates that the erase routine is blocking on this device.
 
#define EEPROM_CAPABILITIES_PART_ERASE_SECONDS   (0x0010U)
 Eeprom capabilities mask that indicateds that the partEraseTime field of HalEepromInformationType is in seconds instead of the usual millisecondss.
 
#define simulatedTimePasses()
 

Function Documentation

◆ halEepromInfo()

const HalEepromInformationType* halEepromInfo ( void  )

Call this function to get information about the external EEPROM and its capabilities.

The format of this call must not be altered. However, the content can be changed to work with a different device.

Returns
A pointer to a HalEepromInformationType data structure, or NULL if the driver does not support this API

Macro Definition Documentation

◆ EEPROM_PAGE_SIZE

#define EEPROM_PAGE_SIZE   (128ul)

Definition of an EEPROM page size, in bytes.

This definition is deprecated, and should no longer be used.

◆ EEPROM_FIRST_PAGE

#define EEPROM_FIRST_PAGE   (0)

Define the location of the first page in EEPROM.

This definition is deprecated, and should no longer be used.

◆ EEPROM_IMAGE_START

#define EEPROM_IMAGE_START   (EEPROM_FIRST_PAGE * EEPROM_PAGE_SIZE)

Define the location of the image start in EEPROM as a function of the EEPROM_FIRST_PAGE and EEPROM_PAGE_SIZE.

This definition is deprecated, and should no longer be used.

◆ EEPROM_SUCCESS

#define EEPROM_SUCCESS   0U

Define EEPROM success status.

◆ EEPROM_ERR

#define EEPROM_ERR   1U

Define EEPROM error status.

◆ EEPROM_ERR_MASK

#define EEPROM_ERR_MASK   0x80U

Define EEPROM error mask.

◆ EEPROM_ERR_PG_BOUNDARY

#define EEPROM_ERR_PG_BOUNDARY   0x81U

Define EEPROM page boundary error.

◆ EEPROM_ERR_PG_SZ

#define EEPROM_ERR_PG_SZ   0x82U

Define EEPROM page size error.

◆ EEPROM_ERR_WRT_DATA

#define EEPROM_ERR_WRT_DATA   0x83U

Define EEPROM write data error.

◆ EEPROM_ERR_IMG_SZ

#define EEPROM_ERR_IMG_SZ   0x84U

Define EEPROM image too large error.

◆ EEPROM_ERR_ADDR

#define EEPROM_ERR_ADDR   0x85U

Define EEPROM invalid address error.

◆ EEPROM_ERR_INVALID_CHIP

#define EEPROM_ERR_INVALID_CHIP   0x86U

Define EEPROM chip initialization error.

◆ EEPROM_ERR_ERASE_REQUIRED

#define EEPROM_ERR_ERASE_REQUIRED   0x87U

Define EEPROM erase required error.

◆ EEPROM_ERR_NO_ERASE_SUPPORT

#define EEPROM_ERR_NO_ERASE_SUPPORT   0x88U

Define EEPROM error for no erase support.

◆ EEPROM_INFO_VERSION

#define EEPROM_INFO_VERSION   (0x0202)

The current version of the HalEepromInformationType data structure.

◆ EEPROM_CAPABILITIES_ERASE_SUPPORTED

#define EEPROM_CAPABILITIES_ERASE_SUPPORTED   (0x0001U)

Eeprom capabilites mask that indicates the erase API is supported.

◆ EEPROM_CAPABILITIES_PAGE_ERASE_REQD

#define EEPROM_CAPABILITIES_PAGE_ERASE_REQD   (0x0002U)

Eeprom capabilites mask that indicates page erasing is required before new data can be written to a device.

◆ EEPROM_CAPABILITIES_BLOCKING_WRITE

#define EEPROM_CAPABILITIES_BLOCKING_WRITE   (0x0004U)

Eeprom capabilites mask that indicates that the write routine is blocking on this device.

◆ EEPROM_CAPABILITIES_BLOCKING_ERASE

#define EEPROM_CAPABILITIES_BLOCKING_ERASE   (0x0008U)

Eeprom capabilites mask that indicates that the erase routine is blocking on this device.

◆ EEPROM_CAPABILITIES_PART_ERASE_SECONDS

#define EEPROM_CAPABILITIES_PART_ERASE_SECONDS   (0x0010U)

Eeprom capabilities mask that indicateds that the partEraseTime field of HalEepromInformationType is in seconds instead of the usual millisecondss.