You are viewing documentation for version: 4.1 (latest) | Version History
◆ psa_drv_se_init_t
A driver initialization function.
- Parameters
-
[in,out] | drv_context | The driver context structure. |
[in,out] | persistent_data | A pointer to the persistent data that allows writing. |
| location | The location value for which this driver is registered. The driver will be invoked for all keys whose lifetime is in this location. |
- Return values
-
PSA_SUCCESS | The driver is operational. The core will update the persistent data in storage. |
- Returns
- Any other return value prevents the driver from being used in this session. The core will NOT update the persistent data in storage.
◆ psa_key_slot_number_t
An internal designation of a key slot between the core part of the PSA Crypto implementation and the driver.
The meaning of this value is driver-dependent.