Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... To update a Gecko OS device using Gecko OS, you need to sign up for an account with the ...
ProductWirelessResource TypeSoftware API documentation
... application (e.g., putting them below FreeRTOS OS atomic for access to OS functions in RAIL callbacks). ... in the release at platform/Device/SiliconLabs/<chipFamily>/Include/<chipFamily>_prs_ ...
Example Example usage. Alphabetical List of Commands ... os pins can only use the strong drive strength. ... Returns the RSSI value from the latest received packet of the current active ...
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/service/api/structsl-cli-command-info-t