// Bluetooth LE//Version 5.0 //API Reference ... _report and sl_bt_evt_scanner_extended_advertisement_report events Data Structures struct ... Value 0 indicates no periodic advertising.
// Bluetooth LE//Version 3.1 //General ... Bluetooth 4.2 specifies the PHY bitrate to be exactly 1 Mbps. ... Data packets, however, must be aligned so that the first packet starts at the start ...
0: Bonding request does not need to be confirmed ... Data includes remote device address and address type as well as security mode for ... address The Bluetooth device address uint32_t *
0 dBm is enough to cover about 10 to 15 m range, based on tests made with iBeacon example and Android ... Bluetooth 5 introduced 2M PHY for faster throughput and higher energy efficiency.
// Bluetooth LE//Version 5.0 //API Reference ... Bits 0 - 2: Highest 3 bits of the data payload length field Bits 3 - 5: Device type Bit value 100: Bluetooth LE Bit value 101: Bluetooth Mesh