Silicon Labs IoT Security Developer's Guide#
The IoT Security Developer's Guide offers detailed information on how to implement each of the device security features. This content is applicable to any protocol that supports the feature described. Additional protocol-specific information for Bluetooth, Bluetooth Mesh, OpenThread, and Zigbee is available in the protocol-specific section.
Series 2 and Series 3 Secure Debug: Explains the different debug lock and unlock features available in Series 2 and Series 3 devices and their capabilities.
Series 2 Secure Boot with RTSL: Describes the design of Secure Boot with RTSL (Root of Trust and Secure Loader) on Series 2 and Series 3 devices. It also provides examples of how to implement the Secure Boot process.
Series 2 TrustZone: Covers the basics of ARMv8-M TrustZone, describes how TrustZone is implemented on Series 2 devices, and provides application examples.
Production Programming of Series 2 and Series 3 Devices: Demonstrates how to properly program, provision, and configure Series 2 and Series 3 devices in a production environment.
Anti-Tamper Protection Configuration and Use: Describes how to program, provision, and configure the Secure Engine anti-tamper module. The anti-tamper module is only available on Secure Vault High and Series 3 Secure Vault devices.
Authenticating Silicon Labs Devices using Device Certificates: Describes how to authenticate an EFR32 Series 2 device with Secure Vault, using secure device certificates and signatures.
Secure Key Storage: Explains how to securely "wrap" keys in EFR32 Series 2 devices with Secure Vault, so they can be stored in non-volatile storage.
Programming Series 2 Devices Using the Debug Challenge Interface (DCI) and Serial Wire Debug (SWD): Describes how to provision and configure Series 2 devices through the DCI and SWD.
Integrating Crypto Functionality Using PSA Crypto Compared to Mbed TLS: Describes how to integrate crypto functionality into applications using PSA Crypto compared to Mbed TLS.