Training ... Support ... Description le_connection_closed le_connection_disable_slave_latency# This command temporarily ... 1 le_connection_mode1_level2 Unauthenticated pairing with encryption
Send an LE credit-based connection response to an LE credit-based connection request received in the sl_bt_evt_l2cap_le_channel_open_request event. ... connection The connection handle [in]
Send an LE credit-based connection response to an LE credit-based connection request received in the sl_bt_evt_l2cap_le_channel_open_request event. ... connection The connection handle [in]
If a connection is closed, the event le_connection_closed will be sent to the ... When a connection event is received(le_connection_opened), the application can determine whether or not there ...
... is initiated, it is still possible at any point in time to update the connection parameters via a call to the routine gecko_cmd_le_connection_set_parameters() in the application layer: