Matter Hardware Requirements#
[SIMPLICITY STUDIO] & [GITHUB]
To run Matter over Thread or over Wi-Fi requires some Silicon Labs hardware in order to run demos and do development. Following are the hardware requirements for both Thread and Wi-Fi use cases broken down by platform and transport protocol.
The following sections describe the hardware that may be used for Matter+OpenThread (Matter Hub and Accessory Device) and for Matter+Wi-Fi (Accessory Device). The EFRMG24 is the preferred starting point for Matter MCUs (including the Matter Hub RCP and both Accessory Devices). It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
Matter Over Thread "Matter Hub" Requirements#
If you are running Matter over Thread and do not have a platform on which to run the Open Thread Border Router and chip-tool, Silicon Labs recommends that you run them on a Raspberry Pi. To do so you will need:
- Raspberry Pi - Raspberry Pi 4 with an SD card with storage >= 64 GB 
 
The Raspberry Pi 4 is used to run the Open Thread Border Router and the chip-tool. In this documentation the combination of this software on the Raspberry Pi is also called the 'Matter Hub' A software image for the Raspberry Pi is provided on the Matter Artifacts page.
- Radio Co-Processor (RCP) - The Matter Hub needs a 15.4 Radio Co-Processor (RCP) in order to create and interact with the Thread network. The RCP can be any Silicon Labs development board that is capable of running the OpenThread RCP firmware. The RCP radio board is connected to the Raspberry Pi via USB. - Over 60 Silicon Labs boards support running the RCP firmware. To build an image for a board which is not listed here, download and build your image in Simplicity Studio. Pre-built OpenThread RCP firmware images are provided for the following boards on the Matter Artifacts page: - Note: The EFR32MG24 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image. - MG24 boards: - BRD4186C / xG24-PK6009A / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4187C / xG24-PK6009A / Wireless Starter Kit / 2.4GHz@20dBm 
 
- MG12 boards: - BRD4161A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4162A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4163A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4164A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
 
 
Matter Over Thread Accessory Device Requirements#
The Matter Accessory Device (MAD) is the actual device that the Matter application firmware (such as the Matter Light or Matter Switch) runs on. Several different platforms for the Matter Accessory Device are supported. Pre-built binary images for the Matter accessory devices are provided on the Matter Artifacts page. Silicon Labs supports development of Matter Accessory Devices for Matter over Thread on the following platforms:
Note: The EFR32MG24 is the preferred starting point for Matter MCUs. It provides Secure Vault and can use the internal flash of the device to store an upgrade image.
- MG24 boards: - BRD4186C / xG24-PK6009A / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4187C / xG24-PK6009A / Wireless Starter Kit / 2.4GHz@20dBm 
- BRD2703A / MG24 Explorer Kit > Note: This board has yet to be released to the public, but it is > supported in the Silicon Labs build flow. 
- BRD2601B / MG24 Explorer Kit 
- BRD4319A / xG24-PK6009A / Wireless Starter Kit/ 2.4GHz@20dBm > Note: This board has yet to be released to the public, but it is > supported in the Silicon Labs build flow. 
- BRD2704A / Sparkfun Thing Plus MGM240P board > Note: This board has yet to be released to the public, but it is > supported in the Silicon Labs build flow. 
- BRD4316A / xG24-PK6009A / Wireless Start Kit / 2.4GHz@10dBm 
- BRD4317A / xG24-PK6009A / Wireless Starter Kit/ 2.4GHz@20dBm 
 
- MG12 boards: - BRD4161A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4162A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4163A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4164A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4166A / SLTB004A / Thunderboard Sense 2 / 2.4GHz@10dBm 
- BRD4170A / SLWSTK6000B / Multiband Wireless Starter Kit / 2.4GHz@19dBm, 915MHz@19dBm 
 
Matter over Wi-Fi Accessory Device Requirements#
The Silicon Labs Matter over Wi-Fi demo and development requires two boards: the Silicon Labs EFR32 Radio board to run the Matter code, and either the RS9116, SiWx917 or WF200, to run the Wi-Fi protocol stack. Pre-built images for the EFR32 are provided on the Matter Artifacts page. Pre-built images for SiWx917 or RS9116 connectivity firmware are available, instructions on the Software Requirements Page. The following boards are supported for the Matter over Wi-Fi demos and development:
Note:
- The EFR32MG24 is the preferred starting point for Matter MCUs. It provides Secure Vault, and can use the internal flash of the device to store an upgrade image. 
- For running with the WF200 in NCP mode, the WF200 connectivity firmware image is included in the pre-built EFR32MG12, or EFR32MG24 images on the Matter Artifacts page. 
On first-time startup, Matter applications download the connectivity firmware onto the WF200.
- MG24 boards: - BRD4186C / xG24-PK6009A / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4187C / xG24-PK6009A / Wireless Starter Kit / 2.4GHz@20dBm 
 
- MG12 boards: - BRD4161A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4162A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4163A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@10dBm 
- BRD4164A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
- BRD4170A / SLWSTK6000B / Wireless Starter Kit / 2.4GHz@19dBm 
 
- Wi-Fi Dev Kits & boards - RS9116 - SB-EVK1 / Single Band Wi-Fi Development Kit / 2.4GHz 
- SB-EVK2 / Single Band Wi-Fi Development Kit / 2.4GHz 
- DB-EVK1 / Dual Band Wi-Fi Development Kit / 2.4GHz & 5GHz - RS9116X-DB-EVK1 > Note: Matter only supported over 2.4GHz on this Dev kit. 
 
- Interconnect board (included in the Wi-Fi kits) 
- SPI Cable (included in the RS9116 kit) 
- Jumper Cables (included in the RS9116 kit) 
 
- SiWx917 
- WF200 - WF200 / Single Band Wi-Fi Expansion Board / 2.4GHz 
- WFM200S / Single Band Wi-Fi Expansion Board / 2.4GHz 
 
 
Additional Matter over Wi-Fi Hardware Requirements#
In addition to your Matter over Wi-Fi Accessory Device you will need the following for both running the demo and for development:
- Access point with Internet access 
- microSD card (>=64GB) (if using Raspberry Pi) 
- [Optional] Android Mobile phone (If using the chip-tool on Android)