Loading firmware Expansion board#
Loading firmware on Expansion board can be done using Teraterm or kermit
- Make sure that the switches on the expansion board are towards UART side.   
- For updating the SiWx917 Firmware, refer Updating the RS9116 Firmware. Instructions are the same for both SiWx917 and RS9116. 
- Once that is done make sure to make switches back to Expansion mode, while using it with the host platform.