Silicon Labs Matter Version 2.6.0-1.4 (June 18, 2025) - Release Notes#
Simplicity SDK Version 2025.6.0
This is the Silicon Labs Matter v2.6.0-1.4 release, which provides the functionality to build Matter applications in the Simplicity Studio environment. This release is intended for developers who wish to run a Matter Demo over Thread (15.4) or Wi-Fi, as well as manually build examples through Simplicity Studio, SLC-CLI or Visual Studio Code.
This release is certifiable to the Connectivity Standards Alliance (CSA) Matter 1.4 certification program (https://csa-iot.org/) for Thread (MG24 / MG26) andWi-Fi NCP platform (MG24/WF200).
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Miscellaneous bug fixes and improvements.
Quality-tested Matter 1.4.1 solution for Thread MG24 / MG26, Wi-Fi SiWx917 SoC and NCP mode, Wi-Fi MG24/WF200 and Wi-Fi MG24/RS9116 (non-sleepy).
For Wi-Fi SiWx917 SoC and NCP mode, there are known timeout issues in certain stress test conditions, which have not been observed with ecosystems under normal conditions. For details see the Known Issues section of the Release Notes.
Works with Simplicity SDK v2025.6.0 and WiSeConnect SDK v3.5.0.
Added the ability to run a concurrent BLE connection with Matter OT+BLE DMP or Matter ZB+OT+BLE CMP.
Added Multi-OTA alpha support for SiWx917 SoC and NCP.
Enable an experimental option to use the TCP/IP NetX stack instead of lwIP for SiWx917 for both SoC and NCP.
API Changes#
None.
Bug Fixes#
Fixes to Matter/WiFi connectivity issues in stress test scenarios.
Chip Enablement#
This release supports series 2 and series 3 EFR32 devices. Use v2.2.x-1.2 for series 1 devices.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Multi-image OTA enhancements feature for SiWx917 (Alpha)
Added Multi-image OTA software update capability for SiWx917.
Implemented application image handling for efficient OTA updates.
Enabled combined image handling for seamless integration of multiple images.
Enabled encryption and decryption support for enhanced security.
Added Provision storage support to store the OTA keys.
Enabled Factory Data OTA upgrade feature for SiWN917.
Ability to run a concurrent BLE connection with Matter OT+BLE DMP or Matter ZB+OT+BLE CMP.
Experimental option to use the TCP/IP NetX stack instead of lwip for SiWx917 for both SoC and NCP.
Enhancements#
None.
Removed Features#
None.
Deprecated Features#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
None.
Modified APIs#
None.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
1381037 | The StartUpOnOff attribute of the OnOff cluster in the Zigbee Matter Light application does not maintain its setting after a reboot. | None | EFR32 |
1367521 | Improved start-up ON time to under 500 ms with Zigbee/Matter CMP Lighting app. | None | EFR32 |
1404385 | Removed duplicated OTA provider after the device detaches and reattaches. | None | EFR32 |
1436791 | StartUpOnOff toggle (2) has the wrong behavior in Zigbee Matter Light sample app. | None | EFR32 |
1445627 | Corrected the PlugOverThread app sequence of actions. | None | EFR32 |
1434945 | Fixed a crash that may occur if the user name is empty when creating a new user with Lock sample app. | None | EFR32 |
1400085 | Fixed an issue with UserIndex missing in Lock sample app when sending a LockOperation. | None | EFR32 |
1432056 | Device hangs during stress test. | None | SiWG917 |
1432647 | Device hangs after being idle overnight. | None | SiWG917 |
1443714 | Observed AP disconnection when the DUT is in an idle state after commissioning. | None | SiWG917 |
1417941 | Missing component file for SGP40 Sparkfun Air Quality Sensor Support with Ait Quality Sensor sample app. | None | SiWG917 |
1430203 | Corrected documentation and commands in the Matter over WiFi SoC Window Covering app. | None | SiWG917 |
1439077 | Corrected documentation in the Matter over WiFi SoC Lock app readme. | None | SiWG917 |
1417728 | Replace the CHIP_ERROR_INTERNAL return code with the appropriate error code. | None | SiWG917 |
Chip Enablement#
Matter over Thread is supported on the following boards#
MG24 boards:
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm - xG24-RB4186C
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm - xG24-RB4187C
BRD2601B / MG24 Developer Kit - xG24-DK2601B
BRD2703A / MG24 Explorer Kit - xG24-EK2703A
MGM24 boards:
BRD4316A / SLWSTK6006A / Wireless Start Kit / 2.4GHz@10dBm - xGM240-RB4316A
BRD4317A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4317A
BRD4318A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4318A
BRD4319A (Rev A00 only) / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm
BRD2704A / Sparkfun Thing Plus MGM240P
BRD4337A / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm - xGM240-RB4337A
MG26 boards
BRD4116A
BRD4117A
BRD4118A
BRD2608A
BRD2709A
MGM26 boards
BRD4350A
BRD4351A
Matter over Wi-Fi is supported on the following boards#
SoC mode:
BRD4338A / SiWG917 Wi-Fi 6 and Bluetooth LE 8 MB Flash SoC Pro Kit - SiWx917-PK6031A
BRD2605A / SiWG917 Wi-Fi 6 and Bluetooth LE Dev Kit - SiWx917-DK2605A
BRD4342A / SiWG917 Wi-Fi 6 and Bluetooth LE 8 MB Flash + 8 MB ext PSRAM Radio Board with an internal RF switch - SiWx91x-RB4342A
BRD4343A / SiWG917Y Module Wi-Fi 6 and Bluetooth LE 8MB Flash RF-Pin Radio Board - SiW917Y-RB4343A
Early access for new module board BRD2708A / SiW917Y-EK2708A
NCP mode:
Host Processor:
BRD4186C / EFR32xG24 Wireless 2.4 GHz +10 dBm Radio Board (EFR32 radio board) - xG24-RB4186C
BRD4187C / EFR32xG24 Wireless 2.4 GHz +20 dBm Radio Board - xG24-RB4187C
Silicon Labs Wi-Fi Processor:
RS9116X EVK1 Wi-Fi + Bluetooth Dev Kit - RS9116X-SB-EVK1 / RS9116X-SB-EVK2 / RS9116X-DB-EVK1
SiWx917-EB4346A - SiWx917 Wi-Fi 6 and Bluetooth LE Co-processor EXP Expansion Kit
SiW917Y-RB4357A - SiWN917Y Module Wi-Fi 6 and Bluetooth LE 4MB Flash RF-Pin Co-Processor Radio Board
SLEXP8022A - WF200 Wi-Fi Expansion Kit
Note: Firmware for RS9116, SiWN917 NCP & SiWG917 SoC can be found in the Matter Software Artifacts page in the documentation or Assets section of this page. Connectivity firmware update is mandatory for new release binaries.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
For the list of supported application examples see Existing Examples. For the details on Matter ecosystems support see Ecosystems.
New Examples#
None.
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
Matter over Wi-Fi with SiWG917 sleepy is Beta quality in this release. It is tested by SQA but is affected by a known issue seen with WiseConnect SDK v3.5.0.
ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
The Matter logs are printed to the UART interface by default. To view the logs use the Simplicity Studio console or a standalone terminal emulator such as PuTTY. The logging destination can be controlled by installing the "Logging To UART" or the "Logging to RTT" component under Matter -> Platform -> Utils in a Matter Studio project. | None | All | ||
The Matter device images require approximately 700k in flash space. As a result, only a subset of EFR32MG2x devices are supported. For a complete list of devices supported, consult the documentation located at Matter Hardware Requirements. | None | All | ||
A Matter SDK Issue: (https://github.com/project-chip/connectedhomeip): BLE Connection/Timeout error occurs occasionally during commissioning with the chip-tool running on Raspberry Pi or Linux (project-chip#16178). Running on these platforms requires an access point with both 2.4 GHz and 5 GHz capabilities. There is BLE-Wi-Fi interference when connected over the 2.4 GHz channel. This is resolved by connecting the chip-tool device to a 5 GHz SSID and the end device to a 2.4 GHz SSID for the same Wi-Fi network. | None | All | ||
In some rare cases a Simplicity Studio project build may fail due to missing files in the | None | Delete the | All | |
Incorrect state error sometimes while commissioning another fabric. | None | All | ||
Window App device goes offline after commissioning with the Apple Ecosystem. | None | All | ||
Unbolt feature is not supported via the ecosystems like Apple, Samsung and Amazon Alexa but it is supported by our device default due to which Unlock with these Ecosystem will fail. To disable unbolt feature, the feature bit for the DoorLock Cluster should be update from 0x1DB3 to 0xDB3. | None | All | ||
1197733 1228823 | Due to an electrical issue on the WPK main boards (BRD4002x), sometimes the current measurement value reported is wrong in the Energy Profiler, making it seem like an ICD is not going to sleep properly even though it is. This issue does not happen when using a WSTK (BRD4001x). | None | All | |
The configuration parameters for the internal storage bootloader used in the OTA software updates must always be custom-configured based on the actual image size for the given application. See https://docs.silabs.com/matter/2.6.0/matter-ota/01-ota-bootloader. | None | All | ||
1370882 | ConnectMaxTimeSeconds attribute (and others) exposed by ZAP even though it cannot be modified (read only). Work in progress in PR#36516. | None | All | |
1445664 | Chip-Cert executable cannot be used in Windows installations of Simplicity Studio v5. | None | All | |
Matter/Thread: Silicon Labs has provided a complete image file for the Raspberry Pi that can be flashed onto an SD card to create the "Matter Hub", which is a Raspberry Pi running Ubuntu and includes a pre-built version of the Open Thread Border Router (OTBR) and chip-tool. The image we have provided is quite large, ~2 GB. As a result it can take quite a while to download the .zip file and flash it onto an SD card. Depending on your connection the process could take up to half an hour. Regardless, the demo and development experiences using this pre-built image is a much faster process than building the Matter Hub from scratch. | None | EFR32 | ||
Matter/Thread: Matter attestation credentials can conflict with Lockbits in Series 2, requiring moving the location of the attestation credentials when lockbits are used. Please see the guide Moving the Matter Attestation Credentials on Series 2 (MG24) for details. (1235425) | None | EFR32 | ||
1378481 | USART for IO Stream (RTT) is not supported in Matter Extension v2.4.0-1.4 | None | EFR32 | |
1367027 | Zigbee Matter Light, in rare occurrence, will momentarily fail to receive packages over 15.4 when utilizing BLE DMP with Thread. This may result in OTA update image transfer failures. | None | EFR32 | |
1418676 | Possible race condition in UART driver when excessive use of the Matter shell is performed (sending commands every 250 ms) | None | Reduce the command rate. | EFR32 |
1442643 | In rare occurrences when OT traffic is high, the CMP app can hang when accessing secure element. | None | EFR32 | |
1453646 | Level attribute may get incorrectly changed on level-control stop. | None | EFR32 | |
1256541 | In high traffic environment, mDNS timeout is seen with SiWG917 SoC and SiWN917 NCP. | None | None | SiWx917 |
1200114 | Observed CASE session timeout during sigma packet transaction while sending a unicast command with the Lock Sleepy app, which sometimes results in a resource busy error from the device (until the device commissioning times out). | None | None | SiWx917 |
Enabling "Logging to RTT" with SiWG917 SoC results in OTA update failure due to JLink connection preventing soft reset. | None | Enabled UART logging | SiWG917 | |
1358324 | The BRD4342A PSRAM support is enabled only for the text segment; it is not working for the data and bss segment. | None | None | BRD4342A |
1366720 | BLE scan issues are observed with Raspberry Pi when the distance between the device and the controller exceeds 3 meters in SQA lab environment. | None | None | SiWG917 |
1387498 | Multi-admin test case fails for sleepy applications with Samsung ecosystems. | None | None | SiWG917 |
1436385 | Observed a delay in controlling the device after power cycling the AP in the Google ecosystem. | None | None | SiWG917 |
The 917 SoC supports only 5 UULP pins, so components like BTN1, LEDs, J-Link, and the shell do not work with sleepy applications, as they are not mapped to UULP pins. When testing for certification, there may be a timeout due to slow response because of NVM3 being near full and causing repacks when a reply is expected. | None | Add more pages for NVM3 | SiWG917 | |
The P37 pin must be pulled up to enable the Matter shell or before executing any JLink command for sleepy applications. | None | None | SiWG917 | |
1409219 | On the BRD2605A board, RGB LED pins are not configurable via the LED component or Pin Tool, requiring manual updates to the RTE device file for any new LED pin configurations. | None | Hardware limitation. | SiWG917 |
1407412 | The Matter over WiFi sample apps are currently hard coded to the US region per default. | None | Change the #define REGION_CODE from US to EU in Wifiinterface.cpp. | SiWG917 |
In EFR32MG24+WF200 device combination, WF200 Firmware exception is observed when both ICD and matter shell is enabled. In order to make matter shell to work for Lock application with this device combination, ICD is disabled. | None | Hardware limitation | SLEXP8022A - WF200 Wi-Fi Expansion Kit | |
The external bootloader should not be used with the EFR32MG24+RS9116/SiWN917 NCP device combination. Only use the internal bootloader. | None | None | SiWN917 | |
OTA Update: sometimes boot loading with latest image does not work with WF200 with EFR32xG24 device combination. This issue is resolved by applying the workaround described in the Matter Wi-Fi FAQ. | None | None | SLEXP8022A - WF200 Wi-Fi Expansion Kit | |
SiWN917 NCP application OTA upgrade with upgraded WiSeConnect SDK may not be backward compatible with the existing TA. | None | None | SiWN917 | |
Group commands only work for some specific access points when IGMP snooping is disabled. | None | None | All Wi-Fi boards | |
1085568 | With EFR32 MG24 + RS9116 after going idle for some time, Apple devices may not be able to control an LED. | None | None | RS9116 |
When setting up the Ozone Debugger on Mac the location of the JLinkDevices.xml file has moved, Follow this documentation in order to place it in the proper location. | None | None | NA | |
1381843 | LCD is disabled on RS9116 and SiWN917 NCP. | None | LCD is disabled. | |
1463849 | The Device takes more than 3 minutes to reconnect after a power cycle. | None | None | SiWN917 |
1357133 | Commissioning failed during the Wi-Fi Network Enable step. | None | None | SiWx917 |
1465345 | The IDM test case returned an incorrect result for WF200, stating that the device supports Thread but does not support Wi-Fi. | None | None | SLEXP8022A - WF200 Wi-Fi Expansion Kit |
1382232 | Commissioning failed during the send complete step. | None | None | SiWG917 |
1327801 | The IP address is still displayed after removing the fabric. | None | None | SiWG917 |
Commission into Matter/OT fails when building OTBR and NCP with low power | None | None | EFR32 |
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
sl_main migration: See sl_system to sl_main migration guide for detailed instructions.
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
Silicon Labs Matter Extension for use with Simplicity Studio and SLC-CLI
Silicon Labs Matter sample applications
Compatible Software#
Software | Compatible Version or Variant |
|---|---|
Simplicity SDK | |
GCC (The GNU Compiler Collection) | 12.2.1 (provided with Simplicity Studio) |
Installation and Use#
To get started, download Simplicity Studio from the following link: https://www.silabs.com/developers/simplicity-studio, and install Simplicity SDK v2025.6.0 along with Silicon Labs Matter v2.6.0. For SiWx917, install WiSeConnect v3.5.0 as well.
Quick-start guides are provided for running pre-compiled demos and for building examples manually.
The Developer's Guide provides information on various technical topics.
For details on Studio project upgrades see Project Upgrades.
In order to run Matter over Thread, a developer must have a Silicon Labs EFR-based device and either:
another EFR-based device and a Raspberry Pi with a 32 GB SD Card
or an ecosystem device with OpenThread Border Router capabilities such as Amazon Echo, Apple HomePod, Samsung SmartThings Hub or Google Nest Hub Wi-Fi.
In order to run Matter over Wi-Fi, a developer must have the following hardware:
Silicon Labs Wireless starter/development kit which is mentioned below.
Raspberry Pi with a 32 GB SD Card or an ecosystem with Matter support To run your first demo, see our Getting Started Guides.
To kick start your development, see our Developer's Guide.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
To learn more about the software in this release, dive into our online documentation.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.
Additional Information#
Existing Examples#
Matter over Thread is supported in Simplicity Studio for the following applications:#
Light
Light Switch
Lock
Window Covering
Thermostat
OnOff Plug
Sensor
Dishwasher
Air Quality Sensor
Refrigerator
Zigbee Matter Light
Matter over Wi-Fi is supported in Simplicity Studio for the following applications:#
SoC and Dev Kit supported applications:
Light
Lock
Light Switch
Window Covering
OnOff Plug
Thermostat
Dishwasher
Air Quality Sensor
Sensor
Fan Control
Refrigerator
NCP supported applications:
Lock
Thermostat
Window Covering
Note: SiWN917 NCP is the only device combination which supports Window Covering App.
Matter over Wi-Fi ICD is supported for the following applications:#
Lock (ICD is enabled by default)
With chip-tool
With EFR32xG24 with SiWN917 in NCP mode
Window Covering (ICD is enabled by default)
With chip-tool
With EFR32xG24 with SiWN917 in NCP mode
Thermostat
With chip-tool
With EFR32xG24 with RS9116, SiWN917 in NCP mode
Light Switch
With chip-tool
With SiWG917 SoC
Reference guide to enable the sleepy functionality for Wi-Fi: Wi-Fi ICD.
Ecosystems#
This release has been tested and proven to work for commissioning and control with the following Ecosystems on the hardware and software versions listed below:
Google#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/Lock/Window/Multi-sensor-app | Hardware: Google Nest Hub, Model : GUIK2 Software: Hub SoftwareChromcast 3.76.463359 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Google Home version: 3.30.1.6 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoCBRD4338A | lighting/Lock/Window/Multi-sensor-app | Hardware: Google Nest Hub, Model : GUIK2 Software: Hub Software Version: Chromcast 3.76.463359 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Google Home version: 3.30.1.6 | ASUS (Model: XT8) |
Apple#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/Lock/Window/Multi-sensor-app | Hardware: Home Pod MiniSoftware: 18.5 (22L572) | Hardware: iPhone 12 pro Software: 17.6 | Apple Home17.6.1 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoC | lighting/Lock/Window/Multi-sensor-app | Hardware: Home Pod MiniSoftware: 18.5 (22L572) | Hardware: iPhone 12 proSoftware : 17.6 | Apple Home17.6.1 | ASUS (Model: XT8) |
Amazon#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/Window/Multi-sensor-app | Hardware: Echo 4th Gen Model: L4S3RE Software: Hub Software Version: 11779349892 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Alexa version: 2.2.6607727 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoCBRD4338A, | lighting/lock/Window/Multi-sensor-app | Hardware: Echo 4th Gen Model: L4S3RE Software: Hub Software Version: 11779349892 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Alexa version: 2.2.6607727 | ASUS (Model: XT8) |
Samsung#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/lock/Window/Multi-sensor-app | Hardware: SmartThings Station Software: Hub Software Version: 000.052.00009 Hardware: Charging Hub Software Controller version: 1.0.15-5 | Hardware: Pixel 5a Software: Android version 14 | SmartThings Version: 1.7.19.19 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoCBRD4338A, | lighting/lock/Window/Multi-sensor-app | Hardware: SmartThings Station Software: Hub Software Version: 000.056.00011 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | SmartThings Version: 1.8.29.24 | ASUS (Model: XT8) |
Project Upgrades#
Upgrades of pre-2.4.0-1.4 projects based on the Lighting application require the that user manually removes the references to OnOffSwitchConfiguration from ZclCallbacks.cpp.
An upgrade of an existing Studio project from Matter 2.2.2-1.2 or earlier to the current version of the extension is not supported.
The Simplicity Studio project upgrade dialog can be exited only by closing the project tab (clicking on the "x" button in the top right corner).
The Multi-Sensor sample application is has the ICD feature enabled by default in this release. It is recommended that the user enables ICD in the Multi-Sensor projects upgraded to the current release.
The Matter and Zigbee SoC Light application does not support project upgrades to the current release.
When upgrading a Studio project to the current release the following changes are required:
Modify AppTask.cpp/AppTask.h in the project's src and include directory:
Rename
AppTask::Init()toAppTask::AppInit()remove the following from
AppInit():
err = BaseApplication::Init(); if (err != CHIP_NO_ERROR) { SILABS_LOG("BaseApplication::Init() failed"); appError(err); }
Matter Software Artifacts#
Matter Software Artifacts: https://docs.silabs.com/matter/2.6.0/matter-prerequisites/matter-artifacts.