New Features#
New Features for v2.7.0-1.4#
Quality-tested Matter 1.4.2 solution for Thread MG24 / MG26, Wi-Fi SiWx917 SoC and NCP mode, Wi-Fi MG24/WF200 and Wi-Fi MG24/RS9116 (non-sleepy).
Provides GA support for Matter Wi-Fi SiWx917
Enabled Matter + AWS (previously known as DIC) support (Alpha Quality).
Provides support for Matter Thread and CMP with SiMG301x.
Support for Scenes in Matter added with Matter 1.4.2.
Fixed the mDNS and CASE session timeouts seen on Wi-Fi SiWx917.
Added Optimized LwIP package in the Matter Extension for Power Improvement in WiFi Devices.
Deprecation notice for Wi-Fi MG24/RS9116.
Removal of the Experimental option to use the TCP/IP NetX stack.
Works with Simplicity SDK v2025.6.2 and WiSeConnect SDK v3.5.2.
RGB LED support with the SiWG917 DevKit.
Miscellaneous bug fixes and improvements.
New Features for v2.6.1-1.4#
Quality-tested Matter 1.4.1 solution for Thread MG24 / MG26, Wi-Fi SiWx917 SoC and NCP mode, Wi-Fi MG24/WF200 and Wi-Fi MG24/RS9116 (non-sleepy).
For Wi-Fi SiWx917 SoC and NCP mode, there are known timeout issues in certain stress test conditions, which have not been observed with ecosystems under normal conditions. For details see the Known Issues section of the Release Notes.
Works with Simplicity SDK v2025.6.1 and WiSeConnect SDK v3.5.1
Miscellaneous bug fixes and improvements.
New Features for v2.6.0-1.4#
Quality-tested Matter 1.4.1 solution for Thread MG24 / MG26, Wi-Fi SiWx917 SoC and NCP mode, Wi-Fi MG24/WF200 and Wi-Fi MG24/RS9116 (non-sleepy).
For Wi-Fi SiWx917 SoC and NCP mode, there are known timeout issues in certain stress test conditions, which have not been observed with ecosystems under normal conditions. For details see the Known Issues section of the Release Notes.
Works with Simplicity SDK v2025.6.0 and WiSeConnect SDK v3.5.0
Added the ability to run a concurrent BLE connection with Matter OT+BLE DMP or Matter ZB+OT+BLE CMP.
Added Multi-OTA alpha support for SiWx917 SoC and NCP.
Enable an experimental option to use the TCP/IP NetX stack instead of lwip for SiWx917 for both SoC and NCP.
Miscellaneous bug fixes and improvements.
New Features for v2.5.2-1.4#
Updated to work with Simplicity SDK v2024.12.2 and WiSeConnect SDK v3.4.2.
Miscellaneous bug fixes.
New Features for v2.5.1-1.4#
Quality-tested Matter 1.4 GA solution for Thread MG24 / MG26, Wi-Fi SiWx917 SoC and RCP mode, Wi-Fi MG24/WF200 and Wi-Fi MG24/RS9116 (non-sleepy).
For Wi-Fi SiWx917 SoC and RCP mode, there are known timeout issues in certain stress test conditions, which have not been observed with ecosystems under normal conditions. For details, see the Known Issues section of the Release Notes.
Works with Simplicity SDK v2024.12.1 and WiSeConnect SDK v3.4.1.
GA support of the Matter Zigbee CMP (concurrent multi-protocol) Light example application.
Some limitations exist. For details, see the Known Issues section of the Release Notes.
Implemented button switch functionality for the Dimmer Switch application.
Fixed compatibility issue related to provisioning storage changes following the mbedTLS version upgrade.
Resolved commissioning issues in the Multi Sensor App on the SiWx917.
Miscellaneous bug fixes and improvements.
New Features for v2.5.0-1.4#
Quality-tested Matter 1.4 GA solution for Thread MG24 / MG26, Wi-Fi MG24/WF200 and Wi-Fi MG24/RS9116 (non-sleepy).
For Wi-Fi SiWx917 SoC and RCP mode, this is an Alpha. Basic functionality works but there are issues with stress testing, for details see the Known Issues section of the Release Notes. If GA quality is desired, use v2.4.0 release until the v2.5.1 patch is available.
Works with Simplicity SDK v2024.12.0 and WiSeConnect SDK v3.4.0.
Expands our existing Matter support in Thread with new hardware and software capabilities.
xG26 support is enabled for BRD4350A module, BRD4351A module, and BRD2709A Explorer Kit.
SixG301 Alpha support is enabled for BRD1019A.
GA support of the Matter Zigbee CMP (concurrent multi-protocol) Lighting example application.
Some limitations exist, for details see the Known Issues section of the Release Notes.
Expands our existing Matter support in Wi-Fi with new hardware and software capabilities.
Improved power numbers for the Wi-Fi SiWx917 SoC with the Selective Listening feature.
Refrigerator application and Dimmer switch application support has been added for SiWx917.
SiWx917 SoC module board support is enabled for BRD4343A and BRD2708A.
SiWx917 NCP board support is enabled for BRD4357A. Matter uses this board as an RCP; LwIP task runs on the EFR32.
Matter SiWx917 RCP Linux Host support has been added.
The mbedTLS library has been upgraded from 2.x to 3.x for the SiWx917.
DX Improvement: Added conformance data to Matter XML files and a 'Device Type Features' page in ZAP. Toggling a feature auto-updates the featureMap and aligns attributes, commands, and events to correct conformance plus shows detailed conformance warnings for them if their enabled state conflicts with conformance value.
Miscellaneous bug fixes and improvements.
New Features for v2.4.0-1.4#
Quality-tested Matter 1.4 GA solution for Thread MG24 / MG26, Wi-Fi 917 SoC and DevKit (BRD2605A), Wi-Fi MG24/WF200 (non-sleepy), Wi-Fi 917 NCP platforms. Beta support for Wi-Fi 917 SoC BRD4342A module and Alpha support for Wi-Fi MG24/RS9116 platforms.
LIT-ICD Support and Quiet Reporting Support is provided.
Sensor App is refactored to be more generic for easier usage and maintenance.
Fan Control App support is added for SiWx917.
Works with Simplicity SDK v2024.6.2 and WiSeConnect SDK v3.3.4.
Miscellaneous bug fixes and improvements.
New Features for v2.3.2-1.3#
Quality-tested Matter 1.3 GA solution for Thread MG24 / MG26, Wi-Fi SiWx917 SoC and DevKit(BRD2605A), Wi-Fi MG24/WF200, Wi-Fi SiWx917 NCP and Wi-Fi MG24/RS9116 (non-sleepy) platforms. Beta solution for Wi-Fi MG24/RS9116 (sleepy) platforms.
Works with Simplicity SDK v2024.6.2 and WiSeConnect SDK v3.3.3
BRD4342A PSRAM board support is enabled for all the Matter Wi-Fi applications - beta quality.
Miscellaneous bug fixes and improvements.
New Features for v2.3.1-1.3#
Quality-tested Matter 1.3 GA solution for Thread MG24 / MG26, Wi-Fi 917 SoC, Wi-Fi MG24/WF200, Wi-Fi 917 NCP (non-sleepy) and Wi-Fi MG24/RS9116 (non-sleepy) platforms. Beta solution for Wi-Fi 917 NCP (sleepy) and Wi-Fi MG24/RS9116 (sleepy) platforms.
Works with Simplicity SDK v2024.6.1 and WiSeConnect SDK v3.3.1.
WiseConnect 2 SDK is updated to v2.10.0 for RS9116.
Improved sleepy stability and power numbers with the Wi-Fi 917 SoC.
BRD2605A board support is enabled for the lighting, lock, and dishwasher Matter Wi-Fi applications - beta quality.
Introduced the Air Quality Sensor example application. The app also works with SparkFun SGP40 air quality sensor - alpha quality.
Miscellaneous bug fixes and improvements.
New Features for v2.3.0-1.3#
Quality-tested Matter 1.3 GA solution for Thread, Wi-Fi MG24/WF200, and Wi-Fi MG24/RS9116 (non-sleepy) platforms. Beta solution for Wi-Fi SiWx917 and Wi-Fi MG24/RS9116 (sleepy) platforms.
Works with Simplicity SDK v2024.6.0 and WiSeConnect SDK v3.3.0.
Introduces Matter over Thread support for BRD4116A, BRD4117A, BRD4118A, and BRD2608A boards from the EFR32MG26 family.
Introduces the Matter Zigbee CMP (concurrent multi-protocol) Lighting example application which demonstrates the usage of the Matter Stack alongside the Silicon Labs Zigbee stack.
Adds support for Long Idle Time ICDs.
Adds Provisioning 2.0 Support for EFR32 and SiWx917 SoC.
Provides Multi-chip OTA functionality support (EFR32-Thread only).
Adds support for TA based flash storage for storing factory data in SiWx917 SoC with alpha quality.
Enables Tickless Idle Mode and sleepy stability improvements for SiWx917 SoC.
Removes support for EFR32 Series 1 MG12 devices: BRD4161A, BRD4162A, BRD4163A, BRD4164A, BRD4170A, and BRD4166A.
Miscellaneous bug fixes and improvements.
New Features for v2.2.1-1.2#
Works with Gecko SDK v4.4.2 and WiSeConnect SDK v3.1.4.
Provides Matter Solutions functionality for all sample applications. Example-only project generation has been removed to simplify user options.
Adds support for custom clusters in Matter Studio projects – simply add the cluster XML file through the "Extensions" menu in ZAP.
Enables LCD and OTA support (M4 image only) for MG24+SiWx917 NCP.
Miscellaneous bug fixes and improvements.
New Features for v2.2.0-1.2#
GA support for Intermittently Connected Devices
Introduction of a third LCD screen to display application information
Introduction of the Dishwasher Demo Application
Adds support of Matter 1.2 on all devices
Adds Matter support on SiWx917 SoC Common flash variants - BRD4338A
Adds LCD display support on SiWx917 SoC for all the Wi-Fi Matter Apps
Adds support for Direct Internet Connectivity on the SiWx917 SoC & NCP
Support for Visual Studio Code integration
Adds support for certificate provisioning on SiWx917 SOC
Adds support for Firmware Upgrade on SiWx917 SOC
Self-Provisioning Mode#
Silicon Labs' Matter examples now include a self-provision mode, which enables the application to be used as Generator Firmware with the provisioning script:
e.g.:
python3 provision.py -c config/silabs.json -gf ../out/light/BRD4187C/matter-silabs-lighting-example.s37
To enter the self-provisioning mode, factory reset the device pressing buttons BTN0 and BTN1 for six seconds. Using this method, the device application only needs to be flashed once, provisioned multiple times, and be ready for commissioning after each provisioning.
Support for Intermittently Connected Devices (ICD)#
With the official introduction of Matter Short Idle Time (SIT) ICDs, both the door-lock sample app and the light-switch sample app are configured as SIT ICDs by default (with the exception of SiWx917 SoC examples).
The default configurations can be found in their respective sl_matter_icd_config.h
configuration files.
Full support for ICD Short Idle Time (SIT) Devices in support of the Matter 1.2 specification
In this release, Silicon Labs has provided full support for Short Idle Time intermittently connected devices
These are ICDs (formerly called Sleepy End Devices) which must remain responsive to user input such as Door Locks and Window Coverings
ICD Management cluster server implementation
Silicon Labs has provided an implementation of the ICD cluster server and the configuration of the ICD
ICD Manager and ICD Event Manager has been implemented to manage the Idle and Active mode of the ICD
NEW DNS advertisement Text Key SAI: indicates the SLEEPY_ACTIVE_INTERVAL (default to 4000 ms when ICD is not enabled)
NEW Matter ICD configuration defines:
CHIP_CONFIG_ICD_IDLE_MODE_INTERVAL sets the value for the ICD IdleInterval attribute
CHIP_CONFIG_ICD_ACTIVE_MODE_INTERVAL sets the value for the ICD ActiveInterval attribute
CHIP_CONFIG_ICD_ACTIVE_MODE_THRESHOLD sets the value for the ICD ActiveThreshold attribute
CHIP_CONFIG_ICD_CLIENTS_SUPPORTED_PER_FABRIC sets the value for the ICD ClientsSupportedPerFabric attribute
All of these defines can be configured within
sl_matter_icd_config.h
inside the config directory (default values listed here):
#define SL_IDLE_MODE_INTERVAL = 600 // 10min Idle Mode Interval
#define SL_ACTIVE_MODE_INTERVAL = 1000 // 1s Active Mode Interval
#define SL_ACTIVE_MODE_THRESHOLD = 500 // 500ms Active Mode Threshold
#define SL_ICD_SUPPORTED_CLIENTS_PER_FABRIC = 2 // 2 registration slots per fabric
// The OpenThread polling rates used in either ICD mode
#define SL_OT_IDLE_INTERVAL = 15000 // 15s Idle Intervals
#define SL_OT_ACTIVE_INTERVAL = 200 // 200ms Active Intervals
CHANGES:
Optimized the subscription reports by synchronizing all client’s subscriptions with the ICD idle mode interval. This ensures the minimal amount of wake ups possible due to subscription reports. This component is introduced as
matter_subscription_synchronization
.The previous
matter_sed
components has been replaced bymatter_icd_management
. This is in line with previous sleepy end device behavior being deprecated and replaced by the ICD behavior.Silicon Labs' Light Switch and Door Lock apps support the ICD implementation and have the ICD cluster enabled.