Silicon Labs Matter Version 2.8.1-1.5 (Mar 25, 2026) - Release Notes#
Simplicity SDK Version 2025.12.2
This is the Silicon Labs Matter v2.8.1-1.5 release, which provides the functionality to build Matter applications in the Simplicity Studio environment. This release is intended for developers who wish to run a Matter Demo over Thread (15.4) or Wi-Fi, and also manually build examples through Simplicity Studio v6 / Visual Studio Code or SLC-CLI.
This release is certifiable to the Connectivity Standards Alliance (CSA) Matter 1.5 certification program (https://csa-iot.org/) for Thread (MG24, MG26 and MG30) and Wi-Fi (SiWx917 and MG24 / WF200).
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added In 2.8.1#
The Silicon Labs Matter repositories are open for external contributions: https://github.com/SiliconLabsSoftware/matter_extension
Added Matter demo for an Oven and Range Hood App for the MG thread devices.
Matter Wi-Fi applications now use the WiseConnect SDK linker files so they are aligned with the underlying platform. For backward compatibility (for OTA upgrades on existing devices) — and specifically for Common-flash boards — add the toolchain_gcc_common component to your project to continue using the Matter-provided linker files.
Added In 2.8.0#
Quality-tested Matter 1.5 solution for Thread and WiFi.
Added support for Amazon Matter Simple Setup (MSS) with 917SoC.
Added Matter demo for an Oven and Range Hood App.
Added further optimizations in LwIP timers.
API Changes#
Changed In 2.8.1#
Using the Wiseconnect SDK linker file rather than matter ones, to use matter available linker file add toolchain_gcc_common component to the project for Common flash boards.
Changed In 2.8.0#
Custom cluster API changes.
Bug Fixes#
See Bug Fixes.
Chip Enablement#
Added in 2.8.1#
None.
Added in 2.8.0#
This release supports Series 2 and Series 3 EFR32 devices. Use v2.2.x-1.2 for Series 1 devices.
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
New Features#
Added In 2.8.1#
PSRAM board support in Matter now uses WiseConnect components. To place specific code/data in PSRAM, enable the corresponding WiseConnect component for the section or region you want to relocate.
The Silicon Labs Matter repositories are open for external contributions: https://github.com/SiliconLabsSoftware/matter_extension
Added In 2.8.0#
Quality-tested Matter 1.5 solution for Thread MG24 / MG26 / MG30, Wi-Fi SiWG917 SoC and SiWN917 NCP mode, and Wi-Fi MG24/WF200.
Works with Simplicity SDK v2025.12.0 and WiseConnect SDK v4.0.0.
Added support for Amazon Matter Simple Setup (MSS) with 917SoC.
Enabled support for Matter + AWS (formerly DIC) on 917 NCP - Alpha Quality.
Added Closure App for Thread and Wi-Fi (SiWG917 SoC).
Added Matter demo for an Oven and Range Hood App.
Added further optimizations in LwIP timers (both IPv4 and IPv6) for improved power efficiency for Wi-Fi Devices.
Added Memory Manager support with SiWG917.
Added RGB LED support for Thread.
Added Platform Template app.
Removed the Matter Wi-Fi support for MG24 + RS9116.
Improved build times for Matter projects.
Miscellaneous bug fixes and improvements.
Added support for TrustZone for EFR32 MG24 for Matter projects.
Enhancements#
Added in 2.8.1#
None.
Added in 2.8.0#
Added further optimizations in LwIP timers (both IPv4 and IPv6) for improved power efficiency for Wi-Fi Devices.
Removed Features#
Removed in 2.8.1#
None.
Removed in 2.8.0#
Matter Wi-Fi support for MG24 + RS9116 has been removed.
Deprecated Features#
Deprecated in 2.8.1#
Deprecation notice — Matter support for MG24 + WF200.
Deprecation notice — The Matter-provided linker files for common flash boards will be discontinued. The default linker file from the WiseConnect SDK is now used instead.
Deprecated in 2.8.0#
None.
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added In 2.8.1#
None.
Added In 2.8.0#
Added a configuration for a shorter idle mode duration when a LIT capable device is operating as a SIT. It can be configured through SL_SHORT_IDLE_MODE_DURATION_S.
Modified APIs#
Modified In 2.8.1#
None.
Modified In 2.8.0#
In order to use a custom cluster in a Matter application, the ZAP file needs to be modified and a component must be enabled. For details, see Custom Matter Device Development.
Removed APIs#
None.
Deprecated APIs#
None.
Bug Fixes#
Fixed In 2.8.1#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
1582257 | Matter examples for BRD4342A bydefault have PSRAM enabled in the Linkerfile. | None | SiWG917 |
1590024 1593258 | Matter examples gives compilation errors if something is configured in the config/FreeRTOSConfig.h file. | None | All |
1579547 | IDM_10_5 Extra cluster found on endpoint with device types errors. | None | SiWx917 |
1571040 | TC-RR-1.1 fails on the Window-app. | None | SiWx917 |
1571039 | TC-DESC-2.2 fails on the Window-app. | None | SiWx917 |
1355000 | Removing the custom linker and the startup files for the 917SoC. | None | SiWG917 |
1564606 | Resolved a syntax error in the sl_matter_ota_config. | None | All |
1556875 | Fixed an issue in OT alarm asserts that may randomly hang Matter. | None | EFR32 |
Fixed In 2.8.0#
ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
1528166 | Intermittent failures see while commissioning on the second fabric. | None | SiWx917 |
1517540 | Cluster revision mismatch for the fan control cluster. | None | SiWG917 |
1556530 | ICD incorrectly enabled for lock application on WF200. | None | EFR32+WF200 |
1397073 | Transition to MODE_CHANGE_FAIL not working in Refrigeration & Temperature Controlled Cabinet application. | None | SiWG917 |
1437684 | Incorrect values in CurrentHeapHighWatermark. | None | SiWG917 |
1407412 | Support for programming the Wi-Fi region code to a different region. | None | SiWx917 |
1396273 1396272 | SSID and BSSID in ap_info structure in WF200 is never populated with the data. | None | EFR32+WF200 |
1448029 | Fixed a build issue when using SL_MATTER_CMP_SECURE_ZIGBEE with the Matter/Zigbee CMP Lighting app. | None | All |
1496432 | Fixed various RAIL timing issues with Zigbee/Matter CMP lighting sample app. | None | EFR32, SiMG301 |
1519604 | Resolved an issue where the switch could become unresponsive after repeated button presses. | None | All |
1519702 | Fixed SSED Matter (over Thread) issue when entering EM2. | None | All |
1564037 | Fixed a Matter SDK issue with double free in binding cluster, leading to a bus fault. | None | All |
Chip Enablement#
Added in 2.8.1#
None.
Added in 2.8.0#
Matter over Thread is supported on the following boards#
MG24 boards:
BRD4186C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@10dBm - xG24-RB4186C
BRD4187C / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm - xG24-RB4187C
BRD2601B / MG24 Developer Kit - xG24-DK2601B
BRD2703A / MG24 Explorer Kit - xG24-EK2703A
MGM24 boards:
BRD4316A / SLWSTK6006A / Wireless Start Kit / 2.4GHz@10dBm - xGM240-RB4316A
BRD4317A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4317A
BRD4318A / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm - xGM240-RB4318A
BRD4319A (Rev A00 only) / SLWSTK6006A / Wireless Starter Kit/ 2.4GHz@20dBm
BRD2704A / Sparkfun Thing Plus MGM240P
BRD4337A / SLWSTK6006A / Wireless Starter Kit / 2.4GHz@20dBm - xGM240-RB4337A
MG26 boards
BRD4116A
BRD4117A
BRD4118A
BRD4120A
BRD4121A
BRD2608A
BRD2709A
MGM26 boards
BRD4350A
BRD4351A
MG30 Boards
BRD4407A
BRD4408A
BRD2719A
Matter over Wi-Fi is supported on the following boards#
SoC mode:
BRD4338A / SiWG917 Wi-Fi 6 and Bluetooth LE 8 MB Flash SoC Pro Kit - SiWx917-PK6031A
BRD2605A / SiWG917 Wi-Fi 6 and Bluetooth LE Dev Kit - SiWx917-DK2605A
BRD4342A / SiWG917 Wi-Fi 6 and Bluetooth LE 8 MB Flash + 8 MB ext PSRAM Radio Board with an internal RF switch - SiWx91x-RB4342A
BRD4343A / SiWG917Y Module Wi-Fi 6 and Bluetooth LE 8MB Flash RF-Pin Radio Board - SiW917Y-RB4343A
Early access for new module board BRD2708A / SiW917Y-EK2708A
NCP mode:
Host Processor:
BRD4186C / EFR32xG24 Wireless 2.4 GHz +10 dBm Radio Board (EFR32 radio board) - xG24-RB4186C
BRD4187C / EFR32xG24 Wireless 2.4 GHz +20 dBm Radio Board - xG24-RB4187C
Silicon Labs Wi-Fi Processor:
SiWx917-EB4346A - SiWx917 Wi-Fi 6 and Bluetooth LE Co-processor EXP Expansion Kit
SiW917Y-RB4357A - SiWN917Y Module Wi-Fi 6 and Bluetooth LE 4MB Flash RF-Pin Co-Processor Radio Board
SLEXP8022A - WF200 Wi-Fi Expansion Kit
Note: Firmware for SiWN917 NCP, and SiWG917 SoC can be found in the Matter Software Artifacts page in the documentation or Assets section of this page. Connectivity firmware update is mandatory for new release binaries.
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
For the list of supported application examples, see Existing Examples. For the details on Matter ecosystems support, see Ecosystems.
New Examples#
None.
Modified Examples#
None.
Removed Examples#
None.
Deprecated Examples#
None.
Known Issues and Limitations#
ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
The Matter logs are printed to the UART interface by default. To view the logs, use the Simplicity Studio console or a standalone terminal emulator such as PuTTY. The logging destination can be controlled by installing the "Logging To UART" or the "Logging to RTT" component under Matter -> Platform -> Utils in a Matter Studio project. | None | All | ||
The Matter device images require approximately 700k in flash space. As a result, only a subset of EFR32MG2x devices are supported. For a complete list of devices supported, consult the documentation located at Matter Hardware Requirements. | None | All | ||
On Windows, Matter projects in Simplicity Studio may fail to build due to a known issue with GCC response files and the operating system's command string length limit. | None | When creating a new project, use shorter Solution and Project names and choose a shorter directory path for the project location. | All | |
A Matter SDK Issue: (https://github.com/project-chip/connectedhomeip). BLE Connection/Timeout error occurs occasionally during commissioning with the chip-tool running on Raspberry Pi or Linux (project-chip#16178). Running on these platforms requires an access point with both 2.4 GHz and 5 GHz capabilities. There is BLE-Wi-Fi interference when connected over the 2.4 GHz channel. | None | This is resolved by connecting the chip-tool device to a 5 GHz SSID and the end device to a 2.4 GHz SSID for the same Wi-Fi network. | All | |
In some rare cases, a Simplicity Studio project build may fail due to missing files in the | None | Delete the | All | |
1197733, 1228823 | Due to an electrical issue on the WPK main boards (BRD4002x), sometimes the current measurement value reported is wrong in the Energy Profiler, making it seem like an ICD is not going to sleep properly even though it is. This issue does not happen when using a WSTK (BRD4001x). | None | All | |
1416694 | The configuration parameters for the internal storage bootloader used in the OTA software updates must always be custom-configured based on the actual image size for the given application. See https://docs.silabs.com/matter/2.8.1/matter-ota/01-ota-bootloader. | None | All | |
1445664 | Chip-Cert executable cannot be used in Windows installations of Simplicity Studio v6. | None | All | |
Matter/Thread: Silicon Labs has provided a complete image file for the Raspberry Pi that can be flashed onto an SD card to create the Matter Hub, which is a Raspberry Pi running Ubuntu and includes a pre-built version of the Open Thread Border Router (OTBR) and chip-tool. The image we have provided is quite large, (approximately 2 GB). As a result, it can take quite a while to download the .zip file and flash it onto an SD card. Depending on your connection, the process could take up to half an hour. Regardless, the demo and development experiences using this pre-built image are a much faster process than building the Matter Hub from scratch. | None | EFR32 | ||
Matter/Thread: Matter attestation credentials can conflict with Lockbits in Series 2, requiring moving the location of the attestation credentials when lockbits are used. Please see the guide Moving the Matter Attestation Credentials on Series 2 (MG24) for details. (1235425) | None | EFR32 | ||
1378481 | USART for IO Stream (RTT) is not supported in Matter Extension v2.8.0-1.5 | None | EFR32 | |
1418676 | Possible race condition in UART driver when excessive use of the Matter shell is performed (sending commands every 250 ms). | None | Reduce the command rate. | EFR32 |
1453646 | Level attribute may get incorrectly changed on level-control stop. | None | EFR32 | |
Enabling "Logging to RTT" with SiWG917 SoC results in OTA update failure due to JLink connection preventing soft reset. | None | Enabled UART logging | SiWG917 | |
1358324 | The BRD4342A PSRAM support is enabled only for the text segment; it is not working for the data and BSS segments. | None | None | BRD4342A |
1366720 | BLE scan issues are observed with Raspberry Pi when the distance between the device and the controller exceeds 3 meters in the SQA lab environment. | None | None | SiWG917 |
The P37 pin must be pulled up to enable the Matter shell or before executing any JLink command for sleepy applications. | None | Hardware limitation | SiWG917 | |
1409219 | On the BRD2605A board, RGB LED pins are not configurable via the LED component or Pin Tool, requiring manual updates to the RTE device file for any new LED pin configurations. | None | Hardware limitation. | SiWG917 |
1557645 | Reset operation fails when trying to debug Matter Wi-Fi using Ozone debugger | None | Update the default reset handler #pragma weak Reset_Handler = RSI_Default_Reset_Handler | SiWG917 |
In the EFR32MG24+WF200 device combination, the WF200 firmware exception is observed when both the ICD and Matter shell are enabled. To enable the Matter shell to work with the Lock application on this device combination, ICD must be disabled. | None | Hardware limitation | SLEXP8022A - WF200 Wi-Fi Expansion Kit | |
The external bootloader should not be used with the EFR32MG24+SiWN917 NCP device combination. Only use the internal bootloader. | None | None | SiWN917 | |
OTA Update: sometimes boot loading with the latest image does not work with the EFR32MG24+WF200 device combination. | None | This issue is resolved by applying the workaround described in the Matter Wi-Fi FAQ. | SLEXP8022A - WF200 Wi-Fi Expansion Kit | |
SiWN917 NCP application OTA upgrade with upgraded WiSeConnect SDK may not be backward compatible with the existing TA. | None | None | SiWN917 | |
Group commands only work for some specific access points when IGMP snooping is disabled. | None | None | All Wi-Fi boards | |
When setting up the Ozone Debugger on Mac, the location of the JLinkDevices.xml file has moved. Follow this documentation to place it in the proper location. | None | None | NA | |
1381843 | LCD is disabled on SiWN917 NCP. | None | LCD is disabled. | SiWN917 |
1485988 | Matter provisioning fails when using CSR over BLE. | None | None | All |
1436465 | Matter/Zigbee CMP Lighting app may reset when add-scene command is received. | None | None | All |
1517161 | Forced NVM3 Repack might add delays during boot or NVM3 heavy operations. | None | None | All |
1513687 | Observed issues creating second fabric with Amazon Alexa related to hardware and version. | None | None | All |
1563443 | Device fails to boot the sleepy apps with LTO build Configuration. | None | None | SiWG917 |
1513661 | Sending UDP packets on SoC Light (over Thread) may cause busfaults. | None | None | All |
1571040, 1571039 | TC-RR-1.1 and TC-DESC-2.2 test cases fail with the Windows App. | None | None | All |
1545117 | ACE 2.1 and 2.2 test cases fail with the test harness. | None | None | All |
1563511 | Windows app not commissioning with the Apple Ecosystem. | Apple Ecosystem Issue | None | All |
1576627 | 917 sometimes fails to advertise BLE. | None | None | SiWx917 |
1446745 | Windows test cases fails with 917SoC. | None | Add delay in between test case run. | SiWG917 |
1388334 | On SiMG301x boards, the Zigbee Matter Light app may, in rare cases, briefly fail to receive Thread packets. This can lead to OTA update image transfer failures. | None | None | SiMG301x |
1569910 | Rare cases of unexpected hangs during schedule setting when running Doorlock sample application on SiMG301x. | None | None | SiMG301x |
1572993 | Rare cases of unexpected hangs during operation when runningThermostat sample application on BRD2719a with the added ethernet port. | None | None | SiMG301x |
1571516 | Rare cases of issues with CMP App that after a successful commissioning, the app drops controller commands and might require reboot or retry commissioning. | None | None | SiMG301x |
1535531 | Manufacturing date length does not match the specs. | None | None | All |
1557629 | Spake2p verifier results in unexpected value with default key, salt and iter params. | None | None | SiWG917 |
1617882 | SiWx devices fail to commission with the latest updated firmware of amazon ecosystem. | None | None | SiWx917 |
1619079 | Hangs seen after commissioning in rare instances on 8MB Series 3 dev kit when running Concurrent Multiprotocol Zigbee and Thread Matter Light. | None | None | BRD4408A |
Impact of Release Changes#
Impact Statements | Migration Guide
Impact Statements#
None.
Migration Guide#
sl_main migration: See sl_system to sl_main migration guide for detailed instructions.
Using This Release#
What's in the Release? | Compatible Software | Installation and Use | Help and Feedback
What's in the Release?#
Silicon Labs Matter Extension for use with Simplicity Studio and SLC-CLI.
Silicon Labs Matter sample applications.
Compatible Software#
Software | Compatible Version or Variant |
|---|---|
Simplicity SDK | |
WiSeConnect SDK | |
GCC (The GNU Compiler Collection) | 12.2.1 (provided with Simplicity Studio) |
Installation and Use#
To get started, download Simplicity Studio from the following link: https://www.silabs.com/developers/simplicity-studio, and install Simplicity SDK v2025.12.2 along with Silicon Labs Matter v2.8.1. For SiWx917, install WiSeConnect v4.0.0 as well.
Quick-start guides are provided for running pre-compiled demos and for building examples manually.
The Developer's Guide provides information on various technical topics.
For details on Studio project upgrades, see Project Upgrades.
In order to run Matter over Thread, a developer must have a Silicon Labs EFR-based device and either:
another EFR-based device and a Raspberry Pi with a 32 GB SD Card,
or an ecosystem device with OpenThread Border Router capabilities, such as Amazon Echo, Apple HomePod, Samsung SmartThings Hub or Google Nest Hub Wi-Fi.
In order to run Matter over Wi-Fi, a developer must have the following hardware:
Silicon Labs Wireless starter/development kit, which is mentioned below.
Raspberry Pi with a 32 GB SD Card or an ecosystem with Matter support
To run your first demo, see our Getting Started Guides.
To kick start your development, see our Developer's Guide.
For information about Secure Vault Integration, see Secure Vault.
To review Security and Software Advisory notifications and manage your notification preferences:
Log in with your account credentials.
Click your profile icon in the upper-right corner of the page.
Select Notifications from the dropdown menu.
In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications.
To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.
To learn more about the software in this release, dive into our online documentation.
Help and Feedback#
Contact Silicon Labs Support.
To use our Ask AI tool to get answers, see the search field at the top of this page.
Note: Ask AI is experimental.
Get help from our developer community.
SDK Release and Maintenance Policy#
See our SDK Release and Maintenance Policy.
Additional Information#
Existing Examples#
Matter over Thread is supported in Simplicity Studio for the following applications#
Light
Light Switch
Lock
Window Covering
Thermostat
OnOff Plug
Sensor
Air Quality Sensor
Refrigerator
Zigbee/Matter CMP Lighting
Closure
Fan Control
Platform Template
Matter over Wi-Fi is supported in Simplicity Studio for the following applications#
SoC and Dev Kit supported applications:
Light
Lock
Light Switch
Window Covering
OnOff Plug
Thermostat
Air Quality Sensor
Sensor
Fan Control
Refrigerator
Oven
Rangehood
Platform Template
Closure
NCP supported applications:
Lock
Thermostat
Window Covering
Note: SiWN917 NCP is the only device combination that supports the Window Covering App.
Matter over Wi-Fi ICD is supported for the following applications#
Lock (ICD is enabled by default)
With chip-tool
With EFR32xG24 with SiWN917 in NCP mode
Window Covering (ICD is enabled by default)
With chip-tool
With EFR32xG24 with SiWN917 in NCP mode
Thermostat
With chip-tool
With EFR32xG24 with SiWN917 in NCP mode
Light Switch
With chip-tool
With SiWG917 SoC
Reference guide to enable the sleepy functionality for Wi-Fi: Wi-Fi ICD.
Ecosystems#
This release has been tested and proven to work for commissioning and control with the following Ecosystems on the hardware and software versions listed below:
Google#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/Lock/Window/Multi-sensor-app | Hardware: Google Nest Hub, Model : GUIK2 Software: Hub SoftwareChromecast 3.78.505901 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Google Home version: 4.3.56.2 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoCBRD4338A | lighting/Lock/Window/Multi-sensor-app | Hardware: Google Nest Hub, Model : GUIK2 Software: Hub Software Version: Chromecast 3.78.505901 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Google Home version: 4.3.56.2 | ASUS (Model: XT8) |
Apple#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/Lock/Window/Multi-sensor-app | Hardware: Home Pod MiniSoftware: (26.1 (23J582)) | Hardware: iPhone 12 pro Software: 17.6 | Apple Home17.6.1 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoC | lighting/Lock/Window/Multi-sensor-app | Hardware: Home Pod MiniSoftware: (26.1 (23J582)) | Hardware: iPhone 12 proSoftware : 17.6 | Apple Home17.6.1 | ASUS (Model: XT8) |
Amazon#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/Window/Multi-sensor-app | Hardware: Echo 4th Gen Model: L4S3RE Software: Hub Software Version:12584499076 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Alexa version: 2.2.641142.0 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoCBRD4338A, | lighting/lock/Window/Multi-sensor-app | Hardware: Echo 4th Gen Model: L4S3RE Software: Hub Software Version:12584499076 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | Alexa version: 2.2.641142.0 | ASUS (Model: XT8) |
Samsung#
Silicon Labs Device | Application | Hub | Phone | App Software | Wi-Fi Access Point | |
|---|---|---|---|---|---|---|
Thread | BRD4187C | lighting/lock/Window/Multi-sensor-app | Hardware: SmartThings Station Software: Hub Software Version: 000.058.00010 Hardware: Charging Hub Software Controller version: 1.0.15-5 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | SmartThings Version: 1.8.37.23 | ASUS (Model: XT8) |
Wi-Fi | SiWx917 SoCBRD4338A, | lighting/lock/Window/Multi-sensor-app | Hardware: SmartThings Station Software: Hub Software Version: 000.058.00010 | Hardware: OPPO Reno CPH1919 Software: Android version 12 | SmartThings Version: 1.8.37.23 | ASUS (Model: XT8) |
Project Upgrades#
Automatic project upgrades from Matter Extension 2.8.0 to 2.8.1 are supported.
Owing to the substantial changes introduced in Matter 1.5, using Studio’s automatic project upgrade flow is not advised for upgrades from pre-2.8.0 Matter Extension projects. Follow these steps to upgrade an existing project from Matter Extension 2.7.0 or earlier to Matter Extension 2.8.1:
Create a new 2.8.1 project for the same application type (Lighting, Lock, etc.).
For each of the files in the project's src/ and include/ directories that were modified from their original version, apply the corresponding changes to the new project.
Replicate the non-default component configurations used in the original project.
Using the ZAP tool, replicate the additional cluster configurations applied in the original project.
Matter Software Artifacts#
Matter Software Artifacts: https://docs.silabs.com/matter/2.8.1/matter-prerequisites/matter-artifacts.