True Random Number Generator (TRNG) Plugin

Detailed Description

True Random Number Generator (TRNG) driver for Silicon Labs devices.

EFR32xG12/EFM32xG12 and newer Silicon Labs devices contains a True Random Number Generator (TRNG) peripheral. The TRNG is a non-deterministic random number generator based on a full hardware solution. The TRNG contains a 64 x 32-bit FIFO for reading out random numbers.

Note
The TRNG peripheral may either be stand-alone or integrated in the SE peripheral depending on the target device.

The samples from entropy source within the TRNG are monitored permanently by 4 built in tests that detect issues with the noise source. The tests are specified in NIST-800-90B and AIS31. The tests that are always checking the entropy source are "Repetition Count Test", "Adaptive Proportion Test (64-sample window)", "Adaptive Proportion Test (4096-sample window)" and the "AIS31 Online Test".

In addition the TRNG has options for running startup tests. When these tests are enabled, the TRNG FIFO will not contain any data before all the startup tests have passed. There are 4 TRNG startup tests, 3 of the tests are specified in NIST-800-90B. These are the "Repetition Count Test", "Adaptive Proportion Test (64-sample window)" and "Adaptive Proportion Test (4096-sample window)". The last startup test is the AIS31 startup test. By default when using this driver all the startup tests are enabled.

The TRNG module implements an entropy source plugin module for mbed TLS that can be used in applications needing random numbers or indirectly using mbed TLS modules that depend on the random number generation interfaces of mbed TLS. Selecting Mbed TLS support for EFM32/EFR32 crypto acceleration component will compile the TRNG module. The TRNG functions are declared in 'mbedtls/sl_crypto/include/trng.h'.

Data Structures

struct  mbedtls_trng_context
 TRNG context structure.
 

Macros

#define MBEDTLS_ERR_TRNG_CONDITIONING_TEST_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000001)
 
#define MBEDTLS_ERR_TRNG_NO_DATA   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000002)
 
#define MBEDTLS_ERR_TRNG_REPETITION_COUNT_TEST_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000003)
 
#define MBEDTLS_ERR_TRNG_ADAPTIVE_PROPORTION_TEST_64_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000004)
 
#define MBEDTLS_ERR_TRNG_ADAPTIVE_PROPORTION_TEST_4096_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000005)
 
#define MBEDTLS_ERR_TRNG_NOISE_ALARM   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000006)
 
#define MBEDTLS_ERR_TRNG_PRELIMINARY_NOISE_ALARM   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000007)
 

Functions

void mbedtls_trng_init (mbedtls_trng_context *ctx)
 Initialize TRNG context.
 
void mbedtls_trng_free (mbedtls_trng_context *ctx)
 Free TRNG context.
 
int mbedtls_trng_set_key (mbedtls_trng_context *ctx, const unsigned char *key)
 Check the TRNG conditioning function.
 
int mbedtls_trng_check_conditioning (mbedtls_trng_context *ctx)
 Check the TRNG conditioning function.
 
int mbedtls_trng_check_entropy (mbedtls_trng_context *ctx)
 Check the TRNG entropy source is producing random data.
 
int mbedtls_trng_poll (mbedtls_trng_context *ctx, unsigned char *output, size_t len, size_t *olen)
 Poll for entropy data.
 
void mbedtls_trng_soft_reset (mbedtls_trng_context *ctx)
 Execute TRNG soft reset.
 
void mbedtls_trng_test_error_callback_set (mbedtls_trng_context *ctx, void(*callback)(void *, int), void *user_arg)
 Set TRNG test error callback.
 

Macro Definition Documentation

#define MBEDTLS_ERR_TRNG_ADAPTIVE_PROPORTION_TEST_4096_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000005)

Adaptive Proportion test over 4096 samples failed. The adaptive proportion test is designed to detect a large loss of entropy that might occur as a result of some physical failure or environmental change affecting the TRNG.

The test will fail when a 2 bit sample from the TRNG is repeated an unusual amount of times within a window of 4096 bits. The adaptive proportion test is further described in NIST-800-90B.

If an application detects this error then the TRNG should be reset. The adaptive proportion test over 4096 samples is always enabled.

Definition at line 122 of file trng.h.

#define MBEDTLS_ERR_TRNG_ADAPTIVE_PROPORTION_TEST_64_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000004)

Adaptive Proportion test over 64 samples failed. The adaptive proportion test is designed to detect a large loss of entropy that might occur as a result of some physical failure or environmental change affecting the TRNG.

The test will fail when a 2 bit sample from the TRNG is repeated an unusual amount of times within a window of 64 bits. The adaptive proportion test is further described in NIST-800-90B.

If an application detects this error then the TRNG should be reset. The adaptive proportion test over 64 samples is always enabled.

Definition at line 109 of file trng.h.

#define MBEDTLS_ERR_TRNG_CONDITIONING_TEST_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000001)

Conditioning test failed.

Definition at line 85 of file trng.h.

#define MBEDTLS_ERR_TRNG_NO_DATA   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000002)

No data received in the TRNG FIFO.

Definition at line 88 of file trng.h.

#define MBEDTLS_ERR_TRNG_NOISE_ALARM   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000006)

AIS31 test noise alarm. The AIS31 test is designed to monitor and verify the statistical distribution of the random numbers from the TRNG. The test performs 512 consecutive 128 bit X^2 calculations with 4 bit words. The details of the AIS31 test can be found in the AIS31 specification.

The test will fail when an unusual statistical distribution of the TRNG output is found.

If an application detects this error then the TRNG should be reset. The AIS31 test is always enabled.

Definition at line 134 of file trng.h.

#define MBEDTLS_ERR_TRNG_PRELIMINARY_NOISE_ALARM   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000007)

AIS31 test Preliminary Noise alarm. The preliminary noise alarms generated from the same AIS31 test that generates MBEDTLS_ERR_TRNG_NOISE_ALARM. The difference between a preliminary noise alarm and a noise alarm is the severity and the expected frequency. A preliminary noise alarm will happen more frequently than a noise alarm, and a preliminary noise alarm is not considered critical. The preliminary noise alarm is not uncommon and should be expected from time to time when reading data from the TRNG.

If an application detects a preliminary noise alarm then the recommended action is to flush the TRNG FIFO, or reset the TRNG.

Definition at line 146 of file trng.h.

#define MBEDTLS_ERR_TRNG_REPETITION_COUNT_TEST_FAILED   ((int)MBEDTLS_ERR_TRNG_BASE | 0x00000003)

Repetition Count test failed. The repetition count test fails when the TRNG detects that the output become "stuck" on a single value for a long period of time. The repetition count test is described in NIST-800-90B.

If an application detects this error then the TRNG should be reset. The repetition count test is always enabled.

Definition at line 96 of file trng.h.

Function Documentation

int mbedtls_trng_check_conditioning ( mbedtls_trng_context ctx)

Check the TRNG conditioning function.

Parameters
ctxTRNG context
Returns
0 if success. MBEDTLS_ERR_TRNG_CONDITIONING_TEST_FAILED on failure.
int mbedtls_trng_check_entropy ( mbedtls_trng_context ctx)

Check the TRNG entropy source is producing random data.

Parameters
ctxTRNG context
Returns
0 if success. Error code if failure. Note that this function can return a MBEDTLS_ERR_TRNG_PRELIMINARY_NOISE_ALARM on some occasions.
void mbedtls_trng_free ( mbedtls_trng_context ctx)

Free TRNG context.

This function will disable the TRNG0 peripheral by stopping the TRNG0 clock. If more than one TRNG contexts are instantiated the user should be aware that one call to mbedtls_trng_free with any of the trng contexts will disable the TRNG0 and effectively disable all other calls in the TRNG API, except mbedtls_trng_init which will enable the TRNG0 again. Normally the application will need only one TRNG context.

Parameters
ctxTRNG context to be released
void mbedtls_trng_init ( mbedtls_trng_context ctx)

Initialize TRNG context.

This function will enable the TRNG0 peripheral by starting the TRNG0 clock, initializing the control register, perform soft reset and wait until data is available in the FIFO. Normally the application will need only one TRNG context. If more than one TRNG contexts are instantiated the user should be aware that mbedtls_trng_free will disable the TRNG0 by stopping the clock, requiring mbedtls_trng_init to be called again before any TRNG API calls can be used. When the TRNG module is used as a standard mbedtls entropy source the context passed to void mbedtls_entropy_init( mbedtls_entropy_context *ctx ) will include one TRNG context and initialize it. The application should not want to keep more than one mbedtls_entropy_context structures as it will consume memory.

Parameters
ctxTRNG context to be initialized
int mbedtls_trng_poll ( mbedtls_trng_context ctx,
unsigned char *  output,
size_t  len,
size_t *  olen 
)

Poll for entropy data.

This function will read available random data from the TRNG FIFO and place it into the output buffer. The len parameter tells this function the maximum number of bytes to read.

Note that the number of bytes read from the TRNG might differ from the number of bytes requested. If any alarms are signaled or the TRNG FIFO is empty then this function will return early.

The return value should be used to see if the operation was successful of if an alarm was encountered while reading the FIFO. The content of the olen parameter can be used to check how many bytes were actually read.

Note
On EFR32 Series 1 devices, the TRNG will have a higher than usual noise alarm rate if the HFPER clock tree is configured to run at HFCLK/2 or faster. For true random numbers, please configure HFPER to HFCLK/4 or slower, if at all possible.
Parameters
ctxTRNG context
outputBuffer to fill with data from the TRNG
lenMaximum number of bytes to fill in output buffer.
olenThe actual amount of bytes put into the buffer (Can be 0)
Returns
  • 0 if no critical failures occurred,
  • MBEDTLS_ERR_TRNG_PRELIMINARY_NOISE_ALARM if a AIS31 preliminary noise alarm was detected while reading the FIFO,
  • MBEDTLS_ERR_TRNG_NOISE_ALARM if an AIS31 noise alarm was detected.
  • MBEDTLS_ERR_TRNG_REPETITION_COUNT_TEST_FAILED if the repetition count test failed while reading the FIFO.
  • MBEDTLS_ERR_TRNG_ADAPTIVE_PROPORTION_TEST_64_FAILED if the adaptive proportion test over 64 samples failed while reading the FIFO.
  • MBEDTLS_ERR_TRNG_ADAPTIVE_PROPORTION_TEST_4096_FAILED if the adaptive proportion test over 4096 samples failed while reading from the FIFO.
int mbedtls_trng_set_key ( mbedtls_trng_context ctx,
const unsigned char *  key 
)

Check the TRNG conditioning function.

Parameters
ctxTRNG context
key128-bit AES key
Returns
0 if success. Error code if failure.
void mbedtls_trng_soft_reset ( mbedtls_trng_context ctx)

Execute TRNG soft reset.

This function performs a TRNG soft reset. The TRNG soft reset can be used to clear error conditions such as Noise Alarms, etc.

Parameters
ctxTRNG context
void mbedtls_trng_test_error_callback_set ( mbedtls_trng_context ctx,
void(*)(void *, int)  callback,
void *  user_arg 
)

Set TRNG test error callback.

This function registers a user defined callback function to be called when an internal TRNG test fails.

Parameters
ctxTRNG context
callbackPointer to callback function which takes a user defined argument as first parameter and the error code as the second parameter.
user_argUser defined argument to be passed to callback function.