mbedtls_cipher_info_t Struct Reference

Cipher information. Allows calling cipher functions in a generic way.

Definition at line 254 of file cipher.h.

#include <cipher.h>

Data Fields

mbedtls_cipher_type_t type
 
mbedtls_cipher_mode_t mode
 
unsigned int key_bitlen
 
const char * name
 
unsigned int iv_size
 
int flags
 
unsigned int block_size
 
const mbedtls_cipher_base_tbase
 

Field Documentation

const mbedtls_cipher_base_t* mbedtls_cipher_info_t::base

Struct for base cipher information and functions.

Definition at line 289 of file cipher.h.

unsigned int mbedtls_cipher_info_t::block_size

The block size, in Bytes.

Definition at line 286 of file cipher.h.

Referenced by mbedtls_cipher_get_block_size().

int mbedtls_cipher_info_t::flags

Bitflag comprised of MBEDTLS_CIPHER_VARIABLE_IV_LEN and MBEDTLS_CIPHER_VARIABLE_KEY_LEN indicating whether the cipher supports variable IV or variable key sizes, respectively.

Definition at line 283 of file cipher.h.

unsigned int mbedtls_cipher_info_t::iv_size

IV or nonce size, in Bytes. For ciphers that accept variable IV sizes, this is the recommended size.

Definition at line 277 of file cipher.h.

Referenced by mbedtls_cipher_get_iv_size().

unsigned int mbedtls_cipher_info_t::key_bitlen

The cipher key length, in bits. This is the default length for variable sized ciphers. Includes parity bits for ciphers like DES.

Definition at line 268 of file cipher.h.

Referenced by mbedtls_cipher_get_key_bitlen().

mbedtls_cipher_mode_t mbedtls_cipher_info_t::mode

The cipher mode. For example, MBEDTLS_MODE_CBC.

Definition at line 262 of file cipher.h.

Referenced by mbedtls_cipher_get_cipher_mode().

const char* mbedtls_cipher_info_t::name

Name of the cipher.

Definition at line 271 of file cipher.h.

Referenced by mbedtls_cipher_get_name().

mbedtls_cipher_type_t mbedtls_cipher_info_t::type

Full cipher identifier. For example, MBEDTLS_CIPHER_AES_256_CBC.

Definition at line 259 of file cipher.h.

Referenced by mbedtls_cipher_get_type().


The documentation for this struct was generated from the following file:
  • cipher.h