mbedtls_trng_context Struct Reference
TRNG context structure.
Definition at line 151
of file trng.h
.
#include <
trng.h
>
Data Fields | |
TRNG_TypeDef * | trng |
void(* | test_error_callback )(void *user_arg, int error_code) |
void * | test_error_callback_user_arg |
Field Documentation
void(* mbedtls_trng_context::test_error_callback) (void *user_arg, int error_code) |
User defined callback to be called when an internal TRNG test fails.
Definition at line 157
of file trng.h
.
void* mbedtls_trng_context::test_error_callback_user_arg |
User defined argument to TRNG test error callback.
Definition at line 160
of file trng.h
.
TRNG_TypeDef* mbedtls_trng_context::trng |
TRNG register block pointer.
Definition at line 154
of file trng.h
.
The documentation for this struct was generated from the following file:
trng.h