Asymmetric cryptography
Functions | |
psa_status_t | psa_sign_hash (psa_key_handle_t handle, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, uint8_t *signature, size_t signature_size, size_t *signature_length) |
Sign a hash or short message with a private key. | |
psa_status_t | psa_verify_hash (psa_key_handle_t handle, psa_algorithm_t alg, const uint8_t *hash, size_t hash_length, const uint8_t *signature, size_t signature_length) |
Verify the signature a hash or short message using a public key. | |
psa_status_t | psa_asymmetric_encrypt (psa_key_handle_t handle, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length) |
Encrypt a short message with a public key. | |
psa_status_t | psa_asymmetric_decrypt (psa_key_handle_t handle, psa_algorithm_t alg, const uint8_t *input, size_t input_length, const uint8_t *salt, size_t salt_length, uint8_t *output, size_t output_size, size_t *output_length) |
Decrypt a short message with a private key. | |
Function Documentation
psa_status_t psa_asymmetric_decrypt | ( | psa_key_handle_t |
handle, |
psa_algorithm_t | alg, |
||
const uint8_t * | input, |
||
size_t | input_length, |
||
const uint8_t * | salt, |
||
size_t | salt_length, |
||
uint8_t * | output, |
||
size_t | output_size, |
||
size_t * | output_length |
||
) |
Decrypt a short message with a private key.
- Parameters
-
handle
Handle to the key to use for the operation. It must be an asymmetric key pair. alg
An asymmetric encryption algorithm that is compatible with the type of handle
.[in] input
The message to decrypt. input_length
Size of the input
buffer in bytes.[in] salt
A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL
. If the algorithm supports an optional salt and you do not want to pass a salt, passNULL
.
- For PSA_ALG_RSA_PKCS1V15_CRYPT, no salt is supported.
- Parameters
-
salt_length
Size of the salt
buffer in bytes. Ifsalt
isNULL
, pass 0.[out] output
Buffer where the decrypted message is to be written. output_size
Size of the output
buffer in bytes.[out] output_length
On success, the number of bytes that make up the returned output.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the output
buffer is too small. You can determine a sufficient buffer size by callingPSA_ASYMMETRIC_DECRYPT_OUTPUT_SIZE
(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofhandle
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_INVALID_PADDING
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
psa_status_t psa_asymmetric_encrypt | ( | psa_key_handle_t |
handle, |
psa_algorithm_t | alg, |
||
const uint8_t * | input, |
||
size_t | input_length, |
||
const uint8_t * | salt, |
||
size_t | salt_length, |
||
uint8_t * | output, |
||
size_t | output_size, |
||
size_t * | output_length |
||
) |
Encrypt a short message with a public key.
- Parameters
-
handle
Handle to the key to use for the operation. It must be a public key or an asymmetric key pair. alg
An asymmetric encryption algorithm that is compatible with the type of handle
.[in] input
The message to encrypt. input_length
Size of the input
buffer in bytes.[in] salt
A salt or label, if supported by the encryption algorithm. If the algorithm does not support a salt, pass NULL
. If the algorithm supports an optional salt and you do not want to pass a salt, passNULL
.
- For PSA_ALG_RSA_PKCS1V15_CRYPT, no salt is supported.
- Parameters
-
salt_length
Size of the salt
buffer in bytes. Ifsalt
isNULL
, pass 0.[out] output
Buffer where the encrypted message is to be written. output_size
Size of the output
buffer in bytes.[out] output_length
On success, the number of bytes that make up the returned output.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the output
buffer is too small. You can determine a sufficient buffer size by callingPSA_ASYMMETRIC_ENCRYPT_OUTPUT_SIZE
(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofhandle
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
psa_status_t psa_sign_hash | ( | psa_key_handle_t |
handle, |
psa_algorithm_t | alg, |
||
const uint8_t * | hash, |
||
size_t | hash_length, |
||
uint8_t * | signature, |
||
size_t | signature_size, |
||
size_t * | signature_length |
||
) |
Sign a hash or short message with a private key.
Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(). Then pass the resulting hash as the hash
parameter to this function. You can use PSA_ALG_SIGN_GET_HASH(alg
) to determine the hash algorithm to use.
- Parameters
-
handle
Handle to the key to use for the operation. It must be an asymmetric key pair. alg
A signature algorithm that is compatible with the type of handle
.[in] hash
The hash or message to sign. hash_length
Size of the hash
buffer in bytes.[out] signature
Buffer where the signature is to be written. signature_size
Size of the signature
buffer in bytes.[out] signature_length
On success, the number of bytes that make up the returned signature value.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the signature
buffer is too small. You can determine a sufficient buffer size by callingPSA_SIGN_OUTPUT_SIZE
(key_type
,key_bits
,alg
) wherekey_type
andkey_bits
are the type and bit-size respectively ofhandle
.PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_ENTROPY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
psa_status_t psa_verify_hash | ( | psa_key_handle_t |
handle, |
psa_algorithm_t | alg, |
||
const uint8_t * | hash, |
||
size_t | hash_length, |
||
const uint8_t * | signature, |
||
size_t | signature_length |
||
) |
Verify the signature a hash or short message using a public key.
Note that to perform a hash-and-sign signature algorithm, you must first calculate the hash by calling psa_hash_setup(), psa_hash_update() and psa_hash_finish(). Then pass the resulting hash as the hash
parameter to this function. You can use PSA_ALG_SIGN_GET_HASH(alg
) to determine the hash algorithm to use.
- Parameters
-
handle
Handle to the key to use for the operation. It must be a public key or an asymmetric key pair. alg
A signature algorithm that is compatible with the type of handle
.[in] hash
The hash or message whose signature is to be verified. hash_length
Size of the hash
buffer in bytes.[in] signature
Buffer containing the signature to verify. signature_length
Size of the signature
buffer in bytes.
- Return values
-
PSA_SUCCESS
The signature is valid. PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
PSA_ERROR_INVALID_SIGNATURE
The calculation was perfomed successfully, but the passed signature is not a valid signature. PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_INVALID_ARGUMENT
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.