Key import and export
Functions | |
psa_status_t | psa_import_key (const psa_key_attributes_t *attributes, const uint8_t *data, size_t data_length, psa_key_handle_t *handle) |
Import a key in binary format. | |
psa_status_t | psa_export_key (psa_key_handle_t handle, uint8_t *data, size_t data_size, size_t *data_length) |
Export a key in binary format. | |
psa_status_t | psa_export_public_key (psa_key_handle_t handle, uint8_t *data, size_t data_size, size_t *data_length) |
Export a public key or the public part of a key pair in binary format. | |
Function Documentation
psa_status_t psa_export_key | ( | psa_key_handle_t |
handle, |
uint8_t * | data, |
||
size_t | data_size, |
||
size_t * | data_length |
||
) |
Export a key in binary format.
The output of this function can be passed to psa_import_key() to create an equivalent object.
If the implementation of psa_import_key() supports other formats beyond the format specified here, the output from psa_export_key() must use the representation specified here, not the original representation.
For standard key types, the output format is as follows:
- For symmetric keys (including MAC keys), the format is the raw bytes of the key.
- For DES, the key data consists of 8 bytes. The parity bits must be correct.
- For Triple-DES, the format is the concatenation of the two or three DES keys.
- For RSA key pairs (PSA_KEY_TYPE_RSA_KEY_PAIR), the format is the non-encrypted DER encoding of the representation defined by PKCS#1 (RFC 8017) as
RSAPrivateKey
, version 0.
``` RSAPrivateKey ::= SEQUENCE { version INTEGER, – must be 0 modulus INTEGER, – n publicExponent INTEGER, – e privateExponent INTEGER, – d prime1 INTEGER, – p prime2 INTEGER, – q exponent1 INTEGER, – d mod (p-1) exponent2 INTEGER, – d mod (q-1) coefficient INTEGER, – (inverse of q) mod p }
```
- For elliptic curve key pairs (key types for which PSA_KEY_TYPE_IS_ECC_KEY_PAIR is true), the format is a representation of the private value as a
ceiling(m/8)
-byte string wherem
is the bit size associated with the curve, i.e. the bit size of the order of the curve's coordinate field. This byte string is in little-endian order for Montgomery curves (curve typesPSA_ECC_FAMILY_CURVEXXX
), and in big-endian order for Weierstrass curves (curve typesPSA_ECC_FAMILY_SECTXXX
,PSA_ECC_FAMILY_SECPXXX
andPSA_ECC_FAMILY_BRAINPOOL_PXXX
). For Weierstrass curves, this is the content of theprivateKey
field of theECPrivateKey
format defined by RFC 5915. For Montgomery curves, the format is defined by RFC 7748, and output is masked according to §5. - For Diffie-Hellman key exchange key pairs (key types for which PSA_KEY_TYPE_IS_DH_KEY_PAIR is true), the format is the representation of the private key
x
as a big-endian byte string. The length of the byte string is the private key size in bytes (leading zeroes are not stripped). - For public keys (key types for which PSA_KEY_TYPE_IS_PUBLIC_KEY is true), the format is the same as for psa_export_public_key().
The policy on the key must have the usage flag PSA_KEY_USAGE_EXPORT set.
- Parameters
-
handle
Handle to the key to export. [out] data
Buffer where the key data is to be written. data_size
Size of the data
buffer in bytes.[out] data_length
On success, the number of bytes that make up the key data.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_NOT_PERMITTED
The key does not have the PSA_KEY_USAGE_EXPORT flag. PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the data
buffer is too small. You can determine a sufficient buffer size by callingPSA_KEY_EXPORT_MAX_SIZE
(type
,bits
) wheretype
is the key type andbits
is the key size in bits.PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
- For elliptic curve key pairs (key types for which PSA_KEY_TYPE_IS_ECC_KEY_PAIR is true), the format is a representation of the private value as a
psa_status_t psa_export_public_key | ( | psa_key_handle_t |
handle, |
uint8_t * | data, |
||
size_t | data_size, |
||
size_t * | data_length |
||
) |
Export a public key or the public part of a key pair in binary format.
The output of this function can be passed to psa_import_key() to create an object that is equivalent to the public key.
This specification supports a single format for each key type. Implementations may support other formats as long as the standard format is supported. Implementations that support other formats should ensure that the formats are clearly unambiguous so as to minimize the risk that an invalid input is accidentally interpreted according to a different format.
For standard key types, the output format is as follows:
- For RSA public keys (PSA_KEY_TYPE_RSA_PUBLIC_KEY), the DER encoding of the representation defined by RFC 3279 §2.3.1 as
RSAPublicKey
.
``` RSAPublicKey ::= SEQUENCE { modulus INTEGER, – n publicExponent INTEGER } – e
```
- For elliptic curve public keys (key types for which PSA_KEY_TYPE_IS_ECC_PUBLIC_KEY is true), the format is the uncompressed representation defined by SEC1 §2.3.3 as the content of an ECPoint. Let
m
be the bit size associated with the curve, i.e. the bit size ofq
for a curve overF_q
. The representation consists of:- The byte 0x04;
x_P
as aceiling(m/8)
-byte string, big-endian;y_P
as aceiling(m/8)
-byte string, big-endian.
- For Diffie-Hellman key exchange public keys (key types for which PSA_KEY_TYPE_IS_DH_PUBLIC_KEY is true), the format is the representation of the public key
y = g^x mod p
as a big-endian byte string. The length of the byte string is the length of the base primep
in bytes.
Exporting a public key object or the public part of a key pair is always permitted, regardless of the key's usage flags.
- Parameters
-
handle
Handle to the key to export. [out] data
Buffer where the key data is to be written. data_size
Size of the data
buffer in bytes.[out] data_length
On success, the number of bytes that make up the key data.
- Return values
-
PSA_SUCCESS
PSA_ERROR_INVALID_HANDLE
PSA_ERROR_INVALID_ARGUMENT
The key is neither a public key nor a key pair. PSA_ERROR_NOT_SUPPORTED
PSA_ERROR_BUFFER_TOO_SMALL
The size of the data
buffer is too small. You can determine a sufficient buffer size by callingPSA_KEY_EXPORT_MAX_SIZE
(PSA_KEY_TYPE_PUBLIC_KEY_OF_KEY_PAIR(type
),bits
) wheretype
is the key type andbits
is the key size in bits.PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.
- For elliptic curve public keys (key types for which PSA_KEY_TYPE_IS_ECC_PUBLIC_KEY is true), the format is the uncompressed representation defined by SEC1 §2.3.3 as the content of an ECPoint. Let
psa_status_t psa_import_key | ( | const psa_key_attributes_t * | attributes, |
const uint8_t * | data, |
||
size_t | data_length, |
||
psa_key_handle_t * |
handle |
||
) |
Import a key in binary format.
This function supports any output from psa_export_key(). Refer to the documentation of psa_export_public_key() for the format of public keys and to the documentation of psa_export_key() for the format for other key types.
The key data determines the key size. The attributes may optionally specify a key size; in this case it must match the size determined from the key data. A key size of 0 in attributes
indicates that the key size is solely determined by the key data.
Implementations must reject an attempt to import a key of size 0.
This specification supports a single format for each key type. Implementations may support other formats as long as the standard format is supported. Implementations that support other formats should ensure that the formats are clearly unambiguous so as to minimize the risk that an invalid input is accidentally interpreted according to a different format.
- Parameters
-
[in] attributes
The attributes for the new key. The key size is always determined from the data
buffer. If the key size inattributes
is nonzero, it must be equal to the size fromdata
.[out] handle
On success, a handle to the newly created key. 0
on failure.[in] data
Buffer containing the key data. The content of this buffer is interpreted according to the type declared in attributes
. All implementations must support at least the format described in the documentation of psa_export_key() or psa_export_public_key() for the chosen type. Implementations may allow other formats, but should be conservative: implementations should err on the side of rejecting content if it may be erroneous (e.g. wrong type or truncated data).data_length
Size of the data
buffer in bytes.
- Return values
-
PSA_SUCCESS
Success. If the key is persistent, the key material and the key's metadata have been saved to persistent storage. PSA_ERROR_ALREADY_EXISTS
This is an attempt to create a persistent key, and there is already a persistent key with the given identifier. PSA_ERROR_NOT_SUPPORTED
The key type or key size is not supported, either by the implementation in general or in this particular persistent location. PSA_ERROR_INVALID_ARGUMENT
The key attributes, as a whole, are invalid. PSA_ERROR_INVALID_ARGUMENT
The key data is not correctly formatted. PSA_ERROR_INVALID_ARGUMENT
The size in attributes
is nonzero and does not match the size of the key data.PSA_ERROR_INSUFFICIENT_MEMORY
PSA_ERROR_INSUFFICIENT_STORAGE
PSA_ERROR_COMMUNICATION_FAILURE
PSA_ERROR_STORAGE_FAILURE
PSA_ERROR_HARDWARE_FAILURE
PSA_ERROR_CORRUPTION_DETECTED
PSA_ERROR_BAD_STATE
The library has not been previously initialized by psa_crypto_init(). It is implementation-dependent whether a failure to initialize results in this error code.