Secure Element Message Authentication Codes
Detailed Description
Generation and authentication of Message Authentication Codes (MACs) using a secure element can be done either as a single function call (via the psa_drv_se_mac_generate_t
or psa_drv_se_mac_verify_t
functions), or in parts using the following sequence:
psa_drv_se_mac_setup_t
psa_drv_se_mac_update_t
psa_drv_se_mac_update_t
- ...
psa_drv_se_mac_finish_t
orpsa_drv_se_mac_finish_verify_t
If a previously started secure element MAC operation needs to be terminated, it should be done so by the psa_drv_se_mac_abort_t
. Failure to do so may result in allocated resources not being freed or in other undefined behavior.
Data Structures | |
struct | psa_drv_se_mac_t |
A struct containing all of the function pointers needed to perform secure element MAC operations. | |
Typedefs | |
typedef psa_status_t(* | psa_drv_se_mac_setup_t) (psa_drv_se_context_t *drv_context, void *op_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm) |
A function that starts a secure element MAC operation for a PSA Crypto Driver implementation. | |
typedef psa_status_t(* | psa_drv_se_mac_update_t) (void *op_context, const uint8_t *p_input, size_t input_length) |
A function that continues a previously started secure element MAC operation. | |
typedef psa_status_t(* | psa_drv_se_mac_finish_t) (void *op_context, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length) |
a function that completes a previously started secure element MAC operation by returning the resulting MAC. | |
typedef psa_status_t(* | psa_drv_se_mac_finish_verify_t) (void *op_context, const uint8_t *p_mac, size_t mac_length) |
A function that completes a previously started secure element MAC operation by comparing the resulting MAC against a provided value. | |
typedef psa_status_t(* | psa_drv_se_mac_abort_t) (void *op_context) |
A function that aborts a previous started secure element MAC operation. | |
typedef psa_status_t(* | psa_drv_se_mac_generate_t) (psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length) |
A function that performs a secure element MAC operation in one command and returns the calculated MAC. | |
typedef psa_status_t(* | psa_drv_se_mac_verify_t) (psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, const uint8_t *p_mac, size_t mac_length) |
A function that performs a secure element MAC operation in one command and compares the resulting MAC against a provided value. | |
Typedef Documentation
typedef psa_status_t(* psa_drv_se_mac_abort_t) (void *op_context) |
A function that aborts a previous started secure element MAC operation.
- Parameters
-
[in,out] op_context
A hardware-specific structure for the previously started MAC operation to be aborted
Definition at line 250
of file crypto_se_driver.h
.
typedef psa_status_t(* psa_drv_se_mac_finish_t) (void *op_context, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length) |
a function that completes a previously started secure element MAC operation by returning the resulting MAC.
- Parameters
-
[in,out] op_context
A hardware-specific structure for the previously started MAC operation to be finished [out] p_mac
A buffer where the generated MAC will be placed [in] mac_size
The size in bytes of the buffer that has been allocated for the output
buffer[out] p_mac_length
After completion, will contain the number of bytes placed in the p_mac
buffer
- Return values
-
PSA_SUCCESS
Success.
Definition at line 219
of file crypto_se_driver.h
.
typedef psa_status_t(* psa_drv_se_mac_finish_verify_t) (void *op_context, const uint8_t *p_mac, size_t mac_length) |
A function that completes a previously started secure element MAC operation by comparing the resulting MAC against a provided value.
- Parameters
-
[in,out] op_context
A hardware-specific structure for the previously started MAC operation to be fiinished [in] p_mac
The MAC value against which the resulting MAC will be compared against [in] mac_length
The size in bytes of the value stored in p_mac
- Return values
-
PSA_SUCCESS
The operation completed successfully and the MACs matched each other PSA_ERROR_INVALID_SIGNATURE
The operation completed successfully, but the calculated MAC did not match the provided MAC
Definition at line 240
of file crypto_se_driver.h
.
typedef psa_status_t(* psa_drv_se_mac_generate_t) (psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length) |
A function that performs a secure element MAC operation in one command and returns the calculated MAC.
- Parameters
-
[in,out] drv_context
The driver context structure. [in] p_input
A buffer containing the message to be MACed [in] input_length
The size in bytes of p_input
[in] key_slot
The slot of the key to be used [in] alg
The algorithm to be used to underlie the MAC operation [out] p_mac
A buffer where the generated MAC will be placed [in] mac_size
The size in bytes of the p_mac
buffer[out] p_mac_length
After completion, will contain the number of bytes placed in the output
buffer
- Return values
-
PSA_SUCCESS
Success.
Definition at line 270
of file crypto_se_driver.h
.
typedef psa_status_t(* psa_drv_se_mac_setup_t) (psa_drv_se_context_t *drv_context, void *op_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm) |
A function that starts a secure element MAC operation for a PSA Crypto Driver implementation.
- Parameters
-
[in,out] drv_context
The driver context structure. [in,out] op_context
A structure that will contain the hardware-specific MAC context [in] key_slot
The slot of the key to be used for the operation [in] algorithm
The algorithm to be used to underly the MAC operation
- Return values
-
PSA_SUCCESS
Success.
Definition at line 184
of file crypto_se_driver.h
.
typedef psa_status_t(* psa_drv_se_mac_update_t) (void *op_context, const uint8_t *p_input, size_t input_length) |
A function that continues a previously started secure element MAC operation.
- Parameters
-
[in,out] op_context
A hardware-specific structure for the previously-established MAC operation to be updated [in] p_input
A buffer containing the message to be appended to the MAC operation [in] input_length
The size in bytes of the input message buffer
Definition at line 199
of file crypto_se_driver.h
.
typedef psa_status_t(* psa_drv_se_mac_verify_t) (psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, const uint8_t *p_mac, size_t mac_length) |
A function that performs a secure element MAC operation in one command and compares the resulting MAC against a provided value.
- Parameters
-
[in,out] drv_context
The driver context structure. [in] p_input
A buffer containing the message to be MACed [in] input_length
The size in bytes of input
[in] key_slot
The slot of the key to be used [in] alg
The algorithm to be used to underlie the MAC operation [in] p_mac
The MAC value against which the resulting MAC will be compared against [in] mac_length
The size in bytes of mac
- Return values
-
PSA_SUCCESS
The operation completed successfully and the MACs matched each other PSA_ERROR_INVALID_SIGNATURE
The operation completed successfully, but the calculated MAC did not match the provided MAC
Definition at line 299
of file crypto_se_driver.h
.