psa_drv_entropy_t Struct Reference
A struct containing all of the function pointers needed to interface to an entropy source.
PSA Crypto API implementations should populate instances of the table as appropriate upon startup.
If one of the functions is not implemented, it should be set to NULL.
Definition at line 94
of file crypto_entropy_driver.h
.
#include <
crypto_entropy_driver.h
>
Data Fields | |
const size_t | context_size |
psa_drv_entropy_init_t | p_init |
psa_drv_entropy_get_bits_t | p_get_bits |
Field Documentation
const size_t psa_drv_entropy_t::context_size |
The driver-specific size of the entropy context
Definition at line 96
of file crypto_entropy_driver.h
.
psa_drv_entropy_get_bits_t psa_drv_entropy_t::p_get_bits |
Function that performs the get_bits operation for the entropy source
Definition at line 100
of file crypto_entropy_driver.h
.
psa_drv_entropy_init_t psa_drv_entropy_t::p_init |
Function that performs initialization for the entropy source
Definition at line 98
of file crypto_entropy_driver.h
.
The documentation for this struct was generated from the following file:
crypto_entropy_driver.h