psa_drv_se_asymmetric_t Struct Reference
A struct containing all of the function pointers needed to implement asymmetric cryptographic operations using secure elements.
PSA Crypto API implementations should populate instances of the table as appropriate upon startup or at build time.
If one of the functions is not implemented, it should be set to NULL.
Definition at line 682
of file crypto_se_driver.h
.
#include <
crypto_se_driver.h
>
Data Fields | |
psa_drv_se_asymmetric_sign_t | p_sign |
psa_drv_se_asymmetric_verify_t | p_verify |
psa_drv_se_asymmetric_encrypt_t | p_encrypt |
psa_drv_se_asymmetric_decrypt_t | p_decrypt |
Field Documentation
psa_drv_se_asymmetric_decrypt_t psa_drv_se_asymmetric_t::p_decrypt |
Function that performs an asymmetric decrypt operation
Definition at line 690
of file crypto_se_driver.h
.
psa_drv_se_asymmetric_encrypt_t psa_drv_se_asymmetric_t::p_encrypt |
Function that performs an asymmetric encrypt operation
Definition at line 688
of file crypto_se_driver.h
.
psa_drv_se_asymmetric_sign_t psa_drv_se_asymmetric_t::p_sign |
Function that performs an asymmetric sign operation
Definition at line 684
of file crypto_se_driver.h
.
psa_drv_se_asymmetric_verify_t psa_drv_se_asymmetric_t::p_verify |
Function that performs an asymmetric verify operation
Definition at line 686
of file crypto_se_driver.h
.
The documentation for this struct was generated from the following file:
crypto_se_driver.h