psa_drv_se_cipher_t Struct Reference
A struct containing all of the function pointers needed to implement cipher operations using secure elements.
PSA Crypto API implementations should populate instances of the table as appropriate upon startup or at build time.
If one of the functions is not implemented (such as psa_drv_se_cipher_ecb_t
), it should be set to NULL.
Definition at line 509
of file crypto_se_driver.h
.
#include <
crypto_se_driver.h
>
Field Documentation
size_t psa_drv_se_cipher_t::context_size |
The size in bytes of the hardware-specific secure element cipher context structure
Definition at line 513
of file crypto_se_driver.h
.
psa_drv_se_cipher_abort_t psa_drv_se_cipher_t::p_abort |
Function that aborts a cipher operation
Definition at line 523
of file crypto_se_driver.h
.
psa_drv_se_cipher_ecb_t psa_drv_se_cipher_t::p_ecb |
Function that performs ECB mode for a cipher operation (Danger: ECB mode should not be used directly by clients of the PSA Crypto Client API)
Definition at line 528
of file crypto_se_driver.h
.
psa_drv_se_cipher_finish_t psa_drv_se_cipher_t::p_finish |
Function that completes a cipher operation
Definition at line 521
of file crypto_se_driver.h
.
psa_drv_se_cipher_set_iv_t psa_drv_se_cipher_t::p_set_iv |
Function that sets a cipher IV (if necessary)
Definition at line 517
of file crypto_se_driver.h
.
psa_drv_se_cipher_setup_t psa_drv_se_cipher_t::p_setup |
Function that performs a cipher setup operation
Definition at line 515
of file crypto_se_driver.h
.
psa_drv_se_cipher_update_t psa_drv_se_cipher_t::p_update |
Function that performs a cipher update operation
Definition at line 519
of file crypto_se_driver.h
.
The documentation for this struct was generated from the following file:
crypto_se_driver.h